SPI Peripheral Driver Error Codes#

Bootloader error codes returned by the SPI Peripheral driver.

Offset from BOOTLOADER_ERROR_SPI_PERIPHERAL_BASE

Macros#

#define
BOOTLOADER_ERROR_SPI_PERIPHERAL_UNINIT (BOOTLOADER_ERROR_SPI_PERIPHERAL_BASE | 0x01)

Operation not allowed because hardware has not been initialized.

#define
BOOTLOADER_ERROR_SPI_PERIPHERAL_INIT (BOOTLOADER_ERROR_SPI_PERIPHERAL_BASE | 0x02)

Hardware fail during initialization.

#define
BOOTLOADER_ERROR_SPI_PERIPHERAL_ARGUMENT (BOOTLOADER_ERROR_SPI_PERIPHERAL_BASE | 0x03)

Invalid argument.

#define
BOOTLOADER_ERROR_SPI_PERIPHERAL_TIMEOUT (BOOTLOADER_ERROR_SPI_PERIPHERAL_BASE | 0x04)

Timeout.

#define
BOOTLOADER_ERROR_SPI_PERIPHERAL_OVERFLOW (BOOTLOADER_ERROR_SPI_PERIPHERAL_BASE | 0x05)

Buffer overflow condition.

#define
BOOTLOADER_ERROR_SPI_PERIPHERAL_BUSY (BOOTLOADER_ERROR_SPI_PERIPHERAL_BASE | 0x06)

Busy condition.

Macro Definition Documentation#

BOOTLOADER_ERROR_SPI_PERIPHERAL_UNINIT#

#define BOOTLOADER_ERROR_SPI_PERIPHERAL_UNINIT
Value:
  (BOOTLOADER_ERROR_SPI_PERIPHERAL_BASE | 0x01)

Operation not allowed because hardware has not been initialized.


Definition at line 310 of file platform/bootloader/api/btl_errorcode.h

BOOTLOADER_ERROR_SPI_PERIPHERAL_INIT#

#define BOOTLOADER_ERROR_SPI_PERIPHERAL_INIT
Value:
  (BOOTLOADER_ERROR_SPI_PERIPHERAL_BASE | 0x02)

Hardware fail during initialization.


Definition at line 313 of file platform/bootloader/api/btl_errorcode.h

BOOTLOADER_ERROR_SPI_PERIPHERAL_ARGUMENT#

#define BOOTLOADER_ERROR_SPI_PERIPHERAL_ARGUMENT
Value:
  (BOOTLOADER_ERROR_SPI_PERIPHERAL_BASE | 0x03)

Invalid argument.


Definition at line 316 of file platform/bootloader/api/btl_errorcode.h

BOOTLOADER_ERROR_SPI_PERIPHERAL_TIMEOUT#

#define BOOTLOADER_ERROR_SPI_PERIPHERAL_TIMEOUT
Value:
  (BOOTLOADER_ERROR_SPI_PERIPHERAL_BASE | 0x04)

Timeout.


Definition at line 319 of file platform/bootloader/api/btl_errorcode.h

BOOTLOADER_ERROR_SPI_PERIPHERAL_OVERFLOW#

#define BOOTLOADER_ERROR_SPI_PERIPHERAL_OVERFLOW
Value:
  (BOOTLOADER_ERROR_SPI_PERIPHERAL_BASE | 0x05)

Buffer overflow condition.


Definition at line 322 of file platform/bootloader/api/btl_errorcode.h

BOOTLOADER_ERROR_SPI_PERIPHERAL_BUSY#

#define BOOTLOADER_ERROR_SPI_PERIPHERAL_BUSY
Value:
  (BOOTLOADER_ERROR_SPI_PERIPHERAL_BASE | 0x06)

Busy condition.


Definition at line 325 of file platform/bootloader/api/btl_errorcode.h