Application Data.

Public Attributes#

uint32_t

Bitfield representing type of application, e.g., APPLICATION_TYPE_ZIGBEE.

uint32_t

Version number for this application.

uint32_t

Capabilities of this application.

uint8_t

Unique ID (UUID or GUID) for the product this application is built for.

Public Attribute Documentation#

type#

uint32_t ApplicationData_t::type

Bitfield representing type of application, e.g., APPLICATION_TYPE_ZIGBEE.


Definition at line 98 of file platform/bootloader/api/application_properties.h

version#

uint32_t ApplicationData_t::version

Version number for this application.


Definition at line 100 of file platform/bootloader/api/application_properties.h

capabilities#

uint32_t ApplicationData_t::capabilities

Capabilities of this application.


Definition at line 102 of file platform/bootloader/api/application_properties.h

productId#

uint8_t ApplicationData_t::productId[16]

Unique ID (UUID or GUID) for the product this application is built for.


Definition at line 104 of file platform/bootloader/api/application_properties.h