Bootload#

Methods to verify and bootload application images.

Functions#

uint32_t

Get base address of the bootloader upgrade image.

uint32_t

Get the version of the bootloader.

bool

Get the version of the application.

bool

Check application properties magic.

bool

Check application properties struct version.

bool
bootload_verifyApplication(uint32_t startAddress)

Verify the application image stored in the Flash memory starting at the address startAddress.

void
bootload_bootloaderCallback(uint32_t offset, uint8_t data[], size_t length, void *context)

Bootloader upgrade callback implementation.

void
bootload_applicationCallback(uint32_t address, uint8_t data[], size_t length, void *context)

Image data callback implementation.

bool
bootload_commitBootloaderUpgrade(uint32_t upgradeAddress, uint32_t size)

Perform a bootloader upgrade using the upgrade image present at upgradeAddress with length size.

bool
bootload_verifyApplicationVersion(uint32_t appVersion, bool checkRemainingAppUpgrades)

Verify the application version for rollback protection.

bool
bootload_storeApplicationVersion(uint32_t startAddress)

Store the application version.

uint32_t

Count the total remaining number of application upgrades.

void

Store application version reset magic.

void

Clean the application versions seen.

uint32_t

Get the application version storage capacity.

uint32_t *

Get the address of the application version storage buffer.

bool
bootload_gotCertificate(const void *appProp)

Check whether the application contains a certificate.

bool
bootload_verifyCertificate(const void *cert)

Verify a certificate with a bootloader certificate.

bool
bootload_verifyApplicationCertificate(const void *appProp, const void *gotCert)

Verify the application certificate.

Function Documentation#

bootload_getUpgradeLocation#

uint32_t bootload_getUpgradeLocation (void )

Get base address of the bootloader upgrade image.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Returns the base address of bootloader upgrade image.


bootload_getBootloaderVersion#

uint32_t bootload_getBootloaderVersion (void )

Get the version of the bootloader.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Returns the version of the bootloader.


bootload_getApplicationVersion#

bool bootload_getApplicationVersion (uint32_t * version)

Get the version of the application.

Parameters
TypeDirectionArgument NameDescription
uint32_t *[out]version

The retrieved application version

Returns

  • Returns true if the version was retrieved successfully


bootload_checkApplicationPropertiesMagic#

bool bootload_checkApplicationPropertiesMagic (void * appProperties)

Check application properties magic.

Parameters
TypeDirectionArgument NameDescription
void *N/AappProperties

Pointer to ApplicationProperties_t

Returns

  • True if the application properties magic is valid.


bootload_checkApplicationPropertiesVersion#

bool bootload_checkApplicationPropertiesVersion (void * appProperties)

Check application properties struct version.

Parameters
TypeDirectionArgument NameDescription
void *N/AappProperties

Pointer to ApplicationProperties_t

Returns

  • True if the application properties struct version is compatible with the bootloader.


bootload_verifyApplication#

bool bootload_verifyApplication (uint32_t startAddress)

Verify the application image stored in the Flash memory starting at the address startAddress.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]startAddress

Starting address of the application

If secure boot is enforced, the function will only return true if the cryptographic signature of the application is valid. Else, the application is verified according to the signature type defined in the ApplicationProperties_t structure embedded in the application. Silicon Labs wireless stacks declare this structure. Applications, which are not using a full wireless stack may need to instantiate the structure.

Examples of results when secure boot is not enforced:

  • App has no signature: Valid if initial stack pointer and program counter have reasonable values

  • App has CRC checksum: Valid if checksum is valid

  • App has ECDSA signature: Valid if ECDSA signature is valid.

When secure boot is enforced, only ECDSA-signed applications with a valid signature are considered valid.

Returns

  • True if the image is deemed valid


bootload_bootloaderCallback#

void bootload_bootloaderCallback (uint32_t offset, uint8_t data, size_t length, void * context)

Bootloader upgrade callback implementation.

Parameters
TypeDirectionArgument NameDescription
uint32_tN/Aoffset

Offset of bootloader data (byte counter incrementing from 0)

uint8_tN/Adata

Raw bootloader data

size_tN/Alength

Size in bytes of raw bootloader data.

void *N/Acontext

A context variable defined by the implementation that is implementing this callback.


bootload_applicationCallback#

void bootload_applicationCallback (uint32_t address, uint8_t data, size_t length, void * context)

Image data callback implementation.

Parameters
TypeDirectionArgument NameDescription
uint32_tN/Aaddress

Address (inside the raw image) the data starts at

uint8_tN/Adata

Raw image data

size_tN/Alength

Size in bytes of raw image data. Always constrained to a multiple of four.

void *N/Acontext

A context variable defined by the implementation that is implementing this callback.


bootload_commitBootloaderUpgrade#

bool bootload_commitBootloaderUpgrade (uint32_t upgradeAddress, uint32_t size)

Perform a bootloader upgrade using the upgrade image present at upgradeAddress with length size.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]upgradeAddress

The starting address of the upgrade image

uint32_t[in]size

The length of the upgrade image in bytes

If the bootloader upgrade process starts successfully, this function does not return and execution will resume from the reset handler of the upgraded bootloader.

Returns

  • False if the bootloader upgrade process didn't start


bootload_verifyApplicationVersion#

bool bootload_verifyApplicationVersion (uint32_t appVersion, bool checkRemainingAppUpgrades)

Verify the application version for rollback protection.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]appVersion

Application version to be checked.

bool[in]checkRemainingAppUpgrades

Check remaining application upgrades.

Returns

  • True if the application version is higher or equal than the application versions seen. False if the application version is lower than the application versions seen. False if no remaining application upgrades are left when checkRemainingAppUpgrades is true.


bootload_storeApplicationVersion#

bool bootload_storeApplicationVersion (uint32_t startAddress)

Store the application version.

Parameters
TypeDirectionArgument NameDescription
uint32_tN/AstartAddress

Start address of application.

Note

  • Only the version of the verified application should be stored.

Returns

  • True if application version is successfully stored.


bootload_remainingApplicationUpgrades#

uint32_t bootload_remainingApplicationUpgrades (void )

Count the total remaining number of application upgrades.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • remaining number of application upgrades.


bootload_storeApplicationVersionResetMagic#

void bootload_storeApplicationVersionResetMagic (void )

Store application version reset magic.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • Store application version reset magic to ensure that application versions are cleaned after a bootloader upgrade.


bootload_removeStoredApplicationVersions#

void bootload_removeStoredApplicationVersions (void )

Clean the application versions seen.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • The application versions are cleaned only if this is requested with a magic and the application version storage is not already empty.


bootload_getApplicationVersionStorageCapacity#

uint32_t bootload_getApplicationVersionStorageCapacity (void )

Get the application version storage capacity.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Application version storage capacity.


bootload_getApplicationVersionStoragePtr#

uint32_t * bootload_getApplicationVersionStoragePtr (uint32_t index)

Get the address of the application version storage buffer.

Parameters
TypeDirectionArgument NameDescription
uint32_tN/Aindex

Index of the application version storage buffer.

Returns

  • Address of the application version storage buffer with the given index.


bootload_gotCertificate#

bool bootload_gotCertificate (const void * appProp)

Check whether the application contains a certificate.

Parameters
TypeDirectionArgument NameDescription
const void *N/AappProp

Pointer to ApplicationProperties_t of application.

Returns

  • True if application contains a certificate.


bootload_verifyCertificate#

bool bootload_verifyCertificate (const void * cert)

Verify a certificate with a bootloader certificate.

Parameters
TypeDirectionArgument NameDescription
const void *N/Acert

Pointer to ApplicationCertificate_t.

Returns

  • True if certificate is verified.


bootload_verifyApplicationCertificate#

bool bootload_verifyApplicationCertificate (const void * appProp, const void * gotCert)

Verify the application certificate.

Parameters
TypeDirectionArgument NameDescription
const void *N/AappProp

Pointer to ApplicationProperties_t of application.

const void *N/AgotCert

Boolean to store application certificate presence.

Note

  • This function will always return true if certificate support is not enabled. Also true if appProp does not contain any certificate and direct signed applications can be accepted.

Returns

  • True if application certificate is verified.