Custom GBL Tags
Handle custom GBL tags for added functionality in the GBL parser.
Modules#
Functions#
bool
gbl_isCustomTag(const GblTagHeader_t *tagHeader)
Indicate whether the GBL tag described by tagHeader is a custom tag.
const GblCustomTag_t *
gbl_getCustomTagProperties(uint32_t tagId)
Get properties for a custom GBL tag.
Function Documentation#
gbl_isCustomTag#
bool gbl_isCustomTag (const GblTagHeader_t * tagHeader)
Indicate whether the GBL tag described by tagHeader is a custom tag.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const GblTagHeader_t * | N/A | tagHeader | Pointer to the GBL tag header |
Returns
True if the tag is a custom tag, else false
gbl_getCustomTagProperties#
const GblCustomTag_t * gbl_getCustomTagProperties (uint32_t tagId)
Get properties for a custom GBL tag.
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | tagId | GBL Tag ID of the custom tag |
Returns
Pointer to the custom tag descriptor