You are viewing documentation for version:
PDFGBL version dependency tag type.
Public Attributes#
uint8_t
Type of image (application, bootloader, SE)
uint8_t
Encoded dependency statement (ex. appVersion > (0).1.2.3)
uint32_t
The version number used in the statement (ex. (0).1.2.3)
Public Attribute Documentation#
imageType#
uint8_t VersionDependency_t::imageType
Type of image (application, bootloader, SE)
statement#
uint8_t VersionDependency_t::statement
Encoded dependency statement (ex. appVersion > (0).1.2.3)
reserved#
uint16_t VersionDependency_t::reserved
Reserved.
version#
uint32_t VersionDependency_t::version
The version number used in the statement (ex. (0).1.2.3)