SMP Two-Page Switch Record#
Bootloader support for selecting application 1 or 2 from a two-page switch record (no NVM3).
Application-side flash helpers for the SMP switch pages.
Requires BTL_SMP_SUPPORT and the address symbols in btl_smp_cfg.h: switch page bases, app 2 base, optional default app id. App 1 base defaults to BTL_APPLICATION_BASE.
Modules#
Functions#
Erase one switch page.
Write a full switch record to one page.
Get SMP switch metadata page base addresses from the bootloader storage vtable.
Request that the next boot runs the given application.
Macros#
Magic value identifying a valid switch record ("SMPP" in ASCII).
Record format version.
Application ID: app 1 (first application region).
Application ID: app 2 (second application region).
Minimum valid app_id (inclusive).
Maximum valid app_id (inclusive). Extend if more apps are added.
Byte length of (magic, seq, app_id, version) used as input to btl_crc32Stream.
Function Documentation#
btl_smp_switch_erase_page#
bool btl_smp_switch_erase_page (bool use_page_1)
Erase one switch page.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | use_page_1 | true = Page 1, false = Page 2. |
The application must not erase the page that holds the current valid record until after the new record is written to the other page.
Returns
Returns true on MSC success, false on MSC error.
btl_smp_switch_write_record#
bool btl_smp_switch_write_record (bool use_page_1, uint16_t seq, uint8_t app_id)
Write a full switch record to one page.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | use_page_1 | true = write to Page 1, false = Page 2. |
| uint16_t | [in] | seq | Sequence value for the record. |
| uint8_t | [in] | app_id | Target app ( |
Note
Non-validating fields are written first, then CRC, then magic last. The implementation sets magic, version (
BTL_SMP_RECORD_VERSION), and crc32; the caller suppliesseqandapp_id.
Returns
Returns true on MSC success, false on MSC error.
get_smp_page_bases_from_storage#
bool get_smp_page_bases_from_storage (uint32_t * page1Base, uint32_t * page2Base)
Get SMP switch metadata page base addresses from the bootloader storage vtable.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t * | [out] | page1Base | Page 1 base if non-NULL. |
| uint32_t * | [out] | page2Base | Page 2 base if non-NULL. |
Requires BOOTLOADER_CAPABILITY_SMP_SWITCH (via bootloader_getInfo()) and a non-NULL getSmpSwitchPageBases pointer in BootloaderStorageFunctions_t. The bootloader supplies bases from its layout; the app does not use btl_smp_cfg.h.
Returns
False if SMP is not supported, or the storage vtable does not expose page bases.
btl_smp_switch_request_next_boot_app#
bool btl_smp_switch_request_next_boot_app (uint8_t next_app_id)
Request that the next boot runs the given application.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | next_app_id | Desired app for next boot ( |
Reads both pages, selects the other page, erases it, and writes a new record (sequence incremented, app_id set). The application should trigger a software reset after success.
Returns
Returns true if the switch record was updated successfully. Returns false if BOOTLOADER_CAPABILITY_SMP_SWITCH is not set, or if read/validate or erase/write failed.
Note
When the next sequence wraps in
uint16_t(65535 + 1),next_seqis 0; both switch pages are erased andseqrestarts at 1 (epoch reset). The target metadata page for the new record stays the same as the non-epoch algorithm would have chosen. Which application boots is alwaysnext_app_id, not the page index.
Macro Definition Documentation#
BTL_SMP_RECORD_MAGIC#
#define BTL_SMP_RECORD_MAGICValue:
0x534D5050UL
Magic value identifying a valid switch record ("SMPP" in ASCII).
BTL_SMP_APP_ID_MIN#
#define BTL_SMP_APP_ID_MINValue:
BTL_SMP_APP_ID_1
Minimum valid app_id (inclusive).
BTL_SMP_APP_ID_MAX#
#define BTL_SMP_APP_ID_MAXValue:
BTL_SMP_APP_ID_2
Maximum valid app_id (inclusive). Extend if more apps are added.
BTL_SMP_RECORD_HEADER_CRC_LEN#
#define BTL_SMP_RECORD_HEADER_CRC_LENValue:
(sizeof(uint32_t) + sizeof(uint16_t) + sizeof(uint8_t) + sizeof(uint8_t))
Byte length of (magic, seq, app_id, version) used as input to btl_crc32Stream.