EepromKit Drivers
Macros | |
#define | EEPROM_DVK_ADDR 0xA0 |
Functions | |
int | EEPROM_Read (I2C_TypeDef *i2c, uint8_t addr, unsigned int offset, uint8_t *data, unsigned int len) |
Read data from EEPROM. | |
int | EEPROM_Write (I2C_TypeDef *i2c, uint8_t addr, unsigned int offset, uint8_t *data, unsigned int len) |
Write data to EEPROM. | |
Macro Definition Documentation
#define EEPROM_DVK_ADDR 0xA0 |
I2C device address for EEPROM on DK
Definition at line 40
of file eeprom.h
.
Function Documentation
int EEPROM_Read | ( | I2C_TypeDef * | i2c, |
uint8_t | addr, |
||
unsigned int | offset, |
||
uint8_t * | data, |
||
unsigned int | len |
||
) |
Read data from EEPROM.
- Parameters
-
[in] i2c
Pointer to I2C peripheral register block. [in] addr
I2C address for EEPROM, in 8 bit format, where LSB is reserved for R/W bit. [in] offset
Offset in EEPROM to start reading from. [out] data
Location to place read data, must be at least len
long.[in] len
Number of bytes to read.
- Returns
- Returns number of bytes read. Less than specified number of bytes is returned if reading beyond end of EEPROM. Negative value is returned is some sort of error occurred during read.
Definition at line 118
of file eeprom.c
.
References I2C_TransferSeq_TypeDef::addr, I2C_TransferSeq_TypeDef::buf, I2C_TransferSeq_TypeDef::data, EEPROM_DVK_LEN, I2C_TransferSeq_TypeDef::flags, I2C_FLAG_WRITE_READ, I2CSPM_Transfer(), i2cTransferDone, and I2C_TransferSeq_TypeDef::len.
int EEPROM_Write | ( | I2C_TypeDef * | i2c, |
uint8_t | addr, |
||
unsigned int | offset, |
||
uint8_t * | data, |
||
unsigned int | len |
||
) |
Write data to EEPROM.
- Parameters
-
[in] i2c
Pointer to I2C peripheral register block. [in] addr
I2C address for EEPROM, in 8 bit format, where LSB is reserved for R/W bit. [in] offset
Offset in EEPROM to start writing to. [out] data
Location holding data to write, must be at least len
long.[in] len
Number of bytes to write.
- Returns
- Returns number of bytes written. Less than specified number of bytes is returned if writing beyond end of EEPROM. Negative value is returned is some sort of error occurred during write.
Definition at line 179
of file eeprom.c
.
References I2C_TransferSeq_TypeDef::addr, I2C_TransferSeq_TypeDef::buf, I2C_TransferSeq_TypeDef::data, EEPROM_AckPoll(), EEPROM_DVK_LEN, EEPROM_DVK_PAGESIZE, I2C_TransferSeq_TypeDef::flags, I2C_FLAG_WRITE_WRITE, I2CSPM_Transfer(), i2cTransferDone, and I2C_TransferSeq_TypeDef::len.