SMU_PrivilegedAccess_TypeDef Struct ReferenceEMLIB > SMU

SMU peripheral privileged access enablers.

Definition at line 332 of file em_smu.h.

#include <em_smu.h>

Data Fields

bool privilegedACMP0: 1
 
bool privilegedACMP1: 1
 
bool privilegedADC0: 1
 
bool privilegedCMU: 1
 
bool privilegedCRYOTIMER: 1
 
bool privilegedCRYPTO0: 1
 
bool privilegedCRYPTO1: 1
 
bool privilegedCSEN: 1
 
bool privilegedEMU: 1
 
bool privilegedFPUEH: 1
 
bool privilegedGPCRC: 1
 
bool privilegedGPIO: 1
 
bool privilegedI2C0: 1
 
bool privilegedI2C1: 1
 
bool privilegedIDAC0: 1
 
bool privilegedLDMA: 1
 
bool privilegedLESENSE: 1
 
bool privilegedLETIMER0: 1
 
bool privilegedLEUART0: 1
 
bool privilegedMSC: 1
 
bool privilegedPCNT0: 1
 
bool privilegedPCNT1: 1
 
bool privilegedPCNT2: 1
 
bool privilegedPRS: 1
 
bool privilegedReserved0: 1
 
bool privilegedReserved1: 1
 
bool privilegedReserved2: 1
 
bool privilegedReserved3: 1
 
bool privilegedReserved4: 1
 
bool privilegedReserved5: 1
 
bool privilegedReserved6: 1
 
bool privilegedReserved7: 1
 
bool privilegedReserved8: 1
 
bool privilegedRMU: 1
 
bool privilegedRTCC: 1
 
bool privilegedSMU: 1
 
bool privilegedTIMER0: 1
 
bool privilegedTIMER1: 1
 
bool privilegedTRNG0: 1
 
bool privilegedUSART0: 1
 
bool privilegedUSART1: 1
 
bool privilegedUSART2: 1
 
bool privilegedUSART3: 1
 
bool privilegedVDAC0: 1
 
bool privilegedWDOG0: 1
 
bool privilegedWDOG1: 1
 
bool privilegedWTIMER0: 1
 
bool privilegedWTIMER1: 1
 

Field Documentation

bool SMU_PrivilegedAccess_TypeDef::privilegedACMP0

Privileged access enabler for ACMP0.

Definition at line 334 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedACMP1

Privileged access enabler for ACMP1.

Definition at line 335 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedADC0

Privileged access enabler for ADC0.

Definition at line 336 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedCMU

Privileged access enabler for CMU.

Definition at line 339 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedCRYOTIMER

Privileged access enabler for CRYOTIMER.

Definition at line 341 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedCRYPTO0

Privileged access enabler for CRYPTO0.

Definition at line 342 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedCRYPTO1

Privileged access enabler for CRYPTO1.

Definition at line 343 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedCSEN

Privileged access enabler for CSEN.

Definition at line 344 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedEMU

Privileged access enabler for EMU.

Definition at line 347 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedFPUEH

Privileged access enabler for FPUEH.

Definition at line 348 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedGPCRC

Privileged access enabler for GPCRC.

Definition at line 350 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedGPIO

Privileged access enabler for GPIO.

Definition at line 351 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedI2C0

Privileged access enabler for I2C0.

Definition at line 352 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedI2C1

Privileged access enabler for I2C1.

Definition at line 353 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedIDAC0

Privileged access enabler for IDAC0.

Definition at line 354 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedLDMA

Privileged access enabler for LDMA.

Definition at line 356 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedLESENSE

Privileged access enabler for LESENSE.

Definition at line 357 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedLETIMER0

Privileged access enabler for LETIMER0.

Definition at line 358 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedLEUART0

Privileged access enabler for LEUART0.

Definition at line 359 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedMSC

Privileged access enabler for MSC.

Definition at line 355 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedPCNT0

Privileged access enabler for PCNT0.

Definition at line 361 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedPCNT1

Privileged access enabler for PCNT1.

Definition at line 362 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedPCNT2

Privileged access enabler for PCNT2.

Definition at line 363 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedPRS

Privileged access enabler for PRS.

Definition at line 346 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved0

Reserved privileged access enabler.

Definition at line 337 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved1

Reserved privileged access enabler.

Definition at line 338 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved2

Reserved privileged access enabler.

Definition at line 340 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved3

Reserved privileged access enabler.

Definition at line 349 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved4

Reserved privileged access enabler.

Definition at line 360 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved5

Reserved privileged access enabler.

Definition at line 364 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved6

Reserved privileged access enabler.

Definition at line 365 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved7

Reserved privileged access enabler.

Definition at line 366 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedReserved8

Reserved privileged access enabler.

Definition at line 370 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedRMU

Privileged access enabler for RMU.

Definition at line 367 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedRTCC

Privileged access enabler for RTCC.

Definition at line 368 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedSMU

Privileged access enabler for SMU.

Definition at line 369 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedTIMER0

Privileged access enabler for TIMER0.

Definition at line 371 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedTIMER1

Privileged access enabler for TIMER1.

Definition at line 372 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedTRNG0

Privileged access enabler for TRNG0.

Definition at line 373 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedUSART0

Privileged access enabler for USART0.

Definition at line 374 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedUSART1

Privileged access enabler for USART1.

Definition at line 375 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedUSART2

Privileged access enabler for USART2.

Definition at line 376 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedUSART3

Privileged access enabler for USART3.

Definition at line 377 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedVDAC0

Privileged access enabler for VDAC0.

Definition at line 345 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedWDOG0

Privileged access enabler for WDOG0.

Definition at line 378 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedWDOG1

Privileged access enabler for WDOG1.

Definition at line 379 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedWTIMER0

Privileged access enabler for WTIMER0.

Definition at line 380 of file em_smu.h.

bool SMU_PrivilegedAccess_TypeDef::privilegedWTIMER1

Privileged access enabler for WTIMER1.

Definition at line 381 of file em_smu.h.


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/em_smu.h