LESENSE_ST_TypeDef Struct ReferenceDevicesDevices > | LESENSE

LESENSE_ST LESENSE ST Register

.

Definition at line 47 of file efm32gg11b_lesense_st.h.

#include <efm32gg11b_lesense_st.h>

Data Fields

__IOM uint32_t TCONFA
 
__IOM uint32_t TCONFB
 

Field Documentation

__IOM uint32_t LESENSE_ST_TypeDef::TCONFA

State Transition Configuration a

Definition at line 48 of file efm32gg11b_lesense_st.h.

__IOM uint32_t LESENSE_ST_TypeDef::TCONFB

State Transition Configuration B

Definition at line 49 of file efm32gg11b_lesense_st.h.


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32GG11B/Include/efm32gg11b_lesense_st.h