EMUEMLIB
Detailed Description
Energy Management Unit (EMU) Peripheral API.
This module contains functions to control the EMU peripheral of Silicon Labs 32-bit MCUs and SoCs. The EMU handles the different low energy modes in Silicon Labs microcontrollers.
Data Structures |
|
| struct | EMU_DCDCInit_TypeDef |
| struct | EMU_EM01Init_TypeDef |
| struct | EMU_EM23Init_TypeDef |
| struct | EMU_EM4Init_TypeDef |
| struct | EMU_VmonHystInit_TypeDef |
| struct | EMU_VmonInit_TypeDef |
Macros |
|
| #define | EMU_DCDCINIT_DEFAULT |
| #define | EMU_EM01INIT_DEFAULT |
| #define | EMU_EM23INIT_DEFAULT |
| #define | EMU_EM4INIT_DEFAULT |
| #define | EMU_VMONHYSTINIT_DEFAULT |
| #define | EMU_VMONINIT_DEFAULT |
| #define | EMU_VSCALE_PRESENT |
| #define | emuDcdcLnFastTransient 160 |
| #define | emuDcdcLnHighEfficiency -1 |
| #define | PWRCFG_DCDCTODVDD_VMAX 3000U |
| #define | PWRCFG_DCDCTODVDD_VMIN 1800U |
Typedefs |
|
| typedef int16_t | EMU_DcdcLnReverseCurrentControl_TypeDef |
Enumerations |
|
| enum |
EMU_BODMode_TypeDef
{
emuBODMode_Active , emuBODMode_Inactive } |
| enum |
EMU_DcdcAnaPeripheralPower_TypeDef
{
emuDcdcAnaPeripheralPower_AVDD = EMU_PWRCTRL_ANASW_AVDD, emuDcdcAnaPeripheralPower_DCDC = EMU_PWRCTRL_ANASW_DVDD } |
| enum |
EMU_DcdcConductionMode_TypeDef
{
emuDcdcConductionMode_ContinuousLN , emuDcdcConductionMode_DiscontinuousLN } |
| enum |
EMU_DcdcLnCompCtrl_TypeDef
{
emuDcdcLnCompCtrl_1u0F , emuDcdcLnCompCtrl_4u7F } |
| enum |
EMU_DcdcLnRcoBand_TypeDef
{
emuDcdcLnRcoBand_3MHz = 0, emuDcdcLnRcoBand_4MHz = 1, emuDcdcLnRcoBand_5MHz = 2, emuDcdcLnRcoBand_6MHz = 3, emuDcdcLnRcoBand_7MHz = 4, emuDcdcLnRcoBand_8MHz = 5, emuDcdcLnRcoBand_9MHz = 6, emuDcdcLnRcoBand_10MHz = 7 } |
| enum |
EMU_DcdcMode_TypeDef
{
emuDcdcMode_Bypass = EMU_DCDCCTRL_DCDCMODE_BYPASS, emuDcdcMode_LowNoise = EMU_DCDCCTRL_DCDCMODE_LOWNOISE, emuDcdcMode_LowPower = EMU_DCDCCTRL_DCDCMODE_LOWPOWER } |
| enum |
EMU_EM4PinRetention_TypeDef
{
emuPinRetentionDisable = EMU_EM4CTRL_EM4IORETMODE_DISABLE, emuPinRetentionEm4Exit = EMU_EM4CTRL_EM4IORETMODE_EM4EXIT, emuPinRetentionLatch = EMU_EM4CTRL_EM4IORETMODE_SWUNLATCH } |
| enum |
EMU_EM4State_TypeDef
{
emuEM4Shutoff = 0, emuEM4Hibernate = 1 } |
| enum |
EMU_PeripheralRetention_TypeDef
{
emuPeripheralRetention_LEUART0 = _EMU_EM23PERNORETAINCTRL_LEUART0DIS_MASK, emuPeripheralRetention_CSEN = _EMU_EM23PERNORETAINCTRL_CSENDIS_MASK, emuPeripheralRetention_LESENSE0 = _EMU_EM23PERNORETAINCTRL_LESENSE0DIS_MASK, emuPeripheralRetention_WDOG1 = _EMU_EM23PERNORETAINCTRL_WDOG1DIS_MASK, emuPeripheralRetention_WDOG0 = _EMU_EM23PERNORETAINCTRL_WDOG0DIS_MASK, emuPeripheralRetention_LETIMER0 = _EMU_EM23PERNORETAINCTRL_LETIMER0DIS_MASK, emuPeripheralRetention_ADC0 = _EMU_EM23PERNORETAINCTRL_ADC0DIS_MASK, emuPeripheralRetention_IDAC0 = _EMU_EM23PERNORETAINCTRL_IDAC0DIS_MASK, emuPeripheralRetention_VDAC0 = _EMU_EM23PERNORETAINCTRL_VDAC0DIS_MASK, emuPeripheralRetention_I2C1 = _EMU_EM23PERNORETAINCTRL_I2C1DIS_MASK, emuPeripheralRetention_I2C0 = _EMU_EM23PERNORETAINCTRL_I2C0DIS_MASK, emuPeripheralRetention_ACMP1 = _EMU_EM23PERNORETAINCTRL_ACMP1DIS_MASK, emuPeripheralRetention_ACMP0 = _EMU_EM23PERNORETAINCTRL_ACMP0DIS_MASK, emuPeripheralRetention_PCNT2 = _EMU_EM23PERNORETAINCTRL_PCNT2DIS_MASK, emuPeripheralRetention_PCNT1 = _EMU_EM23PERNORETAINCTRL_PCNT1DIS_MASK, emuPeripheralRetention_PCNT0 = _EMU_EM23PERNORETAINCTRL_PCNT0DIS_MASK, emuPeripheralRetention_D1 , emuPeripheralRetention_D2 , emuPeripheralRetention_ALL } |
| enum | EMU_PowerConfig_TypeDef { emuPowerConfig_DcdcToDvdd } |
| enum |
EMU_VmonChannel_TypeDef
{
emuVmonChannel_AVDD , emuVmonChannel_ALTAVDD , emuVmonChannel_DVDD , emuVmonChannel_IOVDD0 } |
| enum |
EMU_VScaleEM01_TypeDef
{
emuVScaleEM01_HighPerformance = _EMU_STATUS_VSCALE_VSCALE2, emuVScaleEM01_LowPower = _EMU_STATUS_VSCALE_VSCALE0 } |
| enum |
EMU_VScaleEM23_TypeDef
{
emuVScaleEM23_FastWakeup = _EMU_CTRL_EM23VSCALE_VSCALE2, emuVScaleEM23_LowPower = _EMU_CTRL_EM23VSCALE_VSCALE0 } |
| enum |
EMU_VScaleEM4H_TypeDef
{
emuVScaleEM4H_FastWakeup = _EMU_CTRL_EM4HVSCALE_VSCALE2, emuVScaleEM4H_LowPower = _EMU_CTRL_EM4HVSCALE_VSCALE0 } |
Functions |
|
| void | EMU_DCDCConductionModeSet ( EMU_DcdcConductionMode_TypeDef conductionMode, bool rcoDefaultSet) |
| bool | EMU_DCDCInit (const EMU_DCDCInit_TypeDef *dcdcInit) |
| void | EMU_DCDCLnRcoBandSet ( EMU_DcdcLnRcoBand_TypeDef band) |
| void | EMU_DCDCModeSet ( EMU_DcdcMode_TypeDef dcdcMode) |
| void | EMU_DCDCOptimizeSlice (uint32_t em0LoadCurrentmA) |
| bool | EMU_DCDCOutputVoltageSet (uint32_t mV, bool setLpVoltage, bool setLnVoltage) |
| bool | EMU_DCDCPowerOff (void) |
| void | EMU_EM01Init (const EMU_EM01Init_TypeDef *em01Init) |
|
Update the EMU module with Energy Mode 0 and 1 configuration.
|
|
| void | EMU_EM23Init (const EMU_EM23Init_TypeDef *em23Init) |
|
Update the EMU module with Energy Mode 2 and 3 configuration.
|
|
| void | EMU_EM23PostsleepHook (void) |
|
Energy mode 2/3 post-sleep hook function.
|
|
| void | EMU_EM23PresleepHook (void) |
|
Energy mode 2/3 pre-sleep hook function.
|
|
| __STATIC_INLINE void | EMU_EM2Block (void) |
|
Block entering EM2 or higher number energy modes.
|
|
| __STATIC_INLINE void | EMU_EM2UnBlock (void) |
|
Unblock entering EM2 or higher number energy modes.
|
|
| void | EMU_EM4Init (const EMU_EM4Init_TypeDef *em4Init) |
|
Update the EMU module with Energy Mode 4 configuration.
|
|
| __STATIC_INLINE void | EMU_EnterEM1 (void) |
|
Enter energy mode 1 (EM1).
|
|
| void | EMU_EnterEM2 (bool restore) |
|
Enter energy mode 2 (EM2).
|
|
| void | EMU_EnterEM3 (bool restore) |
|
Enter energy mode 3 (EM3).
|
|
| void | EMU_EnterEM4 (void) |
|
Enter energy mode 4 (EM4).
|
|
| void | EMU_EnterEM4H (void) |
|
Enter energy mode 4 hibernate (EM4H).
|
|
| void | EMU_EnterEM4S (void) |
|
Enter energy mode 4 shutoff (EM4S).
|
|
| __STATIC_INLINE void | EMU_IntClear (uint32_t flags) |
|
Clear one or more pending EMU interrupts.
|
|
| __STATIC_INLINE void | EMU_IntDisable (uint32_t flags) |
|
Disable one or more EMU interrupts.
|
|
| __STATIC_INLINE void | EMU_IntEnable (uint32_t flags) |
|
Enable one or more EMU interrupts.
|
|
| __STATIC_INLINE uint32_t | EMU_IntGet (void) |
|
Get pending EMU interrupt flags.
|
|
| __STATIC_INLINE uint32_t | EMU_IntGetEnabled (void) |
|
Get enabled and pending EMU interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
|
|
| __STATIC_INLINE void | EMU_IntSet (uint32_t flags) |
|
Set one or more pending EMU interrupts.
|
|
| __STATIC_INLINE void | EMU_Lock (void) |
|
Lock EMU registers in order to protect them against unintended modification.
|
|
| void | EMU_MemPwrDown (uint32_t blocks) |
|
Power down memory block.
|
|
| void | EMU_PeripheralRetention ( EMU_PeripheralRetention_TypeDef periMask, bool enable) |
|
Set EM2 3 peripheral retention control.
|
|
| __STATIC_INLINE void | EMU_PowerLock (void) |
|
Lock the EMU regulator control registers in order to protect against unintended modification.
|
|
| __STATIC_INLINE void | EMU_PowerUnlock (void) |
|
Unlock the EMU power control registers so that writing to locked registers again is possible.
|
|
| void | EMU_RamPowerDown (uint32_t start, uint32_t end) |
|
Power down RAM memory blocks.
|
|
| void | EMU_RamPowerUp (void) |
|
Power up all available RAM memory blocks.
|
|
| void | EMU_Restore (void) |
|
Restore CMU HF clock select state, oscillator enable, and voltage scaling (if available) after
EMU_EnterEM2()
or
EMU_EnterEM3()
are called with the restore parameter set to false. Calling this function is equivalent to calling
EMU_EnterEM2()
or
EMU_EnterEM3()
with the restore parameter set to true, but it allows the application to evaluate the wakeup reason before restoring state.
|
|
| void | EMU_Save (void) |
|
Save the CMU HF clock select state, oscillator enable, and voltage scaling (if available) before
EMU_EnterEM2()
or
EMU_EnterEM3()
are called with the restore parameter set to false. Calling this function is equivalent to calling
EMU_EnterEM2()
or
EMU_EnterEM3()
with the restore parameter set to true, but it allows the state to be saved without going to sleep. The state can be restored manually by calling
EMU_Restore()
.
|
|
| __STATIC_INLINE void | EMU_UnlatchPinRetention (void) |
|
When EM4 pin retention is set to emuPinRetentionLatch, then pins are retained through EM4 entry and wakeup. The pin state is released by calling this function. The feature allows peripherals or GPIO to be re-initialized after EM4 exit (reset), and when initialization is done, this function can release pins and return control to the peripherals or GPIO.
|
|
| __STATIC_INLINE void | EMU_Unlock (void) |
|
Unlock the EMU so that writing to locked registers again is possible.
|
|
| void | EMU_UpdateOscConfig (void) |
|
Update EMU module with CMU oscillator selection/enable status.
|
|
| bool | EMU_VmonChannelStatusGet ( EMU_VmonChannel_TypeDef channel) |
|
Get the status of a voltage monitor channel.
|
|
| void | EMU_VmonEnable ( EMU_VmonChannel_TypeDef channel, bool enable) |
|
Enable or disable a VMON channel.
|
|
| void | EMU_VmonHystInit (const EMU_VmonHystInit_TypeDef *vmonInit) |
|
Initialize a VMON channel with hysteresis (separate rise and fall triggers).
|
|
| void | EMU_VmonInit (const EMU_VmonInit_TypeDef *vmonInit) |
|
Initialize a VMON channel.
|
|
| __STATIC_INLINE bool | EMU_VmonStatusGet (void) |
|
Get the status of the voltage monitor (VMON).
|
|
| void | EMU_VScaleEM01 ( EMU_VScaleEM01_TypeDef voltage, bool wait) |
|
Force voltage scaling in EM0 and 1 to a specific voltage level.
|
|
| void | EMU_VScaleEM01ByClock (uint32_t clockFrequency, bool wait) |
|
Voltage scale in EM0 and 1 by clock frequency.
|
|
| __STATIC_INLINE EMU_VScaleEM01_TypeDef | EMU_VScaleGet (void) |
|
Get current voltage scaling level.
|
|
| __STATIC_INLINE void | EMU_VScaleWait (void) |
|
Wait for voltage scaling to complete.
|
|
Macro Definition Documentation
| #define EMU_DCDCINIT_DEFAULT |
Default DCDC initialization.
Definition at line
805
of file
em_emu.h
.
| #define EMU_EM01INIT_DEFAULT |
Default initialization of EM0 and 1 configuration.
Definition at line
571
of file
em_emu.h
.
Referenced by BSP_initEmu() .
| #define EMU_EM23INIT_DEFAULT |
Default initialization of EM2 and 3 configuration.
Definition at line
587
of file
em_emu.h
.
Referenced by BSP_initEmu() .
| #define EMU_EM4INIT_DEFAULT |
Default initialization of EM4 configuration (Series 1 with VSCALE).
Definition at line
636
of file
em_emu.h
.
Referenced by UTIL_shutdown() .
| #define EMU_VMONHYSTINIT_DEFAULT |
Default VMON Hysteresis initialization structure.
Definition at line
886
of file
em_emu.h
.
| #define EMU_VMONINIT_DEFAULT |
Default VMON initialization structure.
Definition at line
865
of file
em_emu.h
.
| #define emuDcdcLnFastTransient   160 |
Default reverse current for fast transient response mode (low noise).
Definition at line
257
of file
em_emu.h
.
| #define emuDcdcLnHighEfficiency   -1 |
High efficiency mode. EMU_DCDCZDETCTRL_ZDETILIMSEL is "don't care".
Definition at line
254
of file
em_emu.h
.
Typedef Documentation
| typedef int16_t EMU_DcdcLnReverseCurrentControl_TypeDef |
DCDC Forced CCM and reverse current limiter control. Positive values have unit mA.
Definition at line
251
of file
em_emu.h
.
Enumeration Type Documentation
| enum EMU_BODMode_TypeDef |
DCDC to DVDD mode analog peripheral power supply select.
Definition at line
241
of file
em_emu.h
.
DCDC conduction modes.
Definition at line
229
of file
em_emu.h
.
DCDC Low-noise RCO band select.
Definition at line
262
of file
em_emu.h
.
| enum EMU_DcdcMode_TypeDef |
| Enumerator | |
|---|---|
| emuPinRetentionDisable |
No Retention: Pads enter reset state when entering EM4. |
| emuPinRetentionEm4Exit |
Retention through EM4: Pads enter reset state when exiting EM4. |
| emuPinRetentionLatch |
Retention through EM4 and wakeup: call EMU_UnlatchPinRetention() to release pins from retention after EM4 wakeup. |
Definition at line
196
of file
em_emu.h
.
| enum EMU_EM4State_TypeDef |
Peripheral EM2 and 3 retention control.
Definition at line
439
of file
em_emu.h
.
VMON channels.
Definition at line
376
of file
em_emu.h
.
Supported EM0/1 Voltage Scaling Levels.
| Enumerator | |
|---|---|
| emuVScaleEM01_HighPerformance |
High-performance voltage level. HF clock can be set to any frequency. |
| emuVScaleEM01_LowPower |
Low-power optimized voltage level. HF clock must be limited to CMU_VSCALEEM01_LOWPOWER_VOLTAGE_CLOCK_MAX Hz at this voltage. EM0/1 voltage scaling is applied when core clock frequency is changed from CMU or when calling EMU_EM01Init() when HF clock is already below the limit. |
Definition at line
401
of file
em_emu.h
.
Supported EM2/3 Voltage Scaling Levels.
| Enumerator | |
|---|---|
| emuVScaleEM23_FastWakeup |
Fast-wakeup voltage level. |
| emuVScaleEM23_LowPower |
Low-power optimized voltage level. Using this voltage level in EM2 and 3 adds approximately 30 us to wakeup time if EM0 and 1 voltage must be scaled up to emuVScaleEM01_HighPerformance on EM2 or 3 exit. |
Definition at line
415
of file
em_emu.h
.
Supported EM4H Voltage Scaling Levels
| Enumerator | |
|---|---|
| emuVScaleEM4H_FastWakeup |
Fast-wakeup voltage level. |
| emuVScaleEM4H_LowPower |
Low-power optimized voltage level. Using this voltage level in EM4H adds approximately 30 us to wakeup time if EM0 and 1 voltage must be scaled up to emuVScaleEM01_HighPerformance on EM4H exit. |
Definition at line
427
of file
em_emu.h
.
Function Documentation
| void EMU_EM01Init | ( | const EMU_EM01Init_TypeDef * |
em01Init
|
) |
Update the EMU module with Energy Mode 0 and 1 configuration.
- Parameters
-
[in] em01InitEnergy Mode 0 and 1 configuration structure.
Definition at line
1298
of file
em_emu.c
.
References EMU_VScaleEM01ByClock() , and EMU_EM01Init_TypeDef::vScaleEM01LowPowerVoltageEnable .
Referenced by BSP_initEmu() .
| void EMU_EM23Init | ( | const EMU_EM23Init_TypeDef * |
em23Init
|
) |
Update the EMU module with Energy Mode 2 and 3 configuration.
- Parameters
-
[in] em23InitEnergy Mode 2 and 3 configuration structure.
Definition at line
1313
of file
em_emu.c
.
References EMU_EM23Init_TypeDef::em23VregFullEn , emuVScaleEM23_LowPower , and EMU_EM23Init_TypeDef::vScaleEM23Voltage .
Referenced by BSP_initEmu() .
| SL_WEAK void EMU_EM23PostsleepHook | ( | void |
|
) |
Energy mode 2/3 post-sleep hook function.
This function is called by EMU_EnterEM2() and EMU_EnterEM3() functions just after wakeup from the WFI instruction. The function implementation does not perform anything, but it is SL_WEAK so that it can be re- implemented in application code if actions are needed.
- Note
- The function is primarily meant to be used in systems with EFP circuitry. (EFP = Energy Friendly Pmic (PMIC = Power Management IC)). In such systems there is a need to drive certain signals to EFP pins to notify about energy mode transitions.
Definition at line
556
of file
em_emu.c
.
Referenced by EMU_EnterEM2() , and EMU_EnterEM3() .
| SL_WEAK void EMU_EM23PresleepHook | ( | void |
|
) |
Energy mode 2/3 pre-sleep hook function.
This function is called by EMU_EnterEM2() and EMU_EnterEM3() functions just prior to execution of the WFI instruction. The function implementation does not perform anything, but it is SL_WEAK so that it can be re- implemented in application code if actions are needed.
- Note
- The function is primarily meant to be used in systems with EFP circuitry. (EFP = Energy Friendly Pmic (PMIC = Power Management IC)). In such systems there is a need to drive certain signals to EFP pins to notify about energy mode transitions.
Definition at line
536
of file
em_emu.c
.
Referenced by EMU_EnterEM2() , and EMU_EnterEM3() .
| void EMU_EM4Init | ( | const EMU_EM4Init_TypeDef * |
em4Init
|
) |
Update the EMU module with Energy Mode 4 configuration.
- Parameters
-
[in] em4InitEnergy Mode 4 configuration structure.
Definition at line
1343
of file
em_emu.c
.
References EMU_EM4Init_TypeDef::em4State , emuEM4Hibernate , EMU_EM4Init_TypeDef::pinRetentionMode , EMU_EM4Init_TypeDef::retainLfrco , EMU_EM4Init_TypeDef::retainLfxo , EMU_EM4Init_TypeDef::retainUlfrco , and EMU_EM4Init_TypeDef::vScaleEM4HVoltage .
Referenced by UTIL_shutdown() .
| void EMU_EnterEM2 | ( | bool |
restore
|
) |
Enter energy mode 2 (EM2).
When entering EM2, high-frequency clocks are disabled, i.e., HFXO, HFRCO and AUXHFRCO (for AUXHFRCO, see exception note below). When re-entering EM0, HFRCO is re-enabled and the core will be clocked by the configured HFRCO band. This ensures a quick wakeup from EM2.
However, prior to entering EM2, the core may have been using another oscillator than HFRCO. The
restore
parameter gives the user the option to restore all HF oscillators according to state prior to entering EM2, as well as the clock used to clock the core. This restore procedure is handled by SW. However, since handled by SW, it will not be restored before completing the interrupt function(s) waking up the core!
- Note
- If restoring core clock to use the HFXO oscillator, which has been disabled during EM2 mode, this function will stall until the oscillator has stabilized. Stalling time can be reduced by adding interrupt support detecting stable oscillator, and an asynchronous switch to the original oscillator. See CMU documentation. Such a feature is however outside the scope of the implementation in this function.
- If ERRATA_FIX_EMU_E110_ENABLE is active, the core's SLEEPONEXIT feature can not be used.
- If HFXO is re-enabled by this function, and NOT used to clock the core, this function will not wait for HFXO to stabilize. This must be considered by the application if trying to use features relying on that oscillator upon return.
-
If a debugger is attached, the AUXHFRCO will not be disabled if enabled upon entering EM2. It will thus remain enabled when returning to EM0 regardless of the
restoreparameter.
-
If HFXO autostart and select is enabled by using
CMU_HFXOAutostartEnable()
, the starting and selecting of the core clocks will be identical to the user independently of the value of the
restoreparameter when waking up on the wakeup sources corresponding to the autostart and select setting.
- If voltage scaling is supported, the restore parameter is true and the EM0 voltage scaling level is set higher than the EM2 level, then the EM0 level is also restored.
Note that the hardware will automatically update the HFRCO frequency in the case where voltage scaling is used in EM2/EM3 and not in EM0/EM1. When the restore argument to this function is true then software will restore the original HFRCO frequency after EM2/EM3 wake up. If the restore argument is false then the HFRCO frequency is 19 MHz when coming out of EM2/EM3 and all wait states are at a safe value.
- Parameters
-
[in] restore- true - save and restore oscillators, clocks and voltage scaling, see function details.
- false - do not save and restore oscillators and clocks, see function details.
-
The
restoreoption should only be used if all clock control is done via the CMU API.
Definition at line
622
of file
em_emu.c
.
References CORE_CRITICAL_SECTION , EMU_EM23PostsleepHook() , EMU_EM23PresleepHook() , and SystemCoreClockUpdate() .
Referenced by CAPLESENSE_Sleep() , UTIL_sleep() , and UTIL_waitForEvent() .
| void EMU_EnterEM3 | ( | bool |
restore
|
) |
Enter energy mode 3 (EM3).
When entering EM3, the high-frequency clocks are disabled by hardware, i.e., HFXO, HFRCO, and AUXHFRCO (for AUXHFRCO, see exception note below). In addition, the low-frequency clocks, i.e., LFXO and LFRCO are disabled by software. When re-entering EM0, HFRCO is re-enabled and the core will be clocked by the configured HFRCO band. This ensures a quick wakeup from EM3.
However, prior to entering EM3, the core may have been using an oscillator other than HFRCO. The
restore
parameter gives the user the option to restore all HF/LF oscillators according to state prior to entering EM3, as well as the clock used to clock the core. This restore procedure is handled by software. However, since it is handled by software, it will not be restored before completing the interrupt function(s) waking up the core!
- Note
- If restoring core clock to use an oscillator other than HFRCO, this function will stall until the oscillator has stabilized. Stalling time can be reduced by adding interrupt support detecting stable oscillator, and an asynchronous switch to the original oscillator. See CMU documentation. This feature is, however, outside the scope of the implementation in this function.
- If ERRATA_FIX_EMU_E110_ENABLE is active, the core's SLEEPONEXIT feature can't be used.
- If HFXO/LFXO/LFRCO are re-enabled by this function, and NOT used to clock the core, this function will not wait for those oscillators to stabilize. This must be considered by the application if trying to use features relying on those oscillators upon return.
-
If a debugger is attached, the AUXHFRCO will not be disabled if enabled upon entering EM3. It will, therefore, remain enabled when returning to EM0 regardless of the
restoreparameter.
- If voltage scaling is supported, the restore parameter is true and the EM0 voltage scaling level is set higher than the EM3 level, then the EM0 level is also restored.
- Parameters
-
[in] restore- true - save and restore oscillators, clocks and voltage scaling, see function details.
- false - do not save and restore oscillators and clocks, see function details.
-
The
restoreoption should only be used if all clock control is done via the CMU API.
Definition at line
749
of file
em_emu.c
.
References CMU_Lock() , CMU_Unlock() , CORE_CRITICAL_SECTION , EMU_EM23PostsleepHook() , EMU_EM23PresleepHook() , and SystemCoreClockUpdate() .
| void EMU_EnterEM4 | ( | void |
|
) |
Enter energy mode 4 (EM4).
- Note
- Only a power on reset or external reset pin can wake the device from EM4.
Definition at line
875
of file
em_emu.c
.
References BUS_RegMaskedClear() , EMU_Unlock() , and emuDcdcMode_Bypass .
Referenced by EMU_EnterEM4H() , EMU_EnterEM4S() , and UTIL_shutdown() .
| void EMU_EnterEM4H | ( | void |
|
) |
Enter energy mode 4 hibernate (EM4H).
- Note
- Retention of clocks and GPIO in EM4 can be configured using EMU_EM4Init before calling this function.
Definition at line
975
of file
em_emu.c
.
References BUS_RegBitWrite() , and EMU_EnterEM4() .
| void EMU_EnterEM4S | ( | void |
|
) |
Enter energy mode 4 shutoff (EM4S).
- Note
- Retention of clocks and GPIO in EM4 can be configured using EMU_EM4Init before calling this function.
Definition at line
991
of file
em_emu.c
.
References BUS_RegBitWrite() , and EMU_EnterEM4() .
| __STATIC_INLINE void EMU_IntClear | ( | uint32_t |
flags
|
) |
Clear one or more pending EMU interrupts.
- Parameters
-
[in] flagsPending EMU interrupt sources to clear. Use one or more valid interrupt flags for the EMU module (EMU_IFC_nnn).
Definition at line
1069
of file
em_emu.h
.
Referenced by disableInterrupts() , and TEMPDRV_IRQHandler() .
| __STATIC_INLINE void EMU_IntDisable | ( | uint32_t |
flags
|
) |
Disable one or more EMU interrupts.
- Parameters
-
[in] flagsEMU interrupt sources to disable. Use one or more valid interrupt flags for the EMU module (EMU_IEN_nnn).
Definition at line
1086
of file
em_emu.h
.
Referenced by disableInterrupts() , and updateInterrupts() .
| __STATIC_INLINE void EMU_IntEnable | ( | uint32_t |
flags
|
) |
Enable one or more EMU interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using EMU_IntClear() prior to enabling the interrupt.
- Parameters
-
[in] flagsEMU interrupt sources to enable. Use one or more valid interrupt flags for the EMU module (EMU_IEN_nnn).
Definition at line
1108
of file
em_emu.h
.
Referenced by updateInterrupts() .
| __STATIC_INLINE uint32_t EMU_IntGet | ( | void |
|
) |
Get pending EMU interrupt flags.
- Note
- Event bits are not cleared by the use of this function.
- Returns
- EMU interrupt sources pending. Returns one or more valid interrupt flags for the EMU module (EMU_IF_nnn).
Definition at line
1128
of file
em_emu.h
.
| __STATIC_INLINE uint32_t EMU_IntGetEnabled | ( | void |
|
) |
Get enabled and pending EMU interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Note
- Interrupt flags are not cleared by the use of this function.
- Returns
-
Pending and enabled EMU interrupt sources Return value is the bitwise AND of
- the enabled interrupt sources in EMU_IEN and
- the pending interrupt flags EMU_IF.
Definition at line
1147
of file
em_emu.h
.
Referenced by TEMPDRV_IRQHandler() .
| __STATIC_INLINE void EMU_IntSet | ( | uint32_t |
flags
|
) |
Set one or more pending EMU interrupts.
- Parameters
-
[in] flagsEMU interrupt sources to set to pending. Use one or more valid interrupt flags for the EMU module (EMU_IFS_nnn).
Definition at line
1163
of file
em_emu.h
.
| __STATIC_INLINE void EMU_Lock | ( | void |
|
) |
Lock EMU registers in order to protect them against unintended modification.
- Note
- If locking EMU registers, they must be unlocked prior to using any EMU API functions modifying EMU registers, excluding interrupt control and regulator control if the architecture has a EMU_PWRCTRL register. An exception to this is the energy mode entering API (EMU_EnterEMn()), which can be used when the EMU registers are locked.
Definition at line
1223
of file
em_emu.h
.
Referenced by RMU_ResetCauseClear() .
| void EMU_MemPwrDown | ( | uint32_t |
blocks
|
) |
Power down memory block.
- Parameters
-
[in] blocksSpecifies a logical OR of bits indicating memory blocks to power down. Bit 0 selects block 1, bit 1 selects block 2, and so on. Memory block 0 cannot be disabled. See the reference manual for available memory blocks for a device.
- Note
- Only a POR reset can power up the specified memory block(s) after power down.
-
Deprecated: - This function is deprecated, use EMU_RamPowerDown() instead which maps a user provided memory range into RAM blocks to power down.
Definition at line
1017
of file
em_emu.c
.
| void EMU_PeripheralRetention | ( | EMU_PeripheralRetention_TypeDef |
periMask,
|
| bool |
enable
|
||
| ) |
Set EM2 3 peripheral retention control.
- Parameters
-
[in] periMaskA peripheral select mask. Use | operator to select multiple peripherals, for example emuPeripheralRetention_LEUART0 | emuPeripheralRetention_VDAC0. [in] enablePeripheral retention enable (true) or disable (false).
- Note
- Only peripheral retention disable is currently supported. Peripherals are enabled by default and can only be disabled.
Definition at line
1179
of file
em_emu.c
.
| void EMU_RamPowerDown | ( | uint32_t |
start,
|
| uint32_t |
end
|
||
| ) |
Power down RAM memory blocks.
This function will power down all the RAM blocks that are within a given range. The RAM block layout is different between device families, so this function can be used in a generic way to power down a RAM memory region which is known to be unused.
This function will only power down blocks which are completely enclosed by the memory range given by [start, end).
This is an example to power down all RAM blocks except the first one. The first RAM block is special in that it cannot be powered down by the hardware. The size of the first RAM block is device-specific. See the reference manual to find the RAM block sizes.
- Note
- Only a reset can power up the specified memory block(s) after power down on a series 0 device.
- Parameters
-
[in] startThe start address of the RAM region to power down. This address is inclusive. [in] endThe end address of the RAM region to power down. This address is exclusive. If this parameter is 0, all RAM blocks contained in the region from start to the upper RAM address will be powered down.
Definition at line
1063
of file
em_emu.c
.
| void EMU_RamPowerUp | ( | void |
|
) |
Power up all available RAM memory blocks.
This function will power up all the RAM blocks on a device, this means that the RAM blocks are retained in EM2/EM3. Note that this functionality is not supported on Series 0 devices. Only a reset will power up the RAM blocks on a series 0 device.
Definition at line
1144
of file
em_emu.c
.
| void EMU_UpdateOscConfig | ( | void |
|
) |
Update EMU module with CMU oscillator selection/enable status.
-
Deprecated: - Oscillator status is saved in EMU_EnterEM2() and EMU_EnterEM3() .
Definition at line
1194
of file
em_emu.c
.
| bool EMU_VmonChannelStatusGet | ( | EMU_VmonChannel_TypeDef |
channel
|
) |
Get the status of a voltage monitor channel.
- Parameters
-
[in] channelA VMON channel to get the status for.
- Returns
- A status of the selected VMON channel. True if the channel is triggered.
Definition at line
3047
of file
em_emu.c
.
References BUS_RegBitRead() .
| void EMU_VmonEnable | ( | EMU_VmonChannel_TypeDef |
channel,
|
| bool |
enable
|
||
| ) |
Enable or disable a VMON channel.
- Parameters
-
[in] channelA VMON channel to enable/disable. [in] enableIndicates whether to enable or disable.
Definition at line
2995
of file
em_emu.c
.
References BUS_RegBitWrite() .
| void EMU_VmonHystInit | ( | const EMU_VmonHystInit_TypeDef * |
vmonInit
|
) |
Initialize a VMON channel with hysteresis (separate rise and fall triggers).
Initialize a VMON channel which supports hysteresis. The AVDD channel is the only channel to support separate rise and fall triggers. The rise and fall thresholds will be converted to a register field value based on the calibration values from the DI page.
- Parameters
-
[in] vmonInitThe VMON hysteresis initialization structure.
Definition at line
2955
of file
em_emu.c
.
References EMU_VmonHystInit_TypeDef::channel , EMU_VmonHystInit_TypeDef::enable , EMU_VmonHystInit_TypeDef::fallThreshold , EMU_VmonHystInit_TypeDef::fallWakeup , EMU_VmonHystInit_TypeDef::riseThreshold , and EMU_VmonHystInit_TypeDef::riseWakeup .
| void EMU_VmonInit | ( | const EMU_VmonInit_TypeDef * |
vmonInit
|
) |
Initialize a VMON channel.
Initialize a VMON channel without hysteresis. If the channel supports separate rise and fall triggers, both thresholds will be set to the same value. The threshold will be converted to a register field value based on calibration values from the DI page.
- Parameters
-
[in] vmonInitThe VMON initialization structure.
Definition at line
2868
of file
em_emu.c
.
References EMU_VmonInit_TypeDef::channel , EMU_VmonInit_TypeDef::enable , EMU_VmonInit_TypeDef::fallWakeup , EMU_VmonInit_TypeDef::retDisable , EMU_VmonInit_TypeDef::riseWakeup , and EMU_VmonInit_TypeDef::threshold .
| __STATIC_INLINE bool EMU_VmonStatusGet | ( | void |
|
) |
Get the status of the voltage monitor (VMON).
- Returns
- Status of the VMON. True if all the enabled channels are ready, false if one or more of the enabled channels are not ready.
Definition at line
1054
of file
em_emu.h
.
References BUS_RegBitRead() .
| void EMU_VScaleEM01 | ( | EMU_VScaleEM01_TypeDef |
voltage,
|
| bool |
wait
|
||
| ) |
Force voltage scaling in EM0 and 1 to a specific voltage level.
- Parameters
-
[in] voltageTarget VSCALE voltage level. [in] waitWait for scaling to complete.
- Note
- This function is useful for upscaling before programming Flash from MSC and downscaling after programming is done. Flash programming is only supported at emuVScaleEM01_HighPerformance .
- This function ignores vScaleEM01LowPowerVoltageEnable set from EMU_EM01Init() .
Definition at line
1256
of file
em_emu.c
.
References EMU_VScaleGet() , EMU_VScaleWait() , emuVScaleEM01_HighPerformance , emuVScaleEM01_LowPower , and SystemHFClockGet() .
Referenced by EMU_VScaleEM01ByClock() .
| void EMU_VScaleEM01ByClock | ( | uint32_t |
clockFrequency,
|
| bool |
wait
|
||
| ) |
Voltage scale in EM0 and 1 by clock frequency.
- Parameters
-
[in] clockFrequencyUse CMSIS HF clock if 0 or override to custom clock. Providing a custom clock frequency is required if using a non-standard HFXO frequency. [in] waitWait for scaling to complete.
- Note
- This function is primarily needed by the CMU module.
Definition at line
1214
of file
em_emu.c
.
References EMU_VScaleEM01() , emuVScaleEM01_HighPerformance , emuVScaleEM01_LowPower , SystemHFClockGet() , and EMU_EM01Init_TypeDef::vScaleEM01LowPowerVoltageEnable .
Referenced by CMU_ClockSelectSet() , CMU_DPLLLock() , CMU_HFRCOBandSet() , CMU_HFXOAutostartEnable() , and EMU_EM01Init() .
| __STATIC_INLINE EMU_VScaleEM01_TypeDef EMU_VScaleGet | ( | void |
|
) |
Get current voltage scaling level.
- Returns
- Current voltage scaling level.
Definition at line
1036
of file
em_emu.h
.
References EMU_VScaleWait() .
Referenced by CMU_DPLLLock() , and EMU_VScaleEM01() .