__BMP_DataType Struct ReferencePlatform Middleware > GLIB
BMP Data type structure to hold information about the bmp data returned.
Definition at line
142
of file
bmp.h
.
#include <
bmp.h
>
Data Fields |
|
uint16_t | bitsPerPixel |
uint32_t | compressionType |
uint32_t | endOfRow |
uint32_t | size |
Field Documentation
uint16_t __BMP_DataType::bitsPerPixel |
Color depth of the data returned from function.
Definition at line
144
of file
bmp.h
.
Referenced by BMP_readRawData() , BMP_readRawData24bit() , BMP_readRawData8bit() , and BMP_readRawDataRLE8() .
uint32_t __BMP_DataType::compressionType |
Compression type
Definition at line
146
of file
bmp.h
.
Referenced by BMP_readRawData() , BMP_readRawData24bit() , BMP_readRawData8bit() , and BMP_readRawDataRLE8() .
uint32_t __BMP_DataType::endOfRow |
Marks whether this data is at the end of the current row. endOfRow == 1, if end of row is reached. endOfRow == 0, if there is still unread data left in the row
Definition at line
150
of file
bmp.h
.
Referenced by BMP_readRawData() , BMP_readRawData24bit() , BMP_readRawData8bit() , BMP_readRawDataRLE8() , BMP_readRgbData() , BMP_readRgbDataRLE8() , and BMP_readRleData() .
uint32_t __BMP_DataType::size |
Byte length of returned data
Definition at line
148
of file
bmp.h
.
Referenced by BMP_readRawData() , BMP_readRawData24bit() , BMP_readRawData8bit() , BMP_readRawDataRLE8() , and BMP_readRgbData() .
The documentation for this struct was generated from the following file:
-
C:/cygwin/home/caamunds/work/super/platform/middleware/glib/glib/
bmp.h