__GLIB_Font_t Struct ReferencePlatform Middleware > GLIB
Font definition structure.
       Definition at line
       
        223
       
       of file
       
        glib.h
       
       .
      
      
       #include <
       
     
        glib.h
       
       >
      
         Data Fields | 
       |
| uint8_t | charSpacing | 
| GLIB_Font_Class | class | 
| uint16_t | cntOfMapElements | 
| uint8_t | fontHeight | 
| uint8_t | fontRowOffset | 
| uint8_t | fontWidth | 
| uint8_t | lineSpacing | 
| void * | pFontPixMap | 
| uint8_t | sizeOfMapElement | 
Field Documentation
| uint8_t __GLIB_Font_t::charSpacing | 
Number of pixels between each character in this font.
        Definition at line
        
         246
        
        of file
        
         glib.h
        
        .
       
Referenced by GLIB_drawChar() , and GLIB_drawString() .
| GLIB_Font_Class __GLIB_Font_t::class | 
The font class is used to tell glib if the font contains numbers only or characters and numbers
        Definition at line
        
         250
        
        of file
        
         glib.h
        
        .
       
Referenced by GLIB_drawChar() , and GLIB_drawString() .
| uint16_t __GLIB_Font_t::cntOfMapElements | 
Number of elements in the font pixel map.
        Definition at line
        
         228
        
        of file
        
         glib.h
        
        .
       
Referenced by GLIB_drawChar() .
| uint8_t __GLIB_Font_t::fontHeight | 
Height in pixels of each character.
        Definition at line
        
         240
        
        of file
        
         glib.h
        
        .
       
Referenced by GLIB_drawChar() , and GLIB_drawString() .
| uint8_t __GLIB_Font_t::fontRowOffset | 
| uint8_t __GLIB_Font_t::fontWidth | 
Width in pixels of each character.
        Definition at line
        
         237
        
        of file
        
         glib.h
        
        .
       
Referenced by GLIB_drawChar() , and GLIB_drawString() .
| uint8_t __GLIB_Font_t::lineSpacing | 
Number of pixels between each line in this font.
        Definition at line
        
         243
        
        of file
        
         glib.h
        
        .
       
Referenced by GLIB_drawString() .
| void* __GLIB_Font_t::pFontPixMap | 
Pointer to the pixel map for the font.
        Definition at line
        
         225
        
        of file
        
         glib.h
        
        .
       
Referenced by GLIB_drawChar() .
| uint8_t __GLIB_Font_t::sizeOfMapElement | 
Size of each element in the font pixel map.
        Definition at line
        
         231
        
        of file
        
         glib.h
        
        .
       
Referenced by GLIB_drawChar() .
The documentation for this struct was generated from the following file:
- 
       C:/cygwin/home/caamunds/work/super/platform/middleware/glib/glib/
       
glib.h