__BMP_DataType Struct ReferencePlatform Middleware > GLIB

BMP Data type structure to hold information about the bmp data returned.

Definition at line 142 of file bmp.h.

#include <bmp.h>

Data Fields

uint16_t bitsPerPixel
 
uint32_t compressionType
 
uint32_t endOfRow
 
uint32_t size
 

Field Documentation

uint16_t __BMP_DataType::bitsPerPixel

Color depth of the data returned from function.

Definition at line 144 of file bmp.h.

Referenced by BMP_readRawData(), BMP_readRawData24bit(), BMP_readRawData8bit(), and BMP_readRawDataRLE8().

uint32_t __BMP_DataType::compressionType

Compression type

Definition at line 146 of file bmp.h.

Referenced by BMP_readRawData(), BMP_readRawData24bit(), BMP_readRawData8bit(), and BMP_readRawDataRLE8().

uint32_t __BMP_DataType::endOfRow

Marks whether this data is at the end of the current row. endOfRow == 1, if end of row is reached. endOfRow == 0, if there is still unread data left in the row

Definition at line 150 of file bmp.h.

Referenced by BMP_readRawData(), BMP_readRawData24bit(), BMP_readRawData8bit(), BMP_readRawDataRLE8(), BMP_readRgbData(), BMP_readRgbDataRLE8(), and BMP_readRleData().

uint32_t __BMP_DataType::size

Byte length of returned data

Definition at line 148 of file bmp.h.

Referenced by BMP_readRawData(), BMP_readRawData24bit(), BMP_readRawData8bit(), BMP_readRawDataRLE8(), and BMP_readRgbData().


The documentation for this struct was generated from the following file:
  • C:/cygwin/home/caamunds/work/super/platform/middleware/glib/glib/bmp.h