RMU
Detailed Description
Reset Management Unit (RMU) Peripheral API.
This module contains functions to control the RMU peripheral of Silicon Labs 32-bit MCUs and SoCs. RMU ensures correct reset operation and is responsible for connecting the different reset sources to the reset lines of the MCU or SoC.
Macros | |
#define | RMU_LockupResetDisable(A) RMU_ResetControl(rmuResetLockUp, A) |
Enumerations | |
enum | RMU_Reset_TypeDef { rmuResetLockUp = _RMU_CTRL_LOCKUPRMODE_MASK, rmuResetWdog = _RMU_CTRL_WDOGRMODE_MASK, rmuResetCoreLockup = _RMU_CTRL_LOCKUPRMODE_MASK, rmuResetSys = _RMU_CTRL_SYSRMODE_MASK, rmuResetPin = _RMU_CTRL_PINRMODE_MASK } |
enum | RMU_ResetMode_TypeDef { rmuResetModeDisabled = _RMU_CTRL_PINRMODE_DISABLED, rmuResetModeLimited = _RMU_CTRL_PINRMODE_LIMITED, rmuResetModeExtended = _RMU_CTRL_PINRMODE_EXTENDED, rmuResetModeFull = _RMU_CTRL_PINRMODE_FULL } |
Functions | |
void | RMU_ResetCauseClear (void) |
Clear the reset cause register. | |
uint32_t | RMU_ResetCauseGet (void) |
Get the cause of the last reset. | |
void | RMU_ResetControl (RMU_Reset_TypeDef reset, RMU_ResetMode_TypeDef mode) |
Disable/enable reset for various peripherals and signal sources. | |
__STATIC_INLINE uint32_t | RMU_UserResetStateGet (void) |
Get user reset state. Reset only by a Power-on-reset and a pin reset. | |
__STATIC_INLINE void | RMU_UserResetStateSet (uint32_t userState) |
Set user reset state. Reset only by a Power-on-reset and a pin reset. | |
Macro Definition Documentation
#define RMU_LockupResetDisable | ( | A | ) | RMU_ResetControl(rmuResetLockUp, A) |
RMU_LockupResetDisable kept for backwards compatibility.
Definition at line 131
of file em_rmu.h
.
Enumeration Type Documentation
enum RMU_Reset_TypeDef |
RMU reset modes.
Definition at line 59
of file em_rmu.h
.
Function Documentation
void RMU_ResetCauseClear | ( | void |
| ) |
Clear the reset cause register.
This function clears all the reset cause bits of the RSTCAUSE register. The reset cause bits must be cleared by software before a new reset occurs. Otherwise, reset causes may accumulate. See RMU_ResetCauseGet().
Definition at line 273
of file em_rmu.c
.
References BUS_RegBitWrite(), EMU_Lock(), and EMU_Unlock().
Referenced by SLEEP_Init().
uint32_t RMU_ResetCauseGet | ( | void |
| ) |
Get the cause of the last reset.
To be useful, the reset cause must be cleared by software before a new reset occurs. Otherwise, reset causes may accumulate. See RMU_ResetCauseClear(). This function call will return the main cause for reset, which can be a bit mask (several causes) and clear away "noise".
- Returns
- A reset cause mask. See the reference manual for a description of the reset cause mask.
Definition at line 316
of file em_rmu.c
.
Referenced by SLEEP_Init().
void RMU_ResetControl | ( | RMU_Reset_TypeDef | reset, |
RMU_ResetMode_TypeDef | mode |
||
) |
Disable/enable reset for various peripherals and signal sources.
- Parameters
-
[in] reset
Reset types to enable/disable.s [in] mode
Reset mode.
Definition at line 245
of file em_rmu.c
.
References BUS_RegBitWrite(), and SL_CTZ().
__STATIC_INLINE uint32_t RMU_UserResetStateGet | ( | void |
| ) |
Get user reset state. Reset only by a Power-on-reset and a pin reset.
- Returns
- Reset surviving user state.
Definition at line 159
of file em_rmu.h
.
__STATIC_INLINE void RMU_UserResetStateSet | ( | uint32_t | userState | ) |
Set user reset state. Reset only by a Power-on-reset and a pin reset.
- Parameters
-
[in] userState
User state to set
Definition at line 144
of file em_rmu.h
.