ezradio_transmit_plugin.c File Reference
EzRadio transmit plug-in managed by the plug-in manager if enabled.
License
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
SPDX-License-Identifier: Zlib
The licensor of this software is Silicon Laboratories Inc.
This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.
Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:
- The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.
- Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.
- This notice may not be removed or altered from any source distribution.
       Definition in file
       
        ezradio_transmit_plugin.c
       
       .
      
       #include <stddef.h>
      
      
       #include <stdbool.h>
      
      
       #include "em_device.h"
      
      
       #include "ezradio_cmd.h"
      
      
       #include "ezradio_prop.h"
      
      
       #include "
       
        ezradio_api_lib.h
       
       "
      
      
       #include "ezradio_api_lib_add.h"
      
      
       #include "
       
        ezradio_plugin_manager.h
       
       "
      
      
       #include "
       
        ezradio_transmit_plugin.h
       
       "
      
      
| Functions | |
| Ecode_t | ezradioStartTransmitBasic ( EZRADIODRV_Handle_t radioHandle, uint16_t packetLength, uint8_t *pioRadioPacket) | 
| Start basic transmission. Radio transmits with data only in the first field in this case. | |
| Ecode_t | ezradioStartTransmitConfigured ( EZRADIODRV_Handle_t radioHandle, uint8_t *pioRadioPacket) | 
| Start transmission using the packet parameters from the generated configuration header file. | |
| Ecode_t | ezradioStartTransmitCustom ( EZRADIODRV_Handle_t radioHandle, EZRADIODRV_PacketLengthConfig_t pktLengthConf, uint8_t *pioRadioPacket) | 
| Start transmission using the packet parameters from pktLengthConf. | |
| Ecode_t | ezradioStartTransmitDefault ( EZRADIODRV_Handle_t radioHandle, uint8_t *pioRadioPacket) | 
| Start a default transmission using the packet information previously set to radioHandle. Depending on the information in the radioHandle parameter the function decides which transmission function has to be called. | |
| Ecode_t | ezradioStartTransmitSmart ( EZRADIODRV_Handle_t radioHandle, EZRADIODRV_PacketLengthConfig_t pktLengthConf, uint8_t *pioRadioPacket) | 
| Start a smart transmission. Depending on the information in the pktLengthConf parameter the function decides which transmission function has to be called. | |