glib_circle.c File Reference
Silicon Labs Graphics Library: Circle Drawing Routines.
License
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
The licensor of this software is Silicon Laboratories Inc. Your use of this software is governed by the terms of Silicon Labs Master Software License Agreement (MSLA) available at www.silabs.com/about-us/legal/master-software-license-agreement. This software is distributed to you in Source Code format and is governed by the sections of the MSLA applicable to Source Code.
Definition in file glib_circle.c
.
#include <stdint.h>
#include "em_types.h"
#include "glib.h
"
Functions | |
EMSTATUS | GLIB_drawCircle (GLIB_Context_t *pContext, int32_t xCenter, int32_t yCenter, uint32_t radius) |
Draws a circle with center at x, y, and a radius. | |
EMSTATUS | GLIB_drawCircleFilled (GLIB_Context_t *pContext, int32_t xCenter, int32_t yCenter, uint32_t radius) |
Draws a filled circle with center at x, y, and a radius. | |
EMSTATUS | GLIB_drawPartialCircle (GLIB_Context_t *pContext, int32_t xCenter, int32_t yCenter, uint32_t radius, uint8_t bitMask) |
Draws a partial circle with center at x, y, and a radius. | |
static EMSTATUS | GLIB_drawPartialCirclePoints (GLIB_Context_t *pContext, int32_t xCenter, int32_t yCenter, int32_t x, int32_t y, uint8_t bitMask) |
Draws circle points using 8-way symmetry. | |
Function Documentation
|
static |
Draws circle points using 8-way symmetry.
Example: bitMask = 4 draws only pixels in 3. octant (00000100). bitMask = 5 draws only pixels in 3. and 1. octant (00000101).
- Parameters
-
pContext
Pointer to a GLIB_Context_t in which the circle is drawn. The circle is drawn using the foreground color. xCenter
Center x-coordinate yCenter
Center y-coordinate x
x-coordinate of circle point y
y-coordinate of circle point bitMask
Bitmask which decides which octants pixels should be drawn The LSB is 1. octant, and the MSB is 8. octant. The octants are ordered from 1 to 8 in counterclockwise order.
- Returns
- Returns GLIB_OK on succes.
- Returns GLIB_ERROR_NOTHING_TO_DRAW if none of the points were drawn
- Returns error code otherwise
Definition at line 249
of file glib_circle.c
.
References GLIB_drawPixel(), GLIB_ERROR_NOTHING_TO_DRAW, and GLIB_OK.
Referenced by GLIB_drawPartialCircle().