SMU

Detailed Description

Security Management Unit (SMU) Peripheral API.

SMU forms the control and status/reporting component of bus-level security in EFM32/EFR32 devices.

Peripheral-level protection is provided via the peripheral protection unit (PPU). PPU provides hardware access barrier to any peripheral that is configured to be protected. When an attempt is made to access a peripheral without the required privilege/security level, PPU detects the fault and intercepts the access. No write or read of the peripheral register space occurs, and an all-zero value is returned if the access is a read.

// SMU is always clocked, so no call to CMU_ClockEnable() is necessary
// Initialize SMU to prevent access to CMU, EMU, SMU and GPIO
init.ppu.access.privilegedCMU = true;
init.ppu.access.privilegedEMU = true;
init.ppu.access.privilegedSMU = true;
init.ppu.access.privilegedGPIO = true;
SMU_Init(&init);

Data Structures

struct  SMU_Init_TypeDef
 
struct  SMU_PrivilegedAccess_TypeDef
 

Macros

#define SMU_INIT_DEFAULT
 

Enumerations

enum  SMU_Peripheral_TypeDef {
  smuPeripheralACMP0 = _SMU_PPUPATD0_ACMP0_SHIFT,
  smuPeripheralACMP1 = _SMU_PPUPATD0_ACMP1_SHIFT,
  smuPeripheralADC0 = _SMU_PPUPATD0_ADC0_SHIFT,
  smuPeripheralCMU = _SMU_PPUPATD0_CMU_SHIFT,
  smuPeripheralCRYOTIMER = _SMU_PPUPATD0_CRYOTIMER_SHIFT,
  smuPeripheralCRYPTO = _SMU_PPUPATD0_CRYPTO0_SHIFT,
  smuPeripheralVDAC0 = _SMU_PPUPATD0_VDAC0_SHIFT,
  smuPeripheralPRS = _SMU_PPUPATD0_PRS_SHIFT,
  smuPeripheralEMU = _SMU_PPUPATD0_EMU_SHIFT,
  smuPeripheralFPUEH = _SMU_PPUPATD0_FPUEH_SHIFT,
  smuPeripheralGPCRC = _SMU_PPUPATD0_GPCRC_SHIFT,
  smuPeripheralGPIO = _SMU_PPUPATD0_GPIO_SHIFT,
  smuPeripheralI2C0 = _SMU_PPUPATD0_I2C0_SHIFT,
  smuPeripheralIDAC0 = _SMU_PPUPATD0_IDAC0_SHIFT,
  smuPeripheralMSC = _SMU_PPUPATD0_MSC_SHIFT,
  smuPeripheralLDMA = _SMU_PPUPATD0_LDMA_SHIFT,
  smuPeripheralLESENSE = _SMU_PPUPATD0_LESENSE_SHIFT,
  smuPeripheralLETIMER0 = _SMU_PPUPATD0_LETIMER0_SHIFT,
  smuPeripheralLEUART = _SMU_PPUPATD0_LEUART0_SHIFT,
  smuPeripheralPCNT0 = _SMU_PPUPATD0_PCNT0_SHIFT,
  smuPeripheralRMU = _SMU_PPUPATD0_RMU_SHIFT,
  smuPeripheralRTCC = _SMU_PPUPATD0_RTCC_SHIFT,
  smuPeripheralSMU = _SMU_PPUPATD0_SMU_SHIFT,
  smuPeripheralTIMER0 = 32 + _SMU_PPUPATD1_TIMER0_SHIFT,
  smuPeripheralTIMER1 = 32 + _SMU_PPUPATD1_TIMER1_SHIFT,
  smuPeripheralTRNG0 = 32 + _SMU_PPUPATD1_TRNG0_SHIFT,
  smuPeripheralUSART0 = 32 + _SMU_PPUPATD1_USART0_SHIFT,
  smuPeripheralUSART1 = 32 + _SMU_PPUPATD1_USART1_SHIFT,
  smuPeripheralWDOG0 = 32 + _SMU_PPUPATD1_WDOG0_SHIFT,
  smuPeripheralWDOG1 = 32 + _SMU_PPUPATD1_WDOG1_SHIFT,
  smuPeripheralWTIMER0 = 32 + _SMU_PPUPATD1_WTIMER0_SHIFT,
  smuPeripheralEnd
}
 

Functions

__STATIC_INLINE void SMU_EnablePPU (bool enable)
 Enable or disable PPU of SMU.
 
__STATIC_INLINE SMU_Peripheral_TypeDef SMU_GetFaultingPeripheral (void)
 Get ID of the peripheral that caused an access fault.
 
__STATIC_INLINE void SMU_Init (const SMU_Init_TypeDef *init)
 Initialize PPU of SMU.
 
__STATIC_INLINE void SMU_IntClear (uint32_t flags)
 Clear one or more pending SMU interrupts.
 
__STATIC_INLINE void SMU_IntDisable (uint32_t flags)
 Disable one or more SMU interrupts.
 
__STATIC_INLINE void SMU_IntEnable (uint32_t flags)
 Enable one or more SMU interrupts.
 
__STATIC_INLINE uint32_t SMU_IntGet (void)
 Get pending SMU interrupts.
 
__STATIC_INLINE uint32_t SMU_IntGetEnabled (void)
 Get enabled and pending SMU interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
 
__STATIC_INLINE void SMU_IntSet (uint32_t flags)
 Set one or more pending SMU interrupts from SW.
 
__STATIC_INLINE void SMU_SetPrivilegedAccess (SMU_Peripheral_TypeDef peripheral, bool privileged)
 Change access settings for a peripheral.
 

Macro Definition Documentation

#define SMU_INIT_DEFAULT
Value:
{ \
{ { 0 } }, /* No peripherals access protected. */ \
true /* Enable SMU.*/ \
}

Default SMU initialization structure settings.

Definition at line 910 of file em_smu.h.

Enumeration Type Documentation

SMU peripheral identifiers.

Enumerator
smuPeripheralACMP0 

SMU peripheral identifier for ACMP0.

smuPeripheralACMP1 

SMU peripheral identifier for ACMP1.

smuPeripheralADC0 

SMU peripheral identifier for ADC0.

smuPeripheralCMU 

SMU peripheral identifier for CMU.

smuPeripheralCRYOTIMER 

SMU peripheral identifier for CRYOTIMER.

smuPeripheralCRYPTO 

SMU peripheral identifier for CRYPTO0.

smuPeripheralVDAC0 

SMU peripheral identifier for VDAC0.

smuPeripheralPRS 

SMU peripheral identifier for PRS.

smuPeripheralEMU 

SMU peripheral identifier for EMU.

smuPeripheralFPUEH 

SMU peripheral identifier for FPUEH.

smuPeripheralGPCRC 

SMU peripheral identifier for GPCRC.

smuPeripheralGPIO 

SMU peripheral identifier for GPIO.

smuPeripheralI2C0 

SMU peripheral identifier for I2C0.

smuPeripheralIDAC0 

SMU peripheral identifier for IDAC0.

smuPeripheralMSC 

SMU peripheral identifier for MSC.

smuPeripheralLDMA 

SMU peripheral identifier for LDMA.

smuPeripheralLESENSE 

SMU peripheral identifier for LESENSE.

smuPeripheralLETIMER0 

SMU peripheral identifier for LETIMER0.

smuPeripheralLEUART 

SMU peripheral identifier for LEUART0.

smuPeripheralPCNT0 

SMU peripheral identifier for PCNT0.

smuPeripheralRMU 

SMU peripheral identifier for RMU.

smuPeripheralRTCC 

SMU peripheral identifier for RTCC.

smuPeripheralSMU 

SMU peripheral identifier for SMU.

smuPeripheralTIMER0 

SMU peripheral identifier for TIMER0.

smuPeripheralTIMER1 

SMU peripheral identifier for TIMER1.

smuPeripheralTRNG0 

SMU peripheral identifier for TRNG0.

smuPeripheralUSART0 

SMU peripheral identifier for USART0.

smuPeripheralUSART1 

SMU peripheral identifier for USART1.

smuPeripheralWDOG0 

SMU peripheral identifier for WDOG0.

smuPeripheralWDOG1 

SMU peripheral identifier for WDOG1.

smuPeripheralWTIMER0 

SMU peripheral identifier for WTIMER0.

Definition at line 77 of file em_smu.h.

Function Documentation

__STATIC_INLINE void SMU_EnablePPU ( bool  enable)

Enable or disable PPU of SMU.

Parameters
[in]enableSet to true to enable PPU; set to false otherwise.

Definition at line 926 of file em_smu.h.

References BUS_RegBitWrite().

Referenced by SMU_Init().

__STATIC_INLINE SMU_Peripheral_TypeDef SMU_GetFaultingPeripheral ( void  )

Get ID of the peripheral that caused an access fault.

Note
The return value is only valid if SMU_IF_PPUPRIV interrupt flag is set.
Returns
ID of the peripheral that caused an access fault.

Definition at line 988 of file em_smu.h.

__STATIC_INLINE void SMU_Init ( const SMU_Init_TypeDef init)

Initialize PPU of SMU.

Parameters
[in]initPointer to initialization structure that defines which peripherals should only be accessed from privileged mode, and if PPU should be enabled.

Definition at line 943 of file em_smu.h.

References SMU_Init_TypeDef::enable, SMU_Init_TypeDef::reg, and SMU_EnablePPU().

__STATIC_INLINE void SMU_IntClear ( uint32_t  flags)

Clear one or more pending SMU interrupts.

Parameters
[in]flagsBitwise logic OR of SMU interrupt sources to clear.

Definition at line 1000 of file em_smu.h.

__STATIC_INLINE void SMU_IntDisable ( uint32_t  flags)

Disable one or more SMU interrupts.

Parameters
[in]flagsSMU interrupt sources to disable.

Definition at line 1016 of file em_smu.h.

__STATIC_INLINE void SMU_IntEnable ( uint32_t  flags)

Enable one or more SMU interrupts.

Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using SMU_IntClear() prior to enabling the interrupt.
Parameters
[in]flagsSMU interrupt sources to enable.

Definition at line 1037 of file em_smu.h.

__STATIC_INLINE uint32_t SMU_IntGet ( void  )

Get pending SMU interrupts.

Returns
SMU interrupt sources pending.

Definition at line 1053 of file em_smu.h.

__STATIC_INLINE uint32_t SMU_IntGetEnabled ( void  )

Get enabled and pending SMU interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.

Note
Interrupt flags are not cleared by this function.
Returns
Pending and enabled SMU interrupt sources. The return value is the bitwise AND combination of
  • the OR combination of enabled interrupt sources in SMU_IEN register and
  • the OR combination of valid interrupt flags in SMU_IF register.

Definition at line 1073 of file em_smu.h.

__STATIC_INLINE void SMU_IntSet ( uint32_t  flags)

Set one or more pending SMU interrupts from SW.

Parameters
[in]flagsSMU interrupt sources to set to pending.

Definition at line 1092 of file em_smu.h.

__STATIC_INLINE void SMU_SetPrivilegedAccess ( SMU_Peripheral_TypeDef  peripheral,
bool  privileged 
)

Change access settings for a peripheral.

Set to limit access of a peripheral from privileged mode.

Parameters
[in]peripheralID of the peripheral to change access settings for.
[in]privilegedSet to true if the peripheral should only be accessed from privileged mode; set to false otherwise.

Definition at line 965 of file em_smu.h.

References BUS_RegBitWrite().