RTC
Detailed Description
Real Time Counter (RTC) Peripheral API.
This module contains functions to control the RTC peripheral of Silicon Labs 32-bit MCUs and SoCs. The RTC ensures timekeeping in low energy modes.
Data Structures | |
struct | RTC_Init_TypeDef |
Macros | |
#define | NUM_RTC_CHANNELS 2U |
#define | RTC_INIT_DEFAULT |
Functions | |
uint32_t | RTC_CompareGet (unsigned int comp) |
Get the RTC compare register value. | |
void | RTC_CompareSet (unsigned int comp, uint32_t value) |
Set the RTC compare register value. | |
__STATIC_INLINE uint32_t | RTC_CounterGet (void) |
Get RTC counter value. | |
void | RTC_CounterReset (void) |
Restart the RTC counter from zero. | |
__STATIC_INLINE void | RTC_CounterSet (uint32_t value) |
Set the RTC counter value. | |
void | RTC_Enable (bool enable) |
Enable/disable RTC. | |
void | RTC_FreezeEnable (bool enable) |
RTC register synchronization freeze control. | |
void | RTC_Init (const RTC_Init_TypeDef *init) |
Initialize RTC. | |
__STATIC_INLINE void | RTC_IntClear (uint32_t flags) |
Clear one or more pending RTC interrupts. | |
__STATIC_INLINE void | RTC_IntDisable (uint32_t flags) |
Disable one or more RTC interrupts. | |
__STATIC_INLINE void | RTC_IntEnable (uint32_t flags) |
Enable one or more RTC interrupts. | |
__STATIC_INLINE uint32_t | RTC_IntGet (void) |
Get pending RTC interrupt flags. | |
__STATIC_INLINE uint32_t | RTC_IntGetEnabled (void) |
Get enabled and pending RTC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler. | |
__STATIC_INLINE void | RTC_IntSet (uint32_t flags) |
Set one or more pending RTC interrupts from SW. | |
void | RTC_Reset (void) |
Restore RTC to reset state. | |
Macro Definition Documentation
#define NUM_RTC_CHANNELS 2U |
The RTC peripheral on series 0 devices support 2 compare channels while the RTC peripheral on series 1 devices support 6 compare channels.
Definition at line 60
of file em_rtc.h
.
Referenced by RTC_Reset().
#define RTC_INIT_DEFAULT |
Suggested default configuration for RTC initialization structure.
Definition at line 77
of file em_rtc.h
.
Referenced by UDELAY_Calibrate().
Function Documentation
uint32_t RTC_CompareGet | ( | unsigned int | comp | ) |
Get the RTC compare register value.
- Parameters
-
[in] comp
A compare register to get. This value must be less than NUM_RTC_CHANNELS.
- Returns
- A compare register value, 0 if invalid register selected.
Definition at line 116
of file em_rtc.c
.
void RTC_CompareSet | ( | unsigned int | comp, |
uint32_t | value |
||
) |
Set the RTC compare register value.
- Note
- The setting of a compare register requires synchronization into the low-frequency domain. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the regSync() internal function call.
- Parameters
-
[in] comp
A compare register to set. This value must be less than NUM_RTC_CHANNELS. [in] value
An initialization value (<= 0x00ffffff).
Definition at line 162
of file em_rtc.c
.
Referenced by RTC_IRQHandler().
__STATIC_INLINE uint32_t RTC_CounterGet | ( | void |
| ) |
Get RTC counter value.
- Returns
- Current RTC counter value.
Definition at line 98
of file em_rtc.h
.
__STATIC_INLINE void RTC_CounterSet | ( | uint32_t | value | ) |
Set the RTC counter value.
- Parameters
-
[in] value
The new RTC counter value.
Definition at line 111
of file em_rtc.h
.
void RTC_Enable | ( | bool | enable | ) |
Enable/disable RTC.
- Note
- The enabling/disabling of RTC modifies the RTC CTRL register which requires synchronization into the low-frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the regSync() internal function call.
- Parameters
-
[in] enable
True to enable counting, false to disable.
Definition at line 225
of file em_rtc.c
.
References BUS_RegBitWrite().
Referenced by RTC_CounterReset(), RTCDRV_DeInit(), and UDELAY_Calibrate().
void RTC_FreezeEnable | ( | bool | enable | ) |
RTC register synchronization freeze control.
Some RTC registers require synchronization into the low-frequency (LF) domain. The freeze feature allows for several registers to be modified before passing them to the LF domain simultaneously (which takes place when the freeze mode is disabled).
- Note
- When enabling freeze mode, this function will wait for all current ongoing RTC synchronization to LF domain to complete (normally synchronization will not be in progress.) However, for this reason, when using freeze mode, modifications of registers requiring LF synchronization should be done within one freeze enable/disable block to avoid unnecessary stalling. This only applies to the Gecko Family. See the reference manual chapter about Access to Low Energy Peripherals (Asynchronos Registers) for details.
- Parameters
-
[in] enable
- True - enable freeze, modified registers are not propagated to the LF domain
- False - disables freeze, modified registers are propagated to LF domain
Definition at line 269
of file em_rtc.c
.
Referenced by UDELAY_Calibrate().
void RTC_Init | ( | const RTC_Init_TypeDef * | init | ) |
Initialize RTC.
Note that the compare values must be set separately with RTC_CompareSet() prior to the use of this function if configuring the RTC to start when initialization is completed.
- Note
- The initialization of the RTC modifies the RTC CTRL register which requires synchronization into the low-frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the regSync() internal function call.
- Parameters
-
[in] init
A pointer to the RTC initialization structure.
Definition at line 310
of file em_rtc.c
.
References RTC_Init_TypeDef::comp0Top, RTC_Init_TypeDef::debugRun, and RTC_Init_TypeDef::enable.
Referenced by RTCDRV_Init(), and UDELAY_Calibrate().
__STATIC_INLINE void RTC_IntClear | ( | uint32_t | flags | ) |
Clear one or more pending RTC interrupts.
- Parameters
-
[in] flags
RTC interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources for the RTC module (RTC_IFS_nnn).
Definition at line 133
of file em_rtc.h
.
Referenced by RTC_IRQHandler().
__STATIC_INLINE void RTC_IntDisable | ( | uint32_t | flags | ) |
Disable one or more RTC interrupts.
- Parameters
-
[in] flags
RTC interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt sources for the RTC module (RTC_IFS_nnn).
Definition at line 147
of file em_rtc.h
.
__STATIC_INLINE void RTC_IntEnable | ( | uint32_t | flags | ) |
Enable one or more RTC interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using RTC_IntClear() prior to enabling the interrupt.
- Parameters
-
[in] flags
RTC interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the RTC module (RTC_IFS_nnn).
Definition at line 166
of file em_rtc.h
.
__STATIC_INLINE uint32_t RTC_IntGet | ( | void |
| ) |
Get pending RTC interrupt flags.
- Note
- Event bits are not cleared by using this function.
- Returns
- Pending RTC interrupt sources. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the RTC module (RTC_IFS_nnn).
Definition at line 182
of file em_rtc.h
.
Referenced by RTC_IRQHandler().
__STATIC_INLINE uint32_t RTC_IntGetEnabled | ( | void |
| ) |
Get enabled and pending RTC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Note
- Interrupt flags are not cleared by using this function.
- Returns
- Pending and enabled RTC interrupt sources. The return value is the bitwise AND of
- the enabled interrupt sources in RTC_IEN and
- the pending interrupt flags RTC_IF.
Definition at line 201
of file em_rtc.h
.
__STATIC_INLINE void RTC_IntSet | ( | uint32_t | flags | ) |
Set one or more pending RTC interrupts from SW.
- Parameters
-
[in] flags
RTC interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the RTC module (RTC_IFS_nnn).
Definition at line 218
of file em_rtc.h
.