Note that PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... Device configuration and utilities (Utilities) ... Reset The device is reset. 7
Threading primitive implementation for mbed TLS. This file contains the glue logic between the mbed TLS threading API and two RTOS'es supported, being Micrium OS and FreeRTOS. ... Note
ProductMicrocontrollersResource TypeSoftware API documentation
// Gecko Platform//Version 4.4.1 //Services //API Documentation //Sleep Timer ... and sleeptimer.h source files for the SLEEPTIMER device driver library are in the service/sleeptimer folder.