Core control (LESENSE_CTRL) descriptor structure.
Definition at line 487
of file em_lesense.h
.
#include <
em_lesense.h
>
Field Documentation
LESENSE_BiasMode_TypeDef LESENSE_CoreCtrlDesc_TypeDef::biasMode |
bool LESENSE_CoreCtrlDesc_TypeDef::bufOverWr |
Set to true in order to always make LESENSE write to the result buffer, even if it is full.
Definition at line 512
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_BufTrigLevel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::bufTrigLevel |
Select trigger conditions for the interrupt and DMA.
Definition at line 515
of file em_lesense.h
.
Referenced by LESENSE_Init().
bool LESENSE_CoreCtrlDesc_TypeDef::debugRun |
Set to true to keep LESENSE running in the debug mode.
Definition at line 524
of file em_lesense.h
.
Referenced by LESENSE_Init().
bool LESENSE_CoreCtrlDesc_TypeDef::dualSample |
Set to true to sample both ACMPs simultaneously.
Definition at line 504
of file em_lesense.h
.
Referenced by LESENSE_Init().
bool LESENSE_CoreCtrlDesc_TypeDef::invACMP0 |
Set to true to invert ACMP0 output.
Definition at line 498
of file em_lesense.h
.
Referenced by LESENSE_Init().
bool LESENSE_CoreCtrlDesc_TypeDef::invACMP1 |
Set to true to invert ACMP1 output.
Definition at line 501
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_PRSSel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::prsSel |
Select PRS source for scan start if scanMode is set to lesensePrsPulse.
Definition at line 492
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_ScanConfSel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::scanConfSel |
Select scan configuration register usage strategy.
Definition at line 495
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_ScanMode_TypeDef LESENSE_CoreCtrlDesc_TypeDef::scanStart |
Select scan start mode to control how the scan start is being triggered.
Definition at line 489
of file em_lesense.h
.
Referenced by CAPLESENSE_setupLESENSE(), and LESENSE_Init().
bool LESENSE_CoreCtrlDesc_TypeDef::storeScanRes |
Set to true in order to store SCANRES in the RAM (accessible via RESDATA) after each scan.
Definition at line 508
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_DMAWakeUp_TypeDef LESENSE_CoreCtrlDesc_TypeDef::wakeupOnDMA |
Configure trigger condition for the DMA wakeup from EM2.
Definition at line 518
of file em_lesense.h
.
Referenced by LESENSE_Init().
The documentation for this struct was generated from the following file:
- C:/HandsOn/super/platform/emlib/inc/
em_lesense.h