MPU Region initialization structure.
       Definition at line
       
        122
       
       of file
       
        em_mpu.h
       
       .
      
      
       #include <
       
     
        em_mpu.h
       
       >
      
         Data Fields | 
       |
| MPU_RegionAp_TypeDef | accessPermission | 
| uint32_t | baseAddress | 
| bool | bufferable | 
| bool | cacheable | 
| bool | disableExec | 
| bool | regionEnable | 
| uint8_t | regionNo | 
| bool | shareable | 
| MPU_RegionSize_TypeDef | size | 
| uint8_t | srd | 
| uint8_t | tex | 
Field Documentation
| MPU_RegionAp_TypeDef MPU_RegionInit_TypeDef::accessPermission | 
Memory access permissions.
        Definition at line
        
         127
        
        of file
        
         em_mpu.h
        
        .
       
Referenced by MPU_ConfigureRegion() .
| uint32_t MPU_RegionInit_TypeDef::baseAddress | 
Region base address.
        Definition at line
        
         125
        
        of file
        
         em_mpu.h
        
        .
       
Referenced by MPU_ConfigureRegion() .
| bool MPU_RegionInit_TypeDef::bufferable | 
Memory attribute for buffering.
        Definition at line
        
         131
        
        of file
        
         em_mpu.h
        
        .
       
Referenced by MPU_ConfigureRegion() .
| bool MPU_RegionInit_TypeDef::cacheable | 
Memory attribute for caching.
        Definition at line
        
         130
        
        of file
        
         em_mpu.h
        
        .
       
Referenced by MPU_ConfigureRegion() .
| bool MPU_RegionInit_TypeDef::disableExec | 
| bool MPU_RegionInit_TypeDef::regionEnable | 
| uint8_t MPU_RegionInit_TypeDef::regionNo | 
| bool MPU_RegionInit_TypeDef::shareable | 
Memory attribute for sharing.
        Definition at line
        
         129
        
        of file
        
         em_mpu.h
        
        .
       
Referenced by MPU_ConfigureRegion() .
| MPU_RegionSize_TypeDef MPU_RegionInit_TypeDef::size | 
| uint8_t MPU_RegionInit_TypeDef::srd | 
Memory subregion disable bits.
        Definition at line
        
         132
        
        of file
        
         em_mpu.h
        
        .
       
Referenced by MPU_ConfigureRegion() .
| uint8_t MPU_RegionInit_TypeDef::tex | 
Memory type extension attributes.
        Definition at line
        
         133
        
        of file
        
         em_mpu.h
        
        .
       
Referenced by MPU_ConfigureRegion() .
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       
em_mpu.h