segmentlcd.c File Reference
Segment LCD Display driver.
License
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
SPDX-License-Identifier: Zlib
The licensor of this software is Silicon Laboratories Inc.
This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.
Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:
- The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.
- Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.
- This notice may not be removed or altered from any source distribution.
Definition in file segmentlcd.c
.
#include <stdio.h>
#include <string.h>
#include <stdlib.h>
#include <stdbool.h>
#include "em_device.h"
#include "em_cmu.h
"
#include "em_gpio.h
"
#include "segmentlcd.h
"
Data Structures | |
struct | ARING_TypeDef |
Defines segment COM and BIT fields for A-wheel (suited for Anim) | |
struct | ARRAY_TypeDef |
Defines segment COM and BIT fields for array. | |
struct | BATTERY_TypeDef |
Defines segment COM and BIT fields for Battery (suited for Anim) | |
struct | Block_TypeDef |
Defines segment COM and BIT fields for top and bottom row blocks. The bit pattern shown above for characters can be split into upper and lower portions for animation purposes. There are separate COM and BIT numbers which together represent a set of stacked blocks which can be shown on two rows in the segmented LCD screen. | |
struct | CHAR_TypeDef |
Defines each text symbol's segment in terms of COM and BIT numbers, in a way that we can enumerate each bit for each text segment in the following bit pattern: | |
struct | EM_TypeDef |
Defines segment COM and BIT fields for Energy Modes on display. | |
struct | MCU_DISPLAY |
Defines prototype for all segments in display. | |
struct | NUMBER_TypeDef |
Defines segment COM and BIT fields numeric display. | |
Macros | |
#define | ALPHA_DIGITS 7 |
#define | ALPHA_VAL_MAX 9999999 |
#define | ALPHA_VAL_MIN -9999999 |
#define | NUM_DIGITS 4 |
#define | NUM_VAL_MAX 9999 |
#define | NUM_VAL_MAX_HEX 0xFFFF |
#define | NUM_VAL_MIN -999 |
Functions | |
static void | displayBlock (SegmentLCD_BlockMode_TypeDef topMode[SEGMENT_LCD_NUM_BLOCK_COLUMNS], SegmentLCD_BlockMode_TypeDef botMode[SEGMENT_LCD_NUM_BLOCK_COLUMNS]) |
Working instance of LCD display. | |
void | SegmentLCD_AllOff (void) |
Disable all segments. | |
void | SegmentLCD_AllOn (void) |
Enable all segments. | |
void | SegmentLCD_AlphaNumberOff (void) |
Turn all segments on alpha characters in display off. | |
void | SegmentLCD_ARing (int anum, int on) |
Light up or shut off Ring of Indicators. | |
void | SegmentLCD_Battery (int batteryLevel) |
Light up or shut off Battery Indicator. | |
void | SegmentLCD_Block (SegmentLCD_BlockMode_TypeDef topMode[SEGMENT_LCD_NUM_BLOCK_COLUMNS], SegmentLCD_BlockMode_TypeDef botMode[SEGMENT_LCD_NUM_BLOCK_COLUMNS]) |
void | SegmentLCD_Disable (void) |
Disables LCD controller. | |
void | SegmentLCD_EnergyMode (int em, int on) |
Light up or shut off Energy Mode indicator. | |
void | SegmentLCD_Init (bool useBoost) |
Segment LCD Initialization routine for EFM32 STK display. | |
void | SegmentLCD_LowerHex (uint32_t num) |
Write a hexadecimal number on lower alphanumeric part of Segment LCD display. | |
void | SegmentLCD_LowerNumber (int num) |
Write number on lower alphanumeric part of Segment LCD display. | |
void | SegmentLCD_Number (int value) |
Write number on numeric part on Segment LCD display. | |
void | SegmentLCD_NumberOff (void) |
Turn all segments on numeric digits in display off. | |
unsigned int | SegmentLCD_segCnt (unsigned int segdl, unsigned int segdh) |
Counting the number of active segments in a single common line. | |
void | SegmentLCD_Symbol (lcdSymbol s, int on) |
Light up or shut off various symbols on Segment LCD. | |
void | SegmentLCD_UnsignedHex (uint32_t value) |
Write hexadecimal number on numeric part on Segment LCD display. | |
void | SegmentLCD_Write (const char *string) |
Write text on LCD display. | |
Variables | |
static const uint16_t | Blocks [] |
Defines highlighted segments for the block display. | |
static const MCU_DISPLAY | EFM_Display = EFM_DISPLAY_DEF |
Working instance of LCD display. | |
static const uint16_t | Segment_Alphabet [] |
Defines higlighted segments for the alphabet, starting from "blank" (SPACE) Uses bit pattern as defined for text segments above. E.g. a capital O, would have bits 0 1 2 3 4 5 => 0x003f defined. | |
static const uint16_t | Segment_Numbers [] |
Defines higlighted segments for the numeric display. | |