USB_StringDescriptor_TypeDef Struct Reference

USB String Descriptor.

Definition at line 504 of file em_usb.h.

#include <em_usb.h>

Data Fields

uint8_t len
 
char16_t name []
 
uint8_t type
 

Field Documentation

uint8_t USB_StringDescriptor_TypeDef::len

Size of this descriptor in bytes.

Definition at line 505 of file em_usb.h.

char16_t USB_StringDescriptor_TypeDef::name[]

The string encoded with UTF-16LE UNICODE charset.

Definition at line 507 of file em_usb.h.

uint8_t USB_StringDescriptor_TypeDef::type

Constant STRING Descriptor Type.

Definition at line 506 of file em_usb.h.


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/platform/middleware/usb_gecko/inc/em_usb.h