LETIMER_Init_TypeDef Struct Reference

LETIMER initialization structure.

Definition at line 91 of file em_letimer.h.

#include <em_letimer.h>

Data Fields

bool bufTop
 
bool comp0Top
 
bool debugRun
 
bool enable
 
uint8_t out0Pol
 
uint8_t out1Pol
 
LETIMER_RepeatMode_TypeDef repMode
 
uint32_t topValue
 
LETIMER_UFOA_TypeDef ufoa0
 
LETIMER_UFOA_TypeDef ufoa1
 

Field Documentation

bool LETIMER_Init_TypeDef::bufTop

Load COMP1 into COMP0 when REP0 reaches 0.

Definition at line 99 of file em_letimer.h.

Referenced by LETIMER_Init().

bool LETIMER_Init_TypeDef::comp0Top

Load COMP0 register into CNT when counter underflows.

Definition at line 98 of file em_letimer.h.

Referenced by LETIMER_Init(), and MIC_init().

bool LETIMER_Init_TypeDef::debugRun

Counter shall keep running during debug halt.

Definition at line 93 of file em_letimer.h.

Referenced by LETIMER_Init().

bool LETIMER_Init_TypeDef::enable

Start counting when initialization completes.

Definition at line 92 of file em_letimer.h.

Referenced by LETIMER_Init(), and MIC_init().

uint8_t LETIMER_Init_TypeDef::out0Pol

Idle value for output 0.

Definition at line 100 of file em_letimer.h.

Referenced by LETIMER_Init().

uint8_t LETIMER_Init_TypeDef::out1Pol

Idle value for output 1.

Definition at line 101 of file em_letimer.h.

Referenced by LETIMER_Init().

LETIMER_RepeatMode_TypeDef LETIMER_Init_TypeDef::repMode

Repeat mode.

Definition at line 104 of file em_letimer.h.

Referenced by LETIMER_Init().

uint32_t LETIMER_Init_TypeDef::topValue

Top value. Counter wraps when top value matches counter value is reached.

Definition at line 105 of file em_letimer.h.

Referenced by LETIMER_Init().

LETIMER_UFOA_TypeDef LETIMER_Init_TypeDef::ufoa0

Underflow output 0 action.

Definition at line 102 of file em_letimer.h.

Referenced by LETIMER_Init(), and MIC_init().

LETIMER_UFOA_TypeDef LETIMER_Init_TypeDef::ufoa1

Underflow output 1 action.

Definition at line 103 of file em_letimer.h.

Referenced by LETIMER_Init().


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/platform/emlib/inc/em_letimer.h