Wi-Fi Demos#
This section describes how to get started with Wi-fi development for iOS and Android smart phones, including:
Wi-Fi OTA firmware update demo, which demonstrates how to update the SiWx91x user application firmware over Wi-Fi connection by downloading the image from a mobile phone.
Wi-Fi 917 Sensor demo, which collects and processes sensor data from the SiWG917 dev kit board, transmits them over a Wi-Fi network, and displays them on the Simplicity Connect iOS/Android application. Learn more about the SiWG917 Dev Kit on the Silicon Labs Github site.
Wi-Fi Throughput demo, which indicates how much data can be transmitted over the Wi-Fi connection within a given time. This demo supports both upload and download operations for TCP, UDP and TLS.
Wi-Fi Provisioning demo, which showcases the provisioning of SiWx917 over Wi-Fi.
AWS IoT cloud demo, which displays the sensor data from the SiWx91x Dev Kit that features built-in sensors. In this demo, the SiWx91x Dev Kit and the mobile application connect to the same access point and then establish a secure connection to the AWS IoT. On successful connection, the application collects and processes sensor data and displays it on the mobile dashboard. Additionally, you can control the LED on the Dev Kit board by pressing a button on the mobile application.
The Smart Lock demo showcases how to control a smart lock using Bluetooth Low Energy (BLE) and Amazon Web Services (AWS). The SiWx91x Development Kit (Dev Kit) functions as the smart lock device. You can control the smart lock device locally via BLE or remotely via AWS.