Coexistence#

  • Zigbee and Thread Coexistence with Wi-Fi: Details the impact of Wi-Fi on Zigbee and Thread, and methods to improve coexistence. First, methods to improve coexistence without direct interaction between Zigbee/Thread and Wi-Fi radios are described. Second, Silicon Labs's Packet Traffic Arbitration (PTA) support to coordinate 2.5 GHz RF traffic for co-located Zigbee/Thread and Wi-Fi radios is described (for the EFR32MG only).

  • Bluetooth Coexistence with Wi-Fi (PDF): Describes the Wi-Fi impact on Bluetooth and methods to improve Bluetooth coexistence with Wi-Fi.Explains design considerations to improve coexistence without direct interaction between Bluetooth and Wi-Fi radios.These techniques are applicable to the EFR32MGx and EFR32BGx series. Discusses the Silicon Labs Packet Traffic Arbitration (PTA) support to coordinate 2.4GHz RF traffic for co-located Bluetooth and Wi-Fi radios.

  • Silicon Labs Coexistence Development Kit (SLWSTK-RSEXBP) (PDF): The Coexistence Development Kit (SLWSTK-COEXBP) is designed by Silicon Labs to demonstrate coexistence between different radios transmitting in the 2.4 GHz ISM band.

  • Configuring Antenna Diversity for OpenThread (PDF): Describes how to use Project Configurator and Component Editor in Simplicity Studio 5 to configure antenna diversity in OpenThread applications.

  • Configuring Antenna Diversity for Zigbee EmberZNet (PDF): Describes how to use Project Configurator and Component Editor in Simplicity Studio 5 to configure Antenna Diversity in Zigbee EmberZNet applications. Both receive and transmit antenna diversity configuration are discussed.