Fundamentals#

This section introduces multiprotocol concepts and describes the basics of improving coexistence with Wi-Fi.

  • Multiprotocol Fundamentals (PDF): Discusses the ways in which more than one protocol can be used on a single chip, including considerations when selecting protocols for multiprotocol implementations. It also describes the basics of the Silicon Labs Radio Scheduler, a required component of a dynamic multiprotocol solution.

  • Wi-Fi Coexistence Fundamentals (PDF): Introduces methods to improve the coexistence of 2.4 GHz IEEE 802.11b/g/n Wi-Fi and other 2.4 GHz radios such as Bluetooth, Bluetooth Mesh, Bluetooth Low Energy, and IEEE 802.15.4-based radios such as Zigbee and OpenThread.