This module includes functions that control the Thread stack's execution.

Functions

void otTaskletsProcess ( otInstance *aInstance)
Run all queued OpenThread tasklets at the time this is called.
bool otTaskletsArePending ( otInstance *aInstance)
Indicates whether or not OpenThread has tasklets pending.
void otTaskletsSignalPending ( otInstance *aInstance)
OpenThread calls this function when the tasklet queue transitions from empty to non-empty.

Detailed Description

This module includes functions that control the Thread stack's execution.

Function Documentation

◆ otTaskletsArePending()

bool otTaskletsArePending ( otInstance * aInstance )

Indicates whether or not OpenThread has tasklets pending.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Return values
TRUE If there are tasklets pending.
FALSE If there are no tasklets pending.

◆ otTaskletsProcess()

void otTaskletsProcess ( otInstance * aInstance )

Run all queued OpenThread tasklets at the time this is called.

Parameters
[in] aInstance A pointer to an OpenThread instance.

◆ otTaskletsSignalPending()

void otTaskletsSignalPending ( otInstance * aInstance )

OpenThread calls this function when the tasklet queue transitions from empty to non-empty.

Parameters
[in] aInstance A pointer to an OpenThread instance.