This module includes functions that control the Thread stack's execution.
Functions |
|
| otError | otDiagProcessCmd ( otInstance *aInstance, uint8_t aArgsLength, char *aArgs[], char *aOutput, size_t aOutputMaxLen) |
|
This function processes a factory diagnostics command line.
|
|
| void | otDiagProcessCmdLine ( otInstance *aInstance, const char *aString, char *aOutput, size_t aOutputMaxLen) |
|
This function processes a factory diagnostics command line.
|
|
| bool | otDiagIsEnabled ( otInstance *aInstance) |
|
This function indicates whether or not the factory diagnostics mode is enabled.
|
|
Detailed Description
This module includes functions that control the Thread stack's execution.
Function Documentation
◆ otDiagIsEnabled()
| bool otDiagIsEnabled | ( | otInstance * |
aInstance
|
) |
This function indicates whether or not the factory diagnostics mode is enabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Return values
-
TRUEif factory diagnostics mode is enabled FALSEif factory diagnostics mode is disabled.
◆ otDiagProcessCmd()
| otError otDiagProcessCmd | ( | otInstance * |
aInstance,
|
| uint8_t |
aArgsLength,
|
||
| char * |
aArgs[],
|
||
| char * |
aOutput,
|
||
| size_t |
aOutputMaxLen
|
||
| ) |
This function processes a factory diagnostics command line.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aArgsLengthThe number of elements in aArgs.[in] aArgsAn array of arguments. [out] aOutputThe diagnostics execution result. [in] aOutputMaxLenThe output buffer size.
- Return values
-
OT_ERROR_INVALID_ARGSThe command is supported but invalid arguments provided. OT_ERROR_NONEThe command is successfully process. OT_ERROR_NOT_IMPLEMENTEDThe command is not supported.
◆ otDiagProcessCmdLine()
| void otDiagProcessCmdLine | ( | otInstance * |
aInstance,
|
| const char * |
aString,
|
||
| char * |
aOutput,
|
||
| size_t |
aOutputMaxLen
|
||
| ) |
This function processes a factory diagnostics command line.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aStringA NULL-terminated input string. [out] aOutputThe diagnostics execution result. [in] aOutputMaxLenThe output buffer size.