UDP Forward
This module includes functions for UDP forward feature.
Typedefs |
|
| typedef void(* | otUdpForwarder ) ( otMessage *aMessage, uint16_t aPeerPort, otIp6Address *aPeerAddr, uint16_t aSockPort, void *aContext) |
|
This function pointer delivers the UDP packet to host and host should send the packet through its own network stack.
|
|
Functions |
|
| void | otUdpForwardSetForwarder ( otInstance *aInstance, otUdpForwarder aForwarder, void *aContext) |
|
Set UDP forward callback to deliver UDP packets to host.
|
|
| void | otUdpForwardReceive ( otInstance *aInstance, otMessage *aMessage, uint16_t aPeerPort, const otIp6Address *aPeerAddr, uint16_t aSockPort) |
|
Handle a UDP packet received from host.
|
|
Detailed Description
This module includes functions for UDP forward feature.
The functions in this module are available when udp-forward feature (
OPENTHREAD_CONFIG_UDP_FORWARD_ENABLE
) is enabled.
Typedef Documentation
◆ otUdpForwarder
| typedef void(* otUdpForwarder) ( otMessage *aMessage, uint16_t aPeerPort, otIp6Address *aPeerAddr, uint16_t aSockPort, void *aContext) |
This function pointer delivers the UDP packet to host and host should send the packet through its own network stack.
- Parameters
-
[in] aMessageA pointer to the UDP Message. [in] aPeerPortThe destination UDP port. [in] aPeerAddrA pointer to the destination IPv6 address. [in] aSockPortThe source UDP port. [in] aContextA pointer to application-specific context.
Function Documentation
◆ otUdpForwardReceive()
| void otUdpForwardReceive | ( | otInstance * |
aInstance,
|
| otMessage * |
aMessage,
|
||
| uint16_t |
aPeerPort,
|
||
| const otIp6Address * |
aPeerAddr,
|
||
| uint16_t |
aSockPort
|
||
| ) |
Handle a UDP packet received from host.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aMessageA pointer to the UDP Message. [in] aPeerPortThe source UDP port. [in] aPeerAddrA pointer to the source address. [in] aSockPortThe destination UDP port.
- Warning
- No matter the call success or fail, the message is freed.
◆ otUdpForwardSetForwarder()
| void otUdpForwardSetForwarder | ( | otInstance * |
aInstance,
|
| otUdpForwarder |
aForwarder,
|
||
| void * |
aContext
|
||
| ) |
Set UDP forward callback to deliver UDP packets to host.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aForwarderA pointer to a function called to forward UDP packet to host. [in] aContextA pointer to application-specific context.