Logging
This module includes the platform abstraction for the debug log service.
Macros |
|
| #define | OT_LOG_LEVEL_NONE 0 |
|
Log level None.
|
|
| #define | OT_LOG_LEVEL_CRIT 1 |
|
Log level Critical.
|
|
| #define | OT_LOG_LEVEL_WARN 2 |
|
Log level Warning.
|
|
| #define | OT_LOG_LEVEL_NOTE 3 |
|
Log level Notice.
|
|
| #define | OT_LOG_LEVEL_INFO 4 |
|
Log level Informational.
|
|
| #define | OT_LOG_LEVEL_DEBG 5 |
|
Log level Debug.
|
|
Typedefs |
|
| typedef int | otLogLevel |
|
This type represents the log level.
|
|
| typedef enum otLogRegion | otLogRegion |
|
This enumeration represents log regions.
|
|
Enumerations |
|
| enum |
otLogRegion
{
OT_LOG_REGION_API = 1, OT_LOG_REGION_MLE = 2, OT_LOG_REGION_ARP = 3, OT_LOG_REGION_NET_DATA = 4, OT_LOG_REGION_ICMP = 5, OT_LOG_REGION_IP6 = 6, OT_LOG_REGION_MAC = 7, OT_LOG_REGION_MEM = 8, OT_LOG_REGION_NCP = 9, OT_LOG_REGION_MESH_COP = 10, OT_LOG_REGION_NET_DIAG = 11, OT_LOG_REGION_PLATFORM = 12, OT_LOG_REGION_COAP = 13, OT_LOG_REGION_CLI = 14, OT_LOG_REGION_CORE = 15, OT_LOG_REGION_UTIL = 16, OT_LOG_REGION_BBR = 17, OT_LOG_REGION_MLR = 18, OT_LOG_REGION_DUA = 19, OT_LOG_REGION_BR = 20, OT_LOG_REGION_SRP = 21, OT_LOG_REGION_DNS = 22 } |
|
This enumeration represents log regions.
|
|
Functions |
|
| void | otPlatLog ( otLogLevel aLogLevel, otLogRegion aLogRegion, const char *aFormat,...) |
|
This function outputs logs.
|
|
| void | otPlatLogLine ( otLogLevel aLogLevel, otLogRegion aLogRegion, const char *aLogLine) |
|
This (optional) platform function outputs a prepared log line.
|
|
Detailed Description
This module includes the platform abstraction for the debug log service.
Macro Definition Documentation
◆ OT_LOG_LEVEL_CRIT
| #define OT_LOG_LEVEL_CRIT 1 |
Log level Critical.
- Note
- Log Levels are defines so that embedded implementations can eliminate code at compile time via #if/#else/#endif.
◆ OT_LOG_LEVEL_DEBG
| #define OT_LOG_LEVEL_DEBG 5 |
Log level Debug.
- Note
- Log Levels are defines so that embedded implementations can eliminate code at compile time via #if/#else/#endif.
◆ OT_LOG_LEVEL_INFO
| #define OT_LOG_LEVEL_INFO 4 |
Log level Informational.
- Note
- Log Levels are defines so that embedded implementations can eliminate code at compile time via #if/#else/#endif.
◆ OT_LOG_LEVEL_NONE
| #define OT_LOG_LEVEL_NONE 0 |
Log level None.
- Note
- Log Levels are defines so that embedded implementations can eliminate code at compile time via #if/#else/#endif.
◆ OT_LOG_LEVEL_NOTE
| #define OT_LOG_LEVEL_NOTE 3 |
Log level Notice.
- Note
- Log Levels are defines so that embedded implementations can eliminate code at compile time via #if/#else/#endif.
◆ OT_LOG_LEVEL_WARN
| #define OT_LOG_LEVEL_WARN 2 |
Log level Warning.
- Note
- Log Levels are defines so that embedded implementations can eliminate code at compile time via #if/#else/#endif.
Enumeration Type Documentation
◆ otLogRegion
| enum otLogRegion |
This enumeration represents log regions.
Function Documentation
◆ otPlatLog()
| void otPlatLog | ( | otLogLevel |
aLogLevel,
|
| otLogRegion |
aLogRegion,
|
||
| const char * |
aFormat,
|
||
...
|
|||
| ) |
This function outputs logs.
- Parameters
-
[in] aLogLevelThe log level. [in] aLogRegionThe log region. [in] aFormatA pointer to the format string. [in] ...Arguments for the format specification.
◆ otPlatLogLine()
| void otPlatLogLine | ( | otLogLevel |
aLogLevel,
|
| otLogRegion |
aLogRegion,
|
||
| const char * |
aLogLine
|
||
| ) |
This (optional) platform function outputs a prepared log line.
This platform function is used by OpenThread core when
OPENTHREAD_CONFIG_LOG_DEFINE_AS_MACRO_ONLY
is not enabled (in this case, the OT core itself will prepare a full log line).
Note that this function is optional and if not provided by platform layer, a default (weak) implementation is provided and used by OpenThread core as
otPlatLog(aLogLevel, aLogResion, "%s", aLogLine)
.
- Parameters
-
[in] aLogLevelThe log level. [in] aLogRegionThe log region. [in] aLogLineA pointer to a log line string.