This module includes functions that control link-layer configuration.
Classes |
|
| struct | otThreadLinkInfo |
|
This structure represents link-specific information for messages received from the Thread radio.
|
|
| struct | otMacFilterEntry |
|
This structure represents a Mac Filter entry.
|
|
| struct | otMacCounters |
|
This structure represents the MAC layer counters.
|
|
| struct | otActiveScanResult |
|
This structure represents a received IEEE 802.15.4 Beacon.
|
|
| struct | otEnergyScanResult |
|
This structure represents an energy scan result.
|
|
Macros |
|
| #define | OT_US_PER_TEN_SYMBOLS 160 |
|
The microseconds per 10 symbols.
|
|
| #define | OT_MAC_FILTER_FIXED_RSS_DISABLED 127 |
|
Used to indicate no fixed received signal strength was set.
|
|
| #define | OT_MAC_FILTER_ITERATOR_INIT 0 |
|
Initializer for otMacFilterIterator.
|
|
Typedefs |
|
| typedef struct otThreadLinkInfo | otThreadLinkInfo |
|
This structure represents link-specific information for messages received from the Thread radio.
|
|
| typedef uint8_t | otMacFilterIterator |
|
Used to iterate through mac filter entries.
|
|
| typedef enum otMacFilterAddressMode | otMacFilterAddressMode |
|
Defines address mode of the mac filter.
|
|
| typedef struct otMacFilterEntry | otMacFilterEntry |
|
This structure represents a Mac Filter entry.
|
|
| typedef struct otMacCounters | otMacCounters |
|
This structure represents the MAC layer counters.
|
|
| typedef struct otActiveScanResult | otActiveScanResult |
|
This structure represents a received IEEE 802.15.4 Beacon.
|
|
| typedef struct otEnergyScanResult | otEnergyScanResult |
|
This structure represents an energy scan result.
|
|
| typedef void(* | otHandleActiveScanResult ) ( otActiveScanResult *aResult, void *aContext) |
|
This function pointer is called during an IEEE 802.15.4 Active Scan when an IEEE 802.15.4 Beacon is received or the scan completes.
|
|
| typedef void(* | otHandleEnergyScanResult ) ( otEnergyScanResult *aResult, void *aContext) |
|
This function pointer is called during an IEEE 802.15.4 Energy Scan when the result for a channel is ready or the scan completes.
|
|
| typedef void(* | otLinkPcapCallback ) (const otRadioFrame *aFrame, bool aIsTx, void *aContext) |
|
This function pointer is called when an IEEE 802.15.4 frame is received.
|
|
Enumerations |
|
| enum |
otMacFilterAddressMode
{
OT_MAC_FILTER_ADDRESS_MODE_DISABLED , OT_MAC_FILTER_ADDRESS_MODE_ALLOWLIST , OT_MAC_FILTER_ADDRESS_MODE_DENYLIST } |
|
Defines address mode of the mac filter.
|
|
Functions |
|
| otError | otLinkActiveScan ( otInstance *aInstance, uint32_t aScanChannels, uint16_t aScanDuration, otHandleActiveScanResult aCallback, void *aCallbackContext) |
|
This function starts an IEEE 802.15.4 Active Scan.
|
|
| bool | otLinkIsActiveScanInProgress ( otInstance *aInstance) |
|
This function indicates whether or not an IEEE 802.15.4 Active Scan is currently in progress.
|
|
| otError | otLinkEnergyScan ( otInstance *aInstance, uint32_t aScanChannels, uint16_t aScanDuration, otHandleEnergyScanResult aCallback, void *aCallbackContext) |
|
This function starts an IEEE 802.15.4 Energy Scan.
|
|
| bool | otLinkIsEnergyScanInProgress ( otInstance *aInstance) |
|
This function indicates whether or not an IEEE 802.15.4 Energy Scan is currently in progress.
|
|
| otError | otLinkSendDataRequest ( otInstance *aInstance) |
|
This function enqueues an IEEE 802.15.4 Data Request message for transmission.
|
|
| bool | otLinkIsInTransmitState ( otInstance *aInstance) |
|
This function indicates whether or not an IEEE 802.15.4 MAC is in the transmit state.
|
|
| uint8_t | otLinkGetChannel ( otInstance *aInstance) |
|
Get the IEEE 802.15.4 channel.
|
|
| otError | otLinkSetChannel ( otInstance *aInstance, uint8_t aChannel) |
|
Set the IEEE 802.15.4 channel.
|
|
| uint32_t | otLinkGetSupportedChannelMask ( otInstance *aInstance) |
|
Get the supported channel mask of MAC layer.
|
|
| otError | otLinkSetSupportedChannelMask ( otInstance *aInstance, uint32_t aChannelMask) |
|
Set the supported channel mask of MAC layer.
|
|
| const otExtAddress * | otLinkGetExtendedAddress ( otInstance *aInstance) |
|
Gets the IEEE 802.15.4 Extended Address.
|
|
| otError | otLinkSetExtendedAddress ( otInstance *aInstance, const otExtAddress *aExtAddress) |
|
Sets the IEEE 802.15.4 Extended Address.
|
|
| void | otLinkGetFactoryAssignedIeeeEui64 ( otInstance *aInstance, otExtAddress *aEui64) |
|
Get the factory-assigned IEEE EUI-64.
|
|
| otPanId | otLinkGetPanId ( otInstance *aInstance) |
|
Get the IEEE 802.15.4 PAN ID.
|
|
| otError | otLinkSetPanId ( otInstance *aInstance, otPanId aPanId) |
|
Set the IEEE 802.15.4 PAN ID.
|
|
| uint32_t | otLinkGetPollPeriod ( otInstance *aInstance) |
|
Get the data poll period of sleepy end device.
|
|
| otError | otLinkSetPollPeriod ( otInstance *aInstance, uint32_t aPollPeriod) |
|
Set/clear user-specified/external data poll period for sleepy end device.
|
|
| otShortAddress | otLinkGetShortAddress ( otInstance *aInstance) |
|
Get the IEEE 802.15.4 Short Address.
|
|
| uint8_t | otLinkGetMaxFrameRetriesDirect ( otInstance *aInstance) |
|
This method returns the maximum number of frame retries during direct transmission.
|
|
| void | otLinkSetMaxFrameRetriesDirect ( otInstance *aInstance, uint8_t aMaxFrameRetriesDirect) |
|
This method sets the maximum number of frame retries during direct transmission.
|
|
| uint8_t | otLinkGetMaxFrameRetriesIndirect ( otInstance *aInstance) |
|
This method returns the maximum number of frame retries during indirect transmission.
|
|
| void | otLinkSetMaxFrameRetriesIndirect ( otInstance *aInstance, uint8_t aMaxFrameRetriesIndirect) |
|
This method sets the maximum number of frame retries during indirect transmission.
|
|
| otMacFilterAddressMode | otLinkFilterGetAddressMode ( otInstance *aInstance) |
|
This function gets the address mode of MAC filter.
|
|
| void | otLinkFilterSetAddressMode ( otInstance *aInstance, otMacFilterAddressMode aMode) |
|
This function sets the address mode of MAC filter.
|
|
| otError | otLinkFilterAddAddress ( otInstance *aInstance, const otExtAddress *aExtAddress) |
|
This method adds an Extended Address to MAC filter.
|
|
| void | otLinkFilterRemoveAddress ( otInstance *aInstance, const otExtAddress *aExtAddress) |
|
This method removes an Extended Address from MAC filter.
|
|
| void | otLinkFilterClearAddresses ( otInstance *aInstance) |
|
This method clears all the Extended Addresses from MAC filter.
|
|
| otError | otLinkFilterGetNextAddress ( otInstance *aInstance, otMacFilterIterator *aIterator, otMacFilterEntry *aEntry) |
|
This method gets an in-use address filter entry.
|
|
| otError | otLinkFilterAddRssIn ( otInstance *aInstance, const otExtAddress *aExtAddress, int8_t aRss) |
|
This method adds a fixed received signal strength (in dBm) entry for the messages from a given Extended Address in MAC Filter.
|
|
| void | otLinkFilterRemoveRssIn ( otInstance *aInstance, const otExtAddress *aExtAddress) |
|
This method removes a MAC Filter entry for fixed received signal strength setting for a given Extended Address.
|
|
| void | otLinkFilterSetDefaultRssIn ( otInstance *aInstance, int8_t aRss) |
|
This method sets the default received signal strength (in dBm) on MAC Filter.
|
|
| void | otLinkFilterClearDefaultRssIn ( otInstance *aInstance) |
|
This method clears any previously set default received signal strength (in dBm) on MAC Filter.
|
|
| void | otLinkFilterClearAllRssIn ( otInstance *aInstance) |
|
This method clears all the received signal strength entries (including default RSS-in) on MAC Filter.
|
|
| otError | otLinkFilterGetNextRssIn ( otInstance *aInstance, otMacFilterIterator *aIterator, otMacFilterEntry *aEntry) |
|
This method gets an in-use RssIn filter entry.
|
|
| void | otLinkSetRadioFilterEnabled ( otInstance *aInstance, bool aFilterEnabled) |
|
This function enables/disables IEEE 802.15.4 radio filter mode.
|
|
| bool | otLinkIsRadioFilterEnabled ( otInstance *aInstance) |
|
This function indicates whether the IEEE 802.15.4 radio filter is enabled or not.
|
|
| uint8_t | otLinkConvertRssToLinkQuality ( otInstance *aInstance, int8_t aRss) |
|
This method converts received signal strength to link quality.
|
|
| int8_t | otLinkConvertLinkQualityToRss ( otInstance *aInstance, uint8_t aLinkQuality) |
|
This method converts link quality to typical received signal strength.
|
|
| const uint32_t * | otLinkGetTxDirectRetrySuccessHistogram ( otInstance *aInstance, uint8_t *aNumberOfEntries) |
|
This method gets histogram of retries for a single direct packet until success.
|
|
| const uint32_t * | otLinkGetTxIndirectRetrySuccessHistogram ( otInstance *aInstance, uint8_t *aNumberOfEntries) |
|
This method gets histogram of retries for a single indirect packet until success.
|
|
| void | otLinkResetTxRetrySuccessHistogram ( otInstance *aInstance) |
|
This method clears histogram statistics for direct and indirect transmissions.
|
|
| const otMacCounters * | otLinkGetCounters ( otInstance *aInstance) |
|
Get the MAC layer counters.
|
|
| void | otLinkResetCounters ( otInstance *aInstance) |
|
Resets the MAC layer counters.
|
|
| void | otLinkSetPcapCallback ( otInstance *aInstance, otLinkPcapCallback aPcapCallback, void *aCallbackContext) |
|
This function registers a callback to provide received raw IEEE 802.15.4 frames.
|
|
| bool | otLinkIsPromiscuous ( otInstance *aInstance) |
|
This function indicates whether or not promiscuous mode is enabled at the link layer.
|
|
| otError | otLinkSetPromiscuous ( otInstance *aInstance, bool aPromiscuous) |
|
This function enables or disables the link layer promiscuous mode.
|
|
| uint8_t | otLinkCslGetChannel ( otInstance *aInstance) |
|
This function gets the CSL channel.
|
|
| otError | otLinkCslSetChannel ( otInstance *aInstance, uint8_t aChannel) |
|
Sets the CSL channel.
|
|
| uint16_t | otLinkCslGetPeriod ( otInstance *aInstance) |
|
This function gets the CSL period.
|
|
| otError | otLinkCslSetPeriod ( otInstance *aInstance, uint16_t aPeriod) |
|
Sets the CSL period in units of 10 symbols.
|
|
| uint32_t | otLinkCslGetTimeout ( otInstance *aInstance) |
|
This function gets the CSL timeout.
|
|
| otError | otLinkCslSetTimeout ( otInstance *aInstance, uint32_t aTimeout) |
|
Sets the CSL timeout in seconds.
|
|
| uint16_t | otLinkGetCcaFailureRate ( otInstance *aInstance) |
|
This function returns the current CCA (Clear Channel Assessment) failure rate.
|
|
| otError | otLinkSetEnabled ( otInstance *aInstance, bool aEnable) |
|
This function enables or disables the link layer.
|
|
| bool | otLinkIsEnabled ( otInstance *aInstance) |
|
This function indicates whether or not the link layer is enabled.
|
|
| otError | otLinkSendEmptyData ( otInstance *aInstance) |
|
This function instructs the device to send an empty IEEE 802.15.4 data frame.
|
|
Detailed Description
This module includes functions that control link-layer configuration.
Macro Definition Documentation
◆ OT_MAC_FILTER_FIXED_RSS_DISABLED
| #define OT_MAC_FILTER_FIXED_RSS_DISABLED 127 |
Used to indicate no fixed received signal strength was set.
Typedef Documentation
◆ otHandleActiveScanResult
| typedef void(* otHandleActiveScanResult) ( otActiveScanResult *aResult, void *aContext) |
This function pointer is called during an IEEE 802.15.4 Active Scan when an IEEE 802.15.4 Beacon is received or the scan completes.
- Parameters
-
[in] aResultA valid pointer to the beacon information or NULL when the active scan completes. [in] aContextA pointer to application-specific context.
◆ otHandleEnergyScanResult
| typedef void(* otHandleEnergyScanResult) ( otEnergyScanResult *aResult, void *aContext) |
This function pointer is called during an IEEE 802.15.4 Energy Scan when the result for a channel is ready or the scan completes.
- Parameters
-
[in] aResultA valid pointer to the energy scan result information or NULL when the energy scan completes. [in] aContextA pointer to application-specific context.
◆ otLinkPcapCallback
| typedef void(* otLinkPcapCallback) (const otRadioFrame *aFrame, bool aIsTx, void *aContext) |
This function pointer is called when an IEEE 802.15.4 frame is received.
- Note
-
This callback is called after FCS processing and
aFramemay not contain the actual FCS that was received. - This callback is called before IEEE 802.15.4 security processing.
- Parameters
-
[in] aFrameA pointer to the received IEEE 802.15.4 frame. [in] aIsTxWhether this frame is transmitted, not received. [in] aContextA pointer to application-specific context.
Enumeration Type Documentation
◆ otMacFilterAddressMode
Function Documentation
◆ otLinkActiveScan()
| otError otLinkActiveScan | ( | otInstance * |
aInstance,
|
| uint32_t |
aScanChannels,
|
||
| uint16_t |
aScanDuration,
|
||
| otHandleActiveScanResult |
aCallback,
|
||
| void * |
aCallbackContext
|
||
| ) |
This function starts an IEEE 802.15.4 Active Scan.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aScanChannelsA bit vector indicating which channels to scan (e.g. OT_CHANNEL_11_MASK). [in] aScanDurationThe time in milliseconds to spend scanning each channel. [in] aCallbackA pointer to a function called on receiving a beacon or scan completes. [in] aCallbackContextA pointer to application-specific context.
- Return values
-
OT_ERROR_NONEAccepted the Active Scan request. OT_ERROR_BUSYAlready performing an Active Scan.
◆ otLinkConvertLinkQualityToRss()
| int8_t otLinkConvertLinkQualityToRss | ( | otInstance * |
aInstance,
|
| uint8_t |
aLinkQuality
|
||
| ) |
This method converts link quality to typical received signal strength.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aLinkQualityLinkQuality value, should be in range [0,3].
- Returns
-
Typical platform received signal strength mapping to
aLinkQuality.
◆ otLinkConvertRssToLinkQuality()
| uint8_t otLinkConvertRssToLinkQuality | ( | otInstance * |
aInstance,
|
| int8_t |
aRss
|
||
| ) |
This method converts received signal strength to link quality.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aRssThe received signal strength value to be converted.
- Returns
-
Link quality value mapping to
aRss.
◆ otLinkCslGetChannel()
| uint8_t otLinkCslGetChannel | ( | otInstance * |
aInstance
|
) |
This function gets the CSL channel.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- The CSL channel.
◆ otLinkCslGetPeriod()
| uint16_t otLinkCslGetPeriod | ( | otInstance * |
aInstance
|
) |
This function gets the CSL period.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- The CSL period in units of 10 symbols.
◆ otLinkCslGetTimeout()
| uint32_t otLinkCslGetTimeout | ( | otInstance * |
aInstance
|
) |
This function gets the CSL timeout.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- The CSL timeout in seconds.
◆ otLinkCslSetChannel()
| otError otLinkCslSetChannel | ( | otInstance * |
aInstance,
|
| uint8_t |
aChannel
|
||
| ) |
Sets the CSL channel.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aChannelThe CSL sample channel. Channel value should be 0(Set CSL Channel unspecified) or within the range [1, 10] (if 915-MHz supported) and 11, 26 .
- Return values
-
OT_ERROR_NONESuccessfully set the CSL parameters. OT_ERROR_INVALID_ARGSInvalid aChannel.
◆ otLinkCslSetPeriod()
| otError otLinkCslSetPeriod | ( | otInstance * |
aInstance,
|
| uint16_t |
aPeriod
|
||
| ) |
Sets the CSL period in units of 10 symbols.
Disable CSL by setting this parameter to
0
.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aPeriodThe CSL period in units of 10 symbols.
- Return values
-
OT_ERROR_NONESuccessfully set the CSL period. OT_ERROR_INVALID_ARGSInvalid CSL period.
◆ otLinkCslSetTimeout()
| otError otLinkCslSetTimeout | ( | otInstance * |
aInstance,
|
| uint32_t |
aTimeout
|
||
| ) |
Sets the CSL timeout in seconds.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aTimeoutThe CSL timeout in seconds.
- Return values
-
OT_ERROR_NONESuccessfully set the CSL timeout. OT_ERROR_INVALID_ARGSInvalid CSL timeout.
◆ otLinkEnergyScan()
| otError otLinkEnergyScan | ( | otInstance * |
aInstance,
|
| uint32_t |
aScanChannels,
|
||
| uint16_t |
aScanDuration,
|
||
| otHandleEnergyScanResult |
aCallback,
|
||
| void * |
aCallbackContext
|
||
| ) |
This function starts an IEEE 802.15.4 Energy Scan.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aScanChannelsA bit vector indicating on which channels to perform energy scan. [in] aScanDurationThe time in milliseconds to spend scanning each channel. [in] aCallbackA pointer to a function called to pass on scan result on indicate scan completion. [in] aCallbackContextA pointer to application-specific context.
- Return values
-
OT_ERROR_NONEAccepted the Energy Scan request. OT_ERROR_BUSYCould not start the energy scan.
◆ otLinkFilterAddAddress()
| otError otLinkFilterAddAddress | ( | otInstance * |
aInstance,
|
| const otExtAddress * |
aExtAddress
|
||
| ) |
This method adds an Extended Address to MAC filter.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aExtAddressA pointer to the Extended Address (MUST NOT be NULL).
- Return values
-
OT_ERROR_NONESuccessfully added aExtAddressto MAC filter.OT_ERROR_NO_BUFSNo available entry exists.
◆ otLinkFilterAddRssIn()
| otError otLinkFilterAddRssIn | ( | otInstance * |
aInstance,
|
| const otExtAddress * |
aExtAddress,
|
||
| int8_t |
aRss
|
||
| ) |
This method adds a fixed received signal strength (in dBm) entry for the messages from a given Extended Address in MAC Filter.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aExtAddressA pointer to the IEEE 802.15.4 Extended Address. MUST NOT be NULL. [in] aRssA received signal strength (in dBm).
- Return values
-
OT_ERROR_NONESuccessfully added an entry for aExtAddressandaRss.OT_ERROR_NO_BUFSNo available entry exists.
◆ otLinkFilterClearAddresses()
| void otLinkFilterClearAddresses | ( | otInstance * |
aInstance
|
) |
This method clears all the Extended Addresses from MAC filter.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
◆ otLinkFilterClearAllRssIn()
| void otLinkFilterClearAllRssIn | ( | otInstance * |
aInstance
|
) |
This method clears all the received signal strength entries (including default RSS-in) on MAC Filter.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
◆ otLinkFilterClearDefaultRssIn()
| void otLinkFilterClearDefaultRssIn | ( | otInstance * |
aInstance
|
) |
This method clears any previously set default received signal strength (in dBm) on MAC Filter.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
◆ otLinkFilterGetAddressMode()
| otMacFilterAddressMode otLinkFilterGetAddressMode | ( | otInstance * |
aInstance
|
) |
This function gets the address mode of MAC filter.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- the address mode.
◆ otLinkFilterGetNextAddress()
| otError otLinkFilterGetNextAddress | ( | otInstance * |
aInstance,
|
| otMacFilterIterator * |
aIterator,
|
||
| otMacFilterEntry * |
aEntry
|
||
| ) |
This method gets an in-use address filter entry.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in,out] aIteratorA pointer to the MAC filter iterator context. To get the first in-use address filter entry, it should be set to OT_MAC_FILTER_ITERATOR_INIT. MUST NOT be NULL. [out] aEntryA pointer to where the information is placed. MUST NOT be NULL.
- Return values
-
OT_ERROR_NONESuccessfully retrieved an in-use address filter entry. OT_ERROR_NOT_FOUNDNo subsequent entry exists.
◆ otLinkFilterGetNextRssIn()
| otError otLinkFilterGetNextRssIn | ( | otInstance * |
aInstance,
|
| otMacFilterIterator * |
aIterator,
|
||
| otMacFilterEntry * |
aEntry
|
||
| ) |
This method gets an in-use RssIn filter entry.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in,out] aIteratorA pointer to the MAC filter iterator context. MUST NOT be NULL. To get the first entry, it should be set to OT_MAC_FILTER_ITERATOR_INIT. [out] aEntryA pointer to where the information is placed. The last entry would have the extended address as all 0xff to indicate the default received signal strength if it was set. aEntryMUST NOT be NULL.
- Return values
-
OT_ERROR_NONESuccessfully retrieved the next entry. OT_ERROR_NOT_FOUNDNo subsequent entry exists.
◆ otLinkFilterRemoveAddress()
| void otLinkFilterRemoveAddress | ( | otInstance * |
aInstance,
|
| const otExtAddress * |
aExtAddress
|
||
| ) |
This method removes an Extended Address from MAC filter.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
No action is performed if there is no existing entry in Filter matching the given Extended Address.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aExtAddressA pointer to the Extended Address (MUST NOT be NULL).
◆ otLinkFilterRemoveRssIn()
| void otLinkFilterRemoveRssIn | ( | otInstance * |
aInstance,
|
| const otExtAddress * |
aExtAddress
|
||
| ) |
This method removes a MAC Filter entry for fixed received signal strength setting for a given Extended Address.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
No action is performed if there is no existing entry in Filter matching the given Extended Address.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aExtAddressA pointer to the IEEE 802.15.4 Extended Address. MUST NOT be NULL.
◆ otLinkFilterSetAddressMode()
| void otLinkFilterSetAddressMode | ( | otInstance * |
aInstance,
|
| otMacFilterAddressMode |
aMode
|
||
| ) |
This function sets the address mode of MAC filter.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aModeThe address mode to set.
◆ otLinkFilterSetDefaultRssIn()
| void otLinkFilterSetDefaultRssIn | ( | otInstance * |
aInstance,
|
| int8_t |
aRss
|
||
| ) |
This method sets the default received signal strength (in dBm) on MAC Filter.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
The default RSS value is used for all received frames from addresses for which there is no explicit RSS-IN entry in the Filter list (added using
otLinkFilterAddRssIn()
).
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aRssThe default received signal strength (in dBm) to set.
◆ otLinkGetCcaFailureRate()
| uint16_t otLinkGetCcaFailureRate | ( | otInstance * |
aInstance
|
) |
This function returns the current CCA (Clear Channel Assessment) failure rate.
The rate is maintained over a window of (roughly) last
OPENTHREAD_CONFIG_CCA_FAILURE_RATE_AVERAGING_WINDOW
frame transmissions.
- Returns
-
The CCA failure rate with maximum value
0xffffcorresponding to 100% failure rate.
◆ otLinkGetChannel()
| uint8_t otLinkGetChannel | ( | otInstance * |
aInstance
|
) |
Get the IEEE 802.15.4 channel.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- The IEEE 802.15.4 channel.
- See also
- otLinkSetChannel
◆ otLinkGetCounters()
| const otMacCounters * otLinkGetCounters | ( | otInstance * |
aInstance
|
) |
Get the MAC layer counters.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- A pointer to the MAC layer counters.
◆ otLinkGetExtendedAddress()
| const otExtAddress * otLinkGetExtendedAddress | ( | otInstance * |
aInstance
|
) |
Gets the IEEE 802.15.4 Extended Address.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- A pointer to the IEEE 802.15.4 Extended Address.
◆ otLinkGetFactoryAssignedIeeeEui64()
| void otLinkGetFactoryAssignedIeeeEui64 | ( | otInstance * |
aInstance,
|
| otExtAddress * |
aEui64
|
||
| ) |
Get the factory-assigned IEEE EUI-64.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [out] aEui64A pointer to where the factory-assigned IEEE EUI-64 is placed.
◆ otLinkGetMaxFrameRetriesDirect()
| uint8_t otLinkGetMaxFrameRetriesDirect | ( | otInstance * |
aInstance
|
) |
This method returns the maximum number of frame retries during direct transmission.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- The maximum number of retries during direct transmission.
◆ otLinkGetMaxFrameRetriesIndirect()
| uint8_t otLinkGetMaxFrameRetriesIndirect | ( | otInstance * |
aInstance
|
) |
This method returns the maximum number of frame retries during indirect transmission.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- The maximum number of retries during indirect transmission.
◆ otLinkGetPanId()
| otPanId otLinkGetPanId | ( | otInstance * |
aInstance
|
) |
Get the IEEE 802.15.4 PAN ID.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- The IEEE 802.15.4 PAN ID.
- See also
- otLinkSetPanId
◆ otLinkGetPollPeriod()
| uint32_t otLinkGetPollPeriod | ( | otInstance * |
aInstance
|
) |
Get the data poll period of sleepy end device.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- The data poll period of sleepy end device in milliseconds.
- See also
- otLinkSetPollPeriod
◆ otLinkGetShortAddress()
| otShortAddress otLinkGetShortAddress | ( | otInstance * |
aInstance
|
) |
Get the IEEE 802.15.4 Short Address.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- A pointer to the IEEE 802.15.4 Short Address.
◆ otLinkGetSupportedChannelMask()
| uint32_t otLinkGetSupportedChannelMask | ( | otInstance * |
aInstance
|
) |
Get the supported channel mask of MAC layer.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
-
The supported channel mask as
uint32_twith bit 0 (lsb) mapping to channel 0, bit 1 to channel 1, so on.
◆ otLinkGetTxDirectRetrySuccessHistogram()
| const uint32_t* otLinkGetTxDirectRetrySuccessHistogram | ( | otInstance * |
aInstance,
|
| uint8_t * |
aNumberOfEntries
|
||
| ) |
This method gets histogram of retries for a single direct packet until success.
This function is valid when OPENTHREAD_CONFIG_MAC_RETRY_SUCCESS_HISTOGRAM_ENABLE configuration is enabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [out] aNumberOfEntriesA pointer to where the size of returned histogram array is placed.
- Returns
- A pointer to the histogram of retries (in a form of an array). The n-th element indicates that the packet has been sent with n-th retry.
◆ otLinkGetTxIndirectRetrySuccessHistogram()
| const uint32_t* otLinkGetTxIndirectRetrySuccessHistogram | ( | otInstance * |
aInstance,
|
| uint8_t * |
aNumberOfEntries
|
||
| ) |
This method gets histogram of retries for a single indirect packet until success.
This function is valid when OPENTHREAD_CONFIG_MAC_RETRY_SUCCESS_HISTOGRAM_ENABLE configuration is enabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [out] aNumberOfEntriesA pointer to where the size of returned histogram array is placed.
- Returns
- A pointer to the histogram of retries (in a form of an array). The n-th element indicates that the packet has been sent with n-th retry.
◆ otLinkIsActiveScanInProgress()
| bool otLinkIsActiveScanInProgress | ( | otInstance * |
aInstance
|
) |
This function indicates whether or not an IEEE 802.15.4 Active Scan is currently in progress.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- true if an IEEE 802.15.4 Active Scan is in progress, false otherwise.
◆ otLinkIsEnabled()
| bool otLinkIsEnabled | ( | otInstance * |
aInstance
|
) |
This function indicates whether or not the link layer is enabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Return values
-
trueLink layer is enabled. falseLink layer is not enabled.
◆ otLinkIsEnergyScanInProgress()
| bool otLinkIsEnergyScanInProgress | ( | otInstance * |
aInstance
|
) |
This function indicates whether or not an IEEE 802.15.4 Energy Scan is currently in progress.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- true if an IEEE 802.15.4 Energy Scan is in progress, false otherwise.
◆ otLinkIsInTransmitState()
| bool otLinkIsInTransmitState | ( | otInstance * |
aInstance
|
) |
This function indicates whether or not an IEEE 802.15.4 MAC is in the transmit state.
MAC module is in the transmit state during CSMA/CA procedure, CCA, Data, Beacon or Data Request frame transmission and receiving an ACK of a transmitted frame. MAC module is not in the transmit state during transmission of an ACK frame or a Beacon Request frame.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- true if an IEEE 802.15.4 MAC is in the transmit state, false otherwise.
◆ otLinkIsPromiscuous()
| bool otLinkIsPromiscuous | ( | otInstance * |
aInstance
|
) |
This function indicates whether or not promiscuous mode is enabled at the link layer.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Return values
-
truePromiscuous mode is enabled. falsePromiscuous mode is not enabled.
◆ otLinkIsRadioFilterEnabled()
| bool otLinkIsRadioFilterEnabled | ( | otInstance * |
aInstance
|
) |
This function indicates whether the IEEE 802.15.4 radio filter is enabled or not.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
- Return values
-
TRUEIf the radio filter is enabled. FALSEIf the radio filter is disabled.
◆ otLinkResetCounters()
| void otLinkResetCounters | ( | otInstance * |
aInstance
|
) |
Resets the MAC layer counters.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
◆ otLinkResetTxRetrySuccessHistogram()
| void otLinkResetTxRetrySuccessHistogram | ( | otInstance * |
aInstance
|
) |
This method clears histogram statistics for direct and indirect transmissions.
This function is valid when OPENTHREAD_CONFIG_MAC_RETRY_SUCCESS_HISTOGRAM_ENABLE configuration is enabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
◆ otLinkSendDataRequest()
| otError otLinkSendDataRequest | ( | otInstance * |
aInstance
|
) |
This function enqueues an IEEE 802.15.4 Data Request message for transmission.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Return values
-
OT_ERROR_NONESuccessfully enqueued an IEEE 802.15.4 Data Request message. OT_ERROR_INVALID_STATEDevice is not in rx-off-when-idle mode. OT_ERROR_NO_BUFSInsufficient message buffers available.
◆ otLinkSendEmptyData()
| otError otLinkSendEmptyData | ( | otInstance * |
aInstance
|
) |
This function instructs the device to send an empty IEEE 802.15.4 data frame.
This function is only supported on an Rx-Off-When-Idle device to send an empty data frame to its parent. Note: available only when
OPENTHREAD_CONFIG_REFERENCE_DEVICE_ENABLE
is enabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Return values
-
OT_ERROR_NONESuccessfully enqueued an empty message. OT_ERROR_INVALID_STATEDevice is not in Rx-Off-When-Idle mode. OT_ERROR_NO_BUFSInsufficient message buffers available.
◆ otLinkSetChannel()
| otError otLinkSetChannel | ( | otInstance * |
aInstance,
|
| uint8_t |
aChannel
|
||
| ) |
Set the IEEE 802.15.4 channel.
This function succeeds only when Thread protocols are disabled. A successful call to this function invalidates the Active and Pending Operational Datasets in non-volatile memory.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aChannelThe IEEE 802.15.4 channel.
- Return values
-
OT_ERROR_NONESuccessfully set the channel. OT_ERROR_INVALID_ARGSIf aChannelis not in the range [11, 26] or is not in the supported channel mask.OT_ERROR_INVALID_STATEThread protocols are enabled.
- See also
- otLinkGetChannel
◆ otLinkSetEnabled()
| otError otLinkSetEnabled | ( | otInstance * |
aInstance,
|
| bool |
aEnable
|
||
| ) |
This function enables or disables the link layer.
- Note
- The link layer may only be enabled / disabled when the Thread Interface is disabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aEnabletrue to enable the link layer, or false otherwise.
- Return values
-
OT_ERROR_NONESuccessfully enabled / disabled the link layer. OT_ERROR_INVALID_STATECould not disable the link layer because the Thread interface is enabled.
◆ otLinkSetExtendedAddress()
| otError otLinkSetExtendedAddress | ( | otInstance * |
aInstance,
|
| const otExtAddress * |
aExtAddress
|
||
| ) |
Sets the IEEE 802.15.4 Extended Address.
- Note
- Only succeeds when Thread protocols are disabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aExtAddressA pointer to the IEEE 802.15.4 Extended Address.
- Return values
-
OT_ERROR_NONESuccessfully set the IEEE 802.15.4 Extended Address. OT_ERROR_INVALID_ARGSaExtAddresswas NULL.OT_ERROR_INVALID_STATEThread protocols are enabled.
◆ otLinkSetMaxFrameRetriesDirect()
| void otLinkSetMaxFrameRetriesDirect | ( | otInstance * |
aInstance,
|
| uint8_t |
aMaxFrameRetriesDirect
|
||
| ) |
This method sets the maximum number of frame retries during direct transmission.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aMaxFrameRetriesDirectThe maximum number of retries during direct transmission.
◆ otLinkSetMaxFrameRetriesIndirect()
| void otLinkSetMaxFrameRetriesIndirect | ( | otInstance * |
aInstance,
|
| uint8_t |
aMaxFrameRetriesIndirect
|
||
| ) |
This method sets the maximum number of frame retries during indirect transmission.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aMaxFrameRetriesIndirectThe maximum number of retries during indirect transmission.
◆ otLinkSetPanId()
| otError otLinkSetPanId | ( | otInstance * |
aInstance,
|
| otPanId |
aPanId
|
||
| ) |
Set the IEEE 802.15.4 PAN ID.
This function succeeds only when Thread protocols are disabled. A successful call to this function also invalidates the Active and Pending Operational Datasets in non-volatile memory.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aPanIdThe IEEE 802.15.4 PAN ID.
- Return values
-
OT_ERROR_NONESuccessfully set the PAN ID. OT_ERROR_INVALID_ARGSIf aPanId is not in the range [0, 65534]. OT_ERROR_INVALID_STATEThread protocols are enabled.
- See also
- otLinkGetPanId
◆ otLinkSetPcapCallback()
| void otLinkSetPcapCallback | ( | otInstance * |
aInstance,
|
| otLinkPcapCallback |
aPcapCallback,
|
||
| void * |
aCallbackContext
|
||
| ) |
This function registers a callback to provide received raw IEEE 802.15.4 frames.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aPcapCallbackA pointer to a function that is called when receiving an IEEE 802.15.4 link frame or NULL to disable the callback. [in] aCallbackContextA pointer to application-specific context.
◆ otLinkSetPollPeriod()
| otError otLinkSetPollPeriod | ( | otInstance * |
aInstance,
|
| uint32_t |
aPollPeriod
|
||
| ) |
Set/clear user-specified/external data poll period for sleepy end device.
- Note
-
This function updates only poll period of sleepy end device. To update child timeout the function
otThreadSetChildTimeout()shall be called. -
Minimal non-zero value should be
OPENTHREAD_CONFIG_MAC_MINIMUM_POLL_PERIOD(10ms). Or zero to clear user-specified poll period. - User-specified value should be no more than the maximal value 0x3FFFFFF ((1 << 26) - 1) allowed, otherwise it would be clipped by the maximal value.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aPollPerioddata poll period in milliseconds.
- Return values
-
OT_ERROR_NONESuccessfully set/cleared user-specified poll period. OT_ERROR_INVALID_ARGSIf aPollPeriod is invalid.
- See also
- otLinkGetPollPeriod
◆ otLinkSetPromiscuous()
| otError otLinkSetPromiscuous | ( | otInstance * |
aInstance,
|
| bool |
aPromiscuous
|
||
| ) |
This function enables or disables the link layer promiscuous mode.
- Note
- Promiscuous mode may only be enabled when the Thread interface is disabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aPromiscuoustrue to enable promiscuous mode, or false otherwise.
- Return values
-
OT_ERROR_NONESuccessfully enabled promiscuous mode. OT_ERROR_INVALID_STATECould not enable promiscuous mode because the Thread interface is enabled.
◆ otLinkSetRadioFilterEnabled()
| void otLinkSetRadioFilterEnabled | ( | otInstance * |
aInstance,
|
| bool |
aFilterEnabled
|
||
| ) |
This function enables/disables IEEE 802.15.4 radio filter mode.
This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.
The radio filter is mainly intended for testing. It can be used to temporarily block all tx/rx on the 802.15.4 radio. When radio filter is enabled, radio is put to sleep instead of receive (to ensure device does not receive any frame and/or potentially send ack). Also the frame transmission requests return immediately without sending the frame over the air (return "no ack" error if ack is requested, otherwise return success).
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aFilterEnabledTRUE to enable radio filter, FALSE to disable
◆ otLinkSetSupportedChannelMask()
| otError otLinkSetSupportedChannelMask | ( | otInstance * |
aInstance,
|
| uint32_t |
aChannelMask
|
||
| ) |
Set the supported channel mask of MAC layer.
This function succeeds only when Thread protocols are disabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aChannelMaskThe supported channel mask (bit 0 or lsb mapping to channel 0, and so on).
- Return values
-
OT_ERROR_NONESuccessfully set the supported channel mask. OT_ERROR_INVALID_STATEThread protocols are enabled.