NAT64
This module includes functions and structs for the NAT64 function on the border router.
Classes |
|
| struct | otIp4Address |
|
This structure represents an IPv4 address.
|
|
| struct | otIp4Cidr |
|
This structure represents an IPv4 CIDR block.
|
|
| struct | otNat64Counters |
|
Represents the counters for NAT64.
|
|
| struct | otNat64ProtocolCounters |
|
Represents the counters for the protocols supported by NAT64.
|
|
| struct | otNat64ErrorCounters |
|
Represents the counters of dropped packets due to errors when handling NAT64 packets.
|
|
| struct | otNat64AddressMapping |
|
Represents an address mapping record for NAT64.
|
|
| struct | otNat64AddressMappingIterator |
|
Used to iterate through NAT64 address mappings.
|
|
Macros |
|
| #define | OT_IP4_ADDRESS_SIZE 4 |
|
Size of an IPv4 address (bytes)
|
|
| #define | OT_IP4_ADDRESS_STRING_SIZE 17 |
|
Length of 000.000.000.000 plus a suffix NUL.
|
|
| #define | OT_IP4_CIDR_STRING_SIZE 20 |
|
Length of 000.000.000.000/00 plus a suffix NUL.
|
|
Typedefs |
|
| typedef struct otIp4Address | otIp4Address |
|
This structure represents an IPv4 address.
|
|
| typedef struct otIp4Cidr | otIp4Cidr |
| typedef struct otNat64Counters | otNat64Counters |
|
Represents the counters for NAT64.
|
|
| typedef struct otNat64ProtocolCounters | otNat64ProtocolCounters |
|
Represents the counters for the protocols supported by NAT64.
|
|
| typedef enum otNat64DropReason | otNat64DropReason |
|
Packet drop reasons.
|
|
| typedef struct otNat64ErrorCounters | otNat64ErrorCounters |
|
Represents the counters of dropped packets due to errors when handling NAT64 packets.
|
|
| typedef struct otNat64AddressMapping | otNat64AddressMapping |
|
Represents an address mapping record for NAT64.
|
|
| typedef struct otNat64AddressMappingIterator | otNat64AddressMappingIterator |
|
Used to iterate through NAT64 address mappings.
|
|
| typedef void(* | otNat64ReceiveIp4Callback ) ( otMessage *aMessage, void *aContext) |
|
This function pointer is called when an IPv4 datagram (translated by NAT64 translator) is received.
|
|
Enumerations |
|
| enum |
otNat64DropReason
{
OT_NAT64_DROP_REASON_UNKNOWN = 0, OT_NAT64_DROP_REASON_ILLEGAL_PACKET , OT_NAT64_DROP_REASON_UNSUPPORTED_PROTO , OT_NAT64_DROP_REASON_NO_MAPPING , OT_NAT64_DROP_REASON_COUNT } |
|
Packet drop reasons.
|
|
| enum |
otNat64State
{
OT_NAT64_STATE_DISABLED = 0, OT_NAT64_STATE_NOT_RUNNING , OT_NAT64_STATE_IDLE , OT_NAT64_STATE_ACTIVE } |
|
States of NAT64.
|
|
Functions |
|
| void | otNat64GetCounters ( otInstance *aInstance, otNat64ProtocolCounters *aCounters) |
|
Gets NAT64 translator counters.
|
|
| void | otNat64GetErrorCounters ( otInstance *aInstance, otNat64ErrorCounters *aCounters) |
|
Gets the NAT64 translator error counters.
|
|
| void | otNat64InitAddressMappingIterator ( otInstance *aInstance, otNat64AddressMappingIterator *aIterator) |
Initializes an
otNat64AddressMappingIterator
.
|
|
| otError | otNat64GetNextAddressMapping ( otInstance *aInstance, otNat64AddressMappingIterator *aIterator, otNat64AddressMapping *aMapping) |
|
Gets the next AddressMapping info (using an iterator).
|
|
| otNat64State | otNat64GetTranslatorState ( otInstance *aInstance) |
|
Gets the state of NAT64 translator.
|
|
| otNat64State | otNat64GetPrefixManagerState ( otInstance *aInstance) |
|
Gets the state of NAT64 prefix manager.
|
|
| void | otNat64SetEnabled ( otInstance *aInstance, bool aEnable) |
|
Enable or disable NAT64 functions.
|
|
| otMessage * | otIp4NewMessage ( otInstance *aInstance, const otMessageSettings *aSettings) |
|
Allocate a new message buffer for sending an IPv4 message to the NAT64 translator.
|
|
| otError | otNat64SetIp4Cidr ( otInstance *aInstance, const otIp4Cidr *aCidr) |
|
Sets the CIDR used when setting the source address of the outgoing translated IPv4 packets.
|
|
| otError | otNat64Send ( otInstance *aInstance, otMessage *aMessage) |
|
Translates an IPv4 datagram to an IPv6 datagram and sends via the Thread interface.
|
|
| void | otNat64SetReceiveIp4Callback ( otInstance *aInstance, otNat64ReceiveIp4Callback aCallback, void *aContext) |
|
Registers a callback to provide received IPv4 datagrams.
|
|
| otError | otNat64GetCidr ( otInstance *aInstance, otIp4Cidr *aCidr) |
|
Gets the IPv4 CIDR configured in the NAT64 translator.
|
|
| bool | otIp4IsAddressEqual (const otIp4Address *aFirst, const otIp4Address *aSecond) |
|
Test if two IPv4 addresses are the same.
|
|
| void | otIp4ExtractFromIp6Address (uint8_t aPrefixLength, const otIp6Address *aIp6Address, otIp4Address *aIp4Address) |
Set
aIp4Address
by performing NAT64 address translation from
aIp6Address
as specified in RFC 6052.
|
|
| void | otIp4AddressToString (const otIp4Address *aAddress, char *aBuffer, uint16_t aSize) |
|
Converts the address to a string.
|
|
| void | otIp4CidrToString (const otIp4Cidr *aCidr, char *aBuffer, uint16_t aSize) |
|
Converts the IPv4 CIDR to a string.
|
|
| otError | otIp4AddressFromString (const char *aString, otIp4Address *aAddress) |
|
Converts a human-readable IPv4 address string into a binary representation.
|
|
| otError | otNat64SynthesizeIp6Address ( otInstance *aInstance, const otIp4Address *aIp4Address, otIp6Address *aIp6Address) |
|
Sets the IPv6 address by performing NAT64 address translation from the preferred NAT64 prefix and the given IPv4 address as specified in RFC 6052.
|
|
Variables |
|
| OT_TOOL_PACKED_BEGIN struct otIp4Address | OT_TOOL_PACKED_END |
Detailed Description
This module includes functions and structs for the NAT64 function on the border router.
These functions are only available when
OPENTHREAD_CONFIG_NAT64_BORDER_ROUTING_ENABLE
is enabled.
Typedef Documentation
◆ otNat64AddressMapping
| typedef struct otNat64AddressMapping otNat64AddressMapping |
Represents an address mapping record for NAT64.
- Note
-
The counters will be reset for each mapping session even for the same address pair. Applications can use
mIdto identify different sessions to calculate the packets correctly.
◆ otNat64AddressMappingIterator
| typedef struct otNat64AddressMappingIterator otNat64AddressMappingIterator |
Used to iterate through NAT64 address mappings.
The fields in this type are opaque (intended for use by OpenThread core only) and therefore should not be accessed or used by caller.
Before using an iterator, it MUST be initialized using
otNat64AddressMappingIteratorInit()
.
◆ otNat64ReceiveIp4Callback
| typedef void(* otNat64ReceiveIp4Callback) ( otMessage *aMessage, void *aContext) |
This function pointer is called when an IPv4 datagram (translated by NAT64 translator) is received.
- Parameters
-
[in] aMessageA pointer to the message buffer containing the received IPv6 datagram. This function transfers the ownership of the aMessageto the receiver of the callback. The message should be freed by the receiver of the callback after it is processed.[in] aContextA pointer to application-specific context.
Enumeration Type Documentation
◆ otNat64DropReason
| enum otNat64DropReason |
Packet drop reasons.
◆ otNat64State
| enum otNat64State |
States of NAT64.
Function Documentation
◆ otIp4AddressFromString()
| otError otIp4AddressFromString | ( | const char * |
aString,
|
| otIp4Address * |
aAddress
|
||
| ) |
Converts a human-readable IPv4 address string into a binary representation.
- Parameters
-
[in] aStringA pointer to a NULL-terminated string. [out] aAddressA pointer to an IPv4 address.
- Return values
-
OT_ERROR_NONESuccessfully parsed the string. OT_ERROR_INVALID_ARGSFailed to parse the string.
◆ otIp4AddressToString()
| void otIp4AddressToString | ( | const otIp4Address * |
aAddress,
|
| char * |
aBuffer,
|
||
| uint16_t |
aSize
|
||
| ) |
Converts the address to a string.
The string format uses quad-dotted notation of four bytes in the address (e.g., "127.0.0.1").
If the resulting string does not fit in
aBuffer
(within its
aSize
characters), the string will be truncated but the outputted string is always null-terminated.
- Parameters
-
[in] aAddressA pointer to an IPv4 address (MUST NOT be NULL). [out] aBufferA pointer to a char array to output the string (MUST NOT be nullptr).[in] aSizeThe size of aBuffer(in bytes).
◆ otIp4CidrToString()
| void otIp4CidrToString | ( | const otIp4Cidr * |
aCidr,
|
| char * |
aBuffer,
|
||
| uint16_t |
aSize
|
||
| ) |
Converts the IPv4 CIDR to a string.
The string format uses quad-dotted notation of four bytes in the address with the length of prefix (e.g., "127.0.0.1/32").
If the resulting string does not fit in
aBuffer
(within its
aSize
characters), the string will be truncated but the outputted string is always null-terminated.
- Parameters
-
[in] aCidrA pointer to an IPv4 CIDR (MUST NOT be NULL). [out] aBufferA pointer to a char array to output the string (MUST NOT be nullptr).[in] aSizeThe size of aBuffer(in bytes).
◆ otIp4ExtractFromIp6Address()
| void otIp4ExtractFromIp6Address | ( | uint8_t |
aPrefixLength,
|
| const otIp6Address * |
aIp6Address,
|
||
| otIp4Address * |
aIp4Address
|
||
| ) |
Set
aIp4Address
by performing NAT64 address translation from
aIp6Address
as specified in RFC 6052.
The NAT64
aPrefixLength
MUST be one of the following values: 32, 40, 48, 56, 64, or 96, otherwise the behavior of this method is undefined.
- Parameters
-
[in] aPrefixLengthThe prefix length to use for IPv4/IPv6 translation. [in] aIp6AddressA pointer to an IPv6 address. [out] aIp4AddressA pointer to output the IPv4 address.
◆ otIp4IsAddressEqual()
| bool otIp4IsAddressEqual | ( | const otIp4Address * |
aFirst,
|
| const otIp4Address * |
aSecond
|
||
| ) |
Test if two IPv4 addresses are the same.
- Parameters
-
[in] aFirstA pointer to the first IPv4 address to compare. [in] aSecondA pointer to the second IPv4 address to compare.
- Return values
-
TRUEThe two IPv4 addresses are the same. FALSEThe two IPv4 addresses are not the same.
◆ otIp4NewMessage()
| otMessage * otIp4NewMessage | ( | otInstance * |
aInstance,
|
| const otMessageSettings * |
aSettings
|
||
| ) |
Allocate a new message buffer for sending an IPv4 message to the NAT64 translator.
Message buffers allocated by this function will have 20 bytes (difference between the size of IPv6 headers and IPv4 header sizes) reserved.
Available when
OPENTHREAD_CONFIG_NAT64_TRANSLATOR_ENABLE
is enabled.
- Note
-
If
aSettingsisNULL, the link layer security is enabled and the message priority is set to OT_MESSAGE_PRIORITY_NORMAL by default.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aSettingsA pointer to the message settings or NULL to set default settings.
- Returns
- A pointer to the message buffer or NULL if no message buffers are available or parameters are invalid.
- See also
- otNat64Send
◆ otNat64GetCidr()
| otError otNat64GetCidr | ( | otInstance * |
aInstance,
|
| otIp4Cidr * |
aCidr
|
||
| ) |
Gets the IPv4 CIDR configured in the NAT64 translator.
Available when
OPENTHREAD_CONFIG_NAT64_TRANSLATOR_ENABLE
is enabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [out] aCidrA pointer to an otIp4Cidr . Where the CIDR will be filled.
◆ otNat64GetCounters()
| void otNat64GetCounters | ( | otInstance * |
aInstance,
|
| otNat64ProtocolCounters * |
aCounters
|
||
| ) |
Gets NAT64 translator counters.
The counter is counted since the instance initialized.
Available when
OPENTHREAD_CONFIG_NAT64_TRANSLATOR_ENABLE
is enabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [out] aCountersA pointer to an otNat64Counterswhere the counters of NAT64 translator will be placed.
◆ otNat64GetErrorCounters()
| void otNat64GetErrorCounters | ( | otInstance * |
aInstance,
|
| otNat64ErrorCounters * |
aCounters
|
||
| ) |
Gets the NAT64 translator error counters.
The counters are initialized to zero when the OpenThread instance is initialized.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [out] aCountersA pointer to an otNat64Counterswhere the counters of NAT64 translator will be placed.
◆ otNat64GetNextAddressMapping()
| otError otNat64GetNextAddressMapping | ( | otInstance * |
aInstance,
|
| otNat64AddressMappingIterator * |
aIterator,
|
||
| otNat64AddressMapping * |
aMapping
|
||
| ) |
Gets the next AddressMapping info (using an iterator).
Available when
OPENTHREAD_CONFIG_NAT64_TRANSLATOR_ENABLE
is enabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in,out] aIteratorA pointer to the iterator. On success the iterator will be updated to point to next NAT64 address mapping record. To get the first entry the iterator should be set to OT_NAT64_ADDRESS_MAPPING_ITERATOR_INIT. [out] aMappingA pointer to an otNat64AddressMappingwhere information of next NAT64 address mapping record is placed (on success).
- Return values
-
OT_ERROR_NONESuccessfully found the next NAT64 address mapping info ( aMappingwas successfully updated).OT_ERROR_NOT_FOUNDNo subsequent NAT64 address mapping info was found.
◆ otNat64GetPrefixManagerState()
| otNat64State otNat64GetPrefixManagerState | ( | otInstance * |
aInstance
|
) |
Gets the state of NAT64 prefix manager.
Available when
OPENTHREAD_CONFIG_NAT64_BORDER_ROUTING_ENABLE
is enabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Return values
-
OT_NAT64_STATE_DISABLEDNAT64 prefix manager is disabled. OT_NAT64_STATE_NOT_RUNNINGNAT64 prefix manager is enabled, but is not running (because the routing manager is not running). OT_NAT64_STATE_IDLENAT64 prefix manager is enabled, but is not publishing a NAT64 prefix. Usually when there is another border router publishing a NAT64 prefix with higher priority. OT_NAT64_STATE_ACTIVENAT64 prefix manager is enabled, and is publishing NAT64 prefix to the Thread network.
◆ otNat64GetTranslatorState()
| otNat64State otNat64GetTranslatorState | ( | otInstance * |
aInstance
|
) |
Gets the state of NAT64 translator.
Available when
OPENTHREAD_CONFIG_NAT64_TRANSLATOR_ENABLE
is enabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Return values
-
OT_NAT64_STATE_DISABLEDNAT64 translator is disabled. OT_NAT64_STATE_NOT_RUNNINGNAT64 translator is enabled, but the translator is not configured with a valid NAT64 prefix and a CIDR. OT_NAT64_STATE_ACTIVENAT64 translator is enabled, and is translating packets.
◆ otNat64InitAddressMappingIterator()
| void otNat64InitAddressMappingIterator | ( | otInstance * |
aInstance,
|
| otNat64AddressMappingIterator * |
aIterator
|
||
| ) |
Initializes an
otNat64AddressMappingIterator
.
An iterator MUST be initialized before it is used.
An iterator can be initialized again to restart from the beginning of the mapping info.
- Parameters
-
[in] aInstanceThe OpenThread instance. [out] aIteratorA pointer to the iterator to initialize.
◆ otNat64Send()
| otError otNat64Send | ( | otInstance * |
aInstance,
|
| otMessage * |
aMessage
|
||
| ) |
Translates an IPv4 datagram to an IPv6 datagram and sends via the Thread interface.
The caller transfers ownership of
aMessage
when making this call. OpenThread will free
aMessage
when processing is complete, including when a value other than
OT_ERROR_NONE
is returned.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aMessageA pointer to the message buffer containing the IPv4 datagram.
- Return values
-
OT_ERROR_NONESuccessfully processed the message. OT_ERROR_DROPMessage was well-formed but not fully processed due to packet processing rules. OT_ERROR_NO_BUFSCould not allocate necessary message buffers when processing the datagram. OT_ERROR_NO_ROUTENo route to host. OT_ERROR_INVALID_SOURCE_ADDRESSSource address is invalid, e.g. an anycast address or a multicast address. OT_ERROR_PARSEEncountered a malformed header when processing the message.
◆ otNat64SetEnabled()
| void otNat64SetEnabled | ( | otInstance * |
aInstance,
|
| bool |
aEnable
|
||
| ) |
Enable or disable NAT64 functions.
Note: This includes the NAT64 Translator (when
OPENTHREAD_CONFIG_NAT64_TRANSLATOR_ENABLE
is enabled) and the NAT64 Prefix Manager (when
OPENTHREAD_CONFIG_NAT64_BORDER_ROUTING_ENABLE
is enabled).
When
OPENTHREAD_CONFIG_NAT64_TRANSLATOR_ENABLE
is enabled, setting disabled to true resets the mapping table in the translator.
Available when
OPENTHREAD_CONFIG_NAT64_TRANSLATOR_ENABLE
or
OPENTHREAD_CONFIG_NAT64_BORDER_ROUTING_ENABLE
is enabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aEnabledA boolean to enable/disable the NAT64 functions
◆ otNat64SetIp4Cidr()
| otError otNat64SetIp4Cidr | ( | otInstance * |
aInstance,
|
| const otIp4Cidr * |
aCidr
|
||
| ) |
Sets the CIDR used when setting the source address of the outgoing translated IPv4 packets.
This function is available only when OPENTHREAD_CONFIG_NAT64_TRANSLATOR_ENABLE is enabled.
- Note
- A valid CIDR must have a non-zero prefix length. The actual addresses pool is limited by the size of the mapping pool and the number of addresses available in the CIDR block.
- This function can be called at any time, but the NAT64 translator will be reset and all existing sessions will be expired when updating the configured CIDR.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aCidrA pointer to an otIp4Cidr for the IPv4 CIDR block for NAT64.
- Return values
-
OT_ERROR_INVALID_ARGSThe given CIDR is not a valid IPv4 CIDR for NAT64. OT_ERROR_NONESuccessfully set the CIDR for NAT64.
- See also
- otBorderRouterSend
- otBorderRouterSetReceiveCallback
◆ otNat64SetReceiveIp4Callback()
| void otNat64SetReceiveIp4Callback | ( | otInstance * |
aInstance,
|
| otNat64ReceiveIp4Callback |
aCallback,
|
||
| void * |
aContext
|
||
| ) |
Registers a callback to provide received IPv4 datagrams.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aCallbackA pointer to a function that is called when an IPv4 datagram is received or NULL to disable the callback. [in] aCallbackContextA pointer to application-specific context.
◆ otNat64SynthesizeIp6Address()
| otError otNat64SynthesizeIp6Address | ( | otInstance * |
aInstance,
|
| const otIp4Address * |
aIp4Address,
|
||
| otIp6Address * |
aIp6Address
|
||
| ) |
Sets the IPv6 address by performing NAT64 address translation from the preferred NAT64 prefix and the given IPv4 address as specified in RFC 6052.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aIp4AddressA pointer to the IPv4 address to translate to IPv6. [out] aIp6AddressA pointer to the synthesized IPv6 address.
- Returns
- OT_ERROR_NONE Successfully synthesized the IPv6 address from NAT64 prefix and IPv4 address.
- OT_ERROR_INVALID_STATE No valid NAT64 prefix in the network data.