otNat64AddressMapping Struct Reference
Represents an address mapping record for NAT64.
#include <
include/openthread/nat64.h
>
Public Attributes |
|
| uint64_t | mId |
|
The unique id for a mapping session.
|
|
| otIp4Address | mIp4 |
|
The IPv4 address of the mapping.
|
|
| otIp6Address | mIp6 |
|
The IPv6 address of the mapping.
|
|
| uint32_t | mRemainingTimeMs |
|
Remaining time before expiry in milliseconds.
|
|
| otNat64ProtocolCounters | mCounters |
Represents an address mapping record for NAT64.
- Note
-
The counters will be reset for each mapping session even for the same address pair. Applications can use
mIdto identify different sessions to calculate the packets correctly.
The documentation for this struct was generated from the following file:
-
include/openthread/
nat64.h