Modules#
Message#
This module includes functions that manipulate OpenThread message buffers.
Enumerations#
This enumeration defines the OpenThread message priority levels.
Typedefs#
This enumeration defines the OpenThread message priority levels.
This structure represents a message settings.
This structure represents information about a message queue.
This structure represents the message buffer information for different queues used by OpenThread stack.
Functions#
Free an allocated message buffer.
Get the message length in bytes.
Set the message length in bytes.
Get the message offset in bytes.
Set the message offset in bytes.
This function indicates whether or not link security is enabled for the message.
This function sets/forces the message to be forwarded using direct transmission.
This function returns the average RSS (received signal strength) associated with the message.
Append bytes to a message.
Read bytes from a message.
Write bytes to a message.
Initialize the message queue.
This function adds a message to the end of the given message queue.
This function adds a message at the head/front of the given message queue.
This function removes a message from the given message queue.
This function returns a pointer to the message at the head of the queue.
This function returns a pointer to the next message in the queue by iterating forward (from head to tail).
Get the Message Buffer information.
Reset the Message Buffer information counter tracking the maximum number buffers in use at the same time.
Enumeration Documentation#
otMessagePriority#
otMessagePriority
This enumeration defines the OpenThread message priority levels.
| Enumerator | |
|---|---|
| OT_MESSAGE_PRIORITY_LOW | Low priority level. |
| OT_MESSAGE_PRIORITY_NORMAL | Normal priority level. |
| OT_MESSAGE_PRIORITY_HIGH | High priority level. |
Typedef Documentation#
otMessage#
typedef struct otMessage otMessage
This type is an opaque representation of an OpenThread message buffer.
otMessagePriority#
typedef enum otMessagePriority otMessagePriority
This enumeration defines the OpenThread message priority levels.
otMessageSettings#
typedef struct otMessageSettings otMessageSettings
This structure represents a message settings.
otMessageQueueInfo#
typedef struct otMessageQueueInfo otMessageQueueInfo
This structure represents information about a message queue.
otBufferInfo#
typedef struct otBufferInfo otBufferInfo
This structure represents the message buffer information for different queues used by OpenThread stack.
Function Documentation#
otMessageFree#
void otMessageFree (otMessage * aMessage)
Free an allocated message buffer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otMessage * | [in] | aMessage | A pointer to a message buffer. |
See Also
otMessageGetLength#
uint16_t otMessageGetLength (const otMessage * aMessage)
Get the message length in bytes.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const otMessage * | [in] | aMessage | A pointer to a message buffer. |
Returns
The message length in bytes.
See Also
otMessageSetLength#
otError otMessageSetLength (otMessage * aMessage, uint16_t aLength)
Set the message length in bytes.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otMessage * | [in] | aMessage | A pointer to a message buffer. |
| uint16_t | [in] | aLength | A length in bytes. |
See Also
otMessageGetOffset#
uint16_t otMessageGetOffset (const otMessage * aMessage)
Get the message offset in bytes.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const otMessage * | [in] | aMessage | A pointer to a message buffer. |
Returns
The message offset value.
See Also
otMessageSetOffset#
void otMessageSetOffset (otMessage * aMessage, uint16_t aOffset)
Set the message offset in bytes.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otMessage * | [in] | aMessage | A pointer to a message buffer. |
| uint16_t | [in] | aOffset | An offset in bytes. |
See Also
otMessageIsLinkSecurityEnabled#
bool otMessageIsLinkSecurityEnabled (const otMessage * aMessage)
This function indicates whether or not link security is enabled for the message.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const otMessage * | [in] | aMessage | A pointer to a message buffer. |
otMessageSetDirectTransmission#
void otMessageSetDirectTransmission (otMessage * aMessage, bool aEnabled)
This function sets/forces the message to be forwarded using direct transmission.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otMessage * | [in] | aMessage | A pointer to a message buffer. |
| bool | [in] | aEnabled | If |
Default setting for a new message is false.
otMessageGetRss#
int8_t otMessageGetRss (const otMessage * aMessage)
This function returns the average RSS (received signal strength) associated with the message.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const otMessage * | N/A | aMessage |
Returns
The average RSS value (in dBm) or OT_RADIO_RSSI_INVALID if no average RSS is available.
otMessageAppend#
otError otMessageAppend (otMessage * aMessage, const void * aBuf, uint16_t aLength)
Append bytes to a message.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otMessage * | [in] | aMessage | A pointer to a message buffer. |
| const void * | [in] | aBuf | A pointer to the data to append. |
| uint16_t | [in] | aLength | Number of bytes to append. |
See Also
otMessageRead#
uint16_t otMessageRead (const otMessage * aMessage, uint16_t aOffset, void * aBuf, uint16_t aLength)
Read bytes from a message.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const otMessage * | [in] | aMessage | A pointer to a message buffer. |
| uint16_t | [in] | aOffset | An offset in bytes. |
| void * | [in] | aBuf | A pointer to a buffer that message bytes are read to. |
| uint16_t | [in] | aLength | Number of bytes to read. |
Returns
The number of bytes read.
See Also
otMessageWrite#
int otMessageWrite (otMessage * aMessage, uint16_t aOffset, const void * aBuf, uint16_t aLength)
Write bytes to a message.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otMessage * | [in] | aMessage | A pointer to a message buffer. |
| uint16_t | [in] | aOffset | An offset in bytes. |
| const void * | [in] | aBuf | A pointer to a buffer that message bytes are written from. |
| uint16_t | [in] | aLength | Number of bytes to write. |
Returns
The number of bytes written.
See Also
otMessageQueueInit#
void otMessageQueueInit (otMessageQueue * aQueue)
Initialize the message queue.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otMessageQueue * | [in] | aQueue | A pointer to a message queue. |
This function MUST be called once and only once for a otMessageQueue instance before any other otMessageQueue functions. The behavior is undefined if other queue APIs are used with an otMessageQueue before it being initialized or if it is initialized more than once.
otMessageQueueEnqueue#
void otMessageQueueEnqueue (otMessageQueue * aQueue, otMessage * aMessage)
This function adds a message to the end of the given message queue.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otMessageQueue * | [in] | aQueue | A pointer to the message queue. |
| otMessage * | [in] | aMessage | The message to add. |
otMessageQueueEnqueueAtHead#
void otMessageQueueEnqueueAtHead (otMessageQueue * aQueue, otMessage * aMessage)
This function adds a message at the head/front of the given message queue.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otMessageQueue * | [in] | aQueue | A pointer to the message queue. |
| otMessage * | [in] | aMessage | The message to add. |
otMessageQueueDequeue#
void otMessageQueueDequeue (otMessageQueue * aQueue, otMessage * aMessage)
This function removes a message from the given message queue.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otMessageQueue * | [in] | aQueue | A pointer to the message queue. |
| otMessage * | [in] | aMessage | The message to remove. |
otMessageQueueGetHead#
otMessage * otMessageQueueGetHead (otMessageQueue * aQueue)
This function returns a pointer to the message at the head of the queue.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otMessageQueue * | [in] | aQueue | A pointer to a message queue. |
Returns
A pointer to the message at the head of queue or NULL if queue is empty.
otMessageQueueGetNext#
otMessage * otMessageQueueGetNext (otMessageQueue * aQueue, const otMessage * aMessage)
This function returns a pointer to the next message in the queue by iterating forward (from head to tail).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otMessageQueue * | [in] | aQueue | A pointer to a message queue. |
| const otMessage * | [in] | aMessage | A pointer to current message buffer. |
Returns
A pointer to the next message in the queue after
aMessageor NULL ifaMessage is the tail of queue. NULL is returned ifaMessageis not in the queueaQueue`.
otMessageGetBufferInfo#
void otMessageGetBufferInfo (otInstance * aInstance, otBufferInfo * aBufferInfo)
Get the Message Buffer information.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to the OpenThread instance. |
| otBufferInfo * | [out] | aBufferInfo | A pointer where the message buffer information is written. |
otMessageResetBufferInfo#
void otMessageResetBufferInfo (otInstance * aInstance)
Reset the Message Buffer information counter tracking the maximum number buffers in use at the same time.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to the OpenThread instance. |
This resets mMaxUsedBuffers in otBufferInfo.