Settings#
This module includes the platform abstraction for non-volatile storage of settings.
Enumerations#
This enumeration defines the keys of settings.
Functions#
Performs any initialization for the settings subsystem, if necessary.
Performs any de-initialization for the settings subsystem, if necessary.
Fetches the value of a setting.
Sets or replaces the value of a setting.
Adds a value to a setting.
Removes a setting from the setting store.
Removes all settings from the setting store.
Enumeration Documentation#
@22#
@22
This enumeration defines the keys of settings.
Note: When adding a new settings key, if the settings corresponding to the key contains security sensitive information, the developer MUST add the key to the array aSensitiveKeys which is passed in otPlatSettingsInit().
| Enumerator | |
|---|---|
| OT_SETTINGS_KEY_ACTIVE_DATASET | Active Operational Dataset. |
| OT_SETTINGS_KEY_PENDING_DATASET | Pending Operational Dataset. |
| OT_SETTINGS_KEY_NETWORK_INFO | Thread network information. |
| OT_SETTINGS_KEY_PARENT_INFO | Parent information. |
| OT_SETTINGS_KEY_CHILD_INFO | Child information. |
| OT_SETTINGS_KEY_SLAAC_IID_SECRET_KEY | SLAAC key to generate semantically opaque IID. |
| OT_SETTINGS_KEY_DAD_INFO | Duplicate Address Detection (DAD) information. |
| OT_SETTINGS_KEY_SRP_ECDSA_KEY | SRP client ECDSA public/private key pair. |
| OT_SETTINGS_KEY_SRP_CLIENT_INFO | The SRP client info (selected SRP server address). |
| OT_SETTINGS_KEY_SRP_SERVER_INFO | The SRP server info (UDP port). |
| OT_SETTINGS_KEY_BR_ULA_PREFIX | BR ULA prefix. |
| OT_SETTINGS_KEY_BR_ON_LINK_PREFIXES | BR local on-link prefixes. |
| OT_SETTINGS_KEY_BORDER_AGENT_ID | Unique Border Agent/Router ID. |
| OT_SETTINGS_KEY_VENDOR_RESERVED_MIN | |
| OT_SETTINGS_KEY_VENDOR_RESERVED_MAX | |
Function Documentation#
otPlatSettingsInit#
void otPlatSettingsInit (otInstance * aInstance, const uint16_t * aSensitiveKeys, uint16_t aSensitiveKeysLength)
Performs any initialization for the settings subsystem, if necessary.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. |
| const uint16_t * | [in] | aSensitiveKeys | A pointer to an array containing the list of sensitive keys. May be NULL only if |
| uint16_t | [in] | aSensitiveKeysLength | The number of entries in the |
This function also sets the sensitive keys that should be stored in the secure area.
Note that the memory pointed by aSensitiveKeys MUST not be released before aInstance is destroyed.
otPlatSettingsDeinit#
void otPlatSettingsDeinit (otInstance * aInstance)
Performs any de-initialization for the settings subsystem, if necessary.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. |
otPlatSettingsGet#
otError otPlatSettingsGet (otInstance * aInstance, uint16_t aKey, int aIndex, uint8_t * aValue, uint16_t * aValueLength)
Fetches the value of a setting.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. |
| uint16_t | [in] | aKey | The key associated with the requested setting. |
| int | [in] | aIndex | The index of the specific item to get. |
| uint8_t * | [out] | aValue | A pointer to where the value of the setting should be written. May be set to NULL if just testing for the presence or length of a setting. |
| uint16_t * | [inout] | aValueLength | A pointer to the length of the value. When called, this pointer should point to an integer containing the maximum value size that can be written to |
This function fetches the value of the setting identified by aKey and write it to the memory pointed to by aValue. It then writes the length to the integer pointed to by aValueLength. The initial value of aValueLength is the maximum number of bytes to be written to aValue.
This function can be used to check for the existence of a key without fetching the value by setting aValue and aValueLength to NULL. You can also check the length of the setting without fetching it by setting only aValue to NULL.
Note that the underlying storage implementation is not required to maintain the order of settings with multiple values. The order of such values MAY change after ANY write operation to the store.
otPlatSettingsSet#
otError otPlatSettingsSet (otInstance * aInstance, uint16_t aKey, const uint8_t * aValue, uint16_t aValueLength)
Sets or replaces the value of a setting.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. |
| uint16_t | [in] | aKey | The key associated with the setting to change. |
| const uint8_t * | [in] | aValue | A pointer to where the new value of the setting should be read from. MUST NOT be NULL if |
| uint16_t | [in] | aValueLength | The length of the data pointed to by aValue. May be zero. |
This function sets or replaces the value of a setting identified by aKey.
Calling this function successfully may cause unrelated settings with multiple values to be reordered.
OpenThread stack guarantees to use otPlatSettingsSet() method for a aKey that was either previously set using otPlatSettingsSet() (i.e., contains a single value) or is empty and/or fully deleted (contains no value).
Platform layer can rely and use this fact for optimizing its implementation.
otPlatSettingsAdd#
otError otPlatSettingsAdd (otInstance * aInstance, uint16_t aKey, const uint8_t * aValue, uint16_t aValueLength)
Adds a value to a setting.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. |
| uint16_t | [in] | aKey | The key associated with the setting to change. |
| const uint8_t * | [in] | aValue | A pointer to where the new value of the setting should be read from. MUST NOT be NULL if |
| uint16_t | [in] | aValueLength | The length of the data pointed to by |
This function adds the value to a setting identified by aKey, without replacing any existing values.
Note that the underlying implementation is not required to maintain the order of the items associated with a specific key. The added value may be added to the end, the beginning, or even somewhere in the middle. The order of any pre-existing values may also change.
Calling this function successfully may cause unrelated settings with multiple values to be reordered.
OpenThread stack guarantees to use otPlatSettingsAdd() method for a aKey that was either previously managed by otPlatSettingsAdd() (i.e., contains one or more items) or is empty and/or fully deleted (contains no value).
Platform layer can rely and use this fact for optimizing its implementation.
otPlatSettingsDelete#
otError otPlatSettingsDelete (otInstance * aInstance, uint16_t aKey, int aIndex)
Removes a setting from the setting store.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. |
| uint16_t | [in] | aKey | The key associated with the requested setting. |
| int | [in] | aIndex | The index of the value to be removed. If set to -1, all values for this |
This function deletes a specific value from the setting identified by aKey from the settings store.
Note that the underlying implementation is not required to maintain the order of the items associated with a specific key.
otPlatSettingsWipe#
void otPlatSettingsWipe (otInstance * aInstance)
Removes all settings from the setting store.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. |
This function deletes all settings from the settings store, resetting it to its initial factory state.