Represents statistics of a ping request.

Public Attributes#

uint16_t

The number of ping requests already sent.

uint16_t

The number of ping replies received.

uint32_t

The total round trip time of ping requests.

uint16_t

The min round trip time among ping requests.

uint16_t

The max round trip time among ping requests.

bool

Whether this is a multicast ping request.

Public Attribute Documentation#

mSentCount#

uint16_t otPingSenderStatistics::mSentCount

The number of ping requests already sent.


Definition at line 77 of file include/openthread/ping_sender.h

mReceivedCount#

uint16_t otPingSenderStatistics::mReceivedCount

The number of ping replies received.


Definition at line 78 of file include/openthread/ping_sender.h

mTotalRoundTripTime#

uint32_t otPingSenderStatistics::mTotalRoundTripTime

The total round trip time of ping requests.


Definition at line 79 of file include/openthread/ping_sender.h

mMinRoundTripTime#

uint16_t otPingSenderStatistics::mMinRoundTripTime

The min round trip time among ping requests.


Definition at line 80 of file include/openthread/ping_sender.h

mMaxRoundTripTime#

uint16_t otPingSenderStatistics::mMaxRoundTripTime

The max round trip time among ping requests.


Definition at line 81 of file include/openthread/ping_sender.h

mIsMulticast#

bool otPingSenderStatistics::mIsMulticast

Whether this is a multicast ping request.


Definition at line 82 of file include/openthread/ping_sender.h