Represents a Server configuration.

Public Attributes#

bool

Whether this config is considered Stable Network Data.

uint8_t

Length of server data.

uint8_t

Server data bytes.

uint16_t

The Server RLOC16.

Public Attribute Documentation#

mStable#

bool otServerConfig::mStable

Whether this config is considered Stable Network Data.


Definition at line 121 of file include/openthread/netdata.h

mServerDataLength#

uint8_t otServerConfig::mServerDataLength

Length of server data.


Definition at line 122 of file include/openthread/netdata.h

mServerData#

uint8_t otServerConfig::mServerData[OT_SERVER_DATA_MAX_SIZE]

Server data bytes.


Definition at line 123 of file include/openthread/netdata.h

mRloc16#

uint16_t otServerConfig::mRloc16

The Server RLOC16.


Definition at line 124 of file include/openthread/netdata.h