Router/Leader#

This module includes functions for Thread Routers and Leaders.

Modules#

otChildInfo

otCacheEntryInfo

otCacheEntryIterator

otDeviceProperties

otNeighborTableEntryInfo

Enumerations#

enum
OT_CACHE_ENTRY_STATE_CACHED = 0
OT_CACHE_ENTRY_STATE_SNOOPED = 1
OT_CACHE_ENTRY_STATE_QUERY = 2
OT_CACHE_ENTRY_STATE_RETRY_QUERY = 3
}

Defines the EID cache entry state.

enum
OT_POWER_SUPPLY_BATTERY = 0
OT_POWER_SUPPLY_EXTERNAL = 1
OT_POWER_SUPPLY_EXTERNAL_STABLE = 2
OT_POWER_SUPPLY_EXTERNAL_UNSTABLE = 3
}

Represents the power supply property on a device.

enum
OT_NEIGHBOR_TABLE_EVENT_CHILD_ADDED
OT_NEIGHBOR_TABLE_EVENT_CHILD_REMOVED
OT_NEIGHBOR_TABLE_EVENT_CHILD_MODE_CHANGED
OT_NEIGHBOR_TABLE_EVENT_ROUTER_ADDED
OT_NEIGHBOR_TABLE_EVENT_ROUTER_REMOVED
}

Defines the constants used in otNeighborTableCallback to indicate changes in neighbor table.

Typedefs#

typedef uint16_t

Used to iterate through IPv6 addresses of a Thread Child entry.

typedef enum otCacheEntryState

Defines the EID cache entry state.

typedef struct otCacheEntryInfo

Represents an EID cache entry.

typedef struct otCacheEntryIterator

Represents an iterator used for iterating through the EID cache table entries.

typedef struct otDeviceProperties

Represents the device properties which are used for calculating the local leader weight on a device.

typedef void(*
otNeighborTableCallback)(otNeighborTableEvent aEvent, const otNeighborTableEntryInfo *aEntryInfo)

Pointer is called to notify that there is a change in the neighbor table.

Functions#

uint16_t
otThreadGetMaxAllowedChildren(otInstance *aInstance)

Gets the maximum number of children currently allowed.

otThreadSetMaxAllowedChildren(otInstance *aInstance, uint16_t aMaxChildren)

Sets the maximum number of children currently allowed.

bool
otThreadIsRouterEligible(otInstance *aInstance)

Indicates whether or not the device is router-eligible.

otThreadSetRouterEligible(otInstance *aInstance, bool aEligible)

Sets whether or not the device is router-eligible.

otThreadSetPreferredRouterId(otInstance *aInstance, uint8_t aRouterId)

Set the preferred Router Id.

otThreadGetDeviceProperties(otInstance *aInstance)

Get the current device properties.

void
otThreadSetDeviceProperties(otInstance *aInstance, const otDeviceProperties *aDeviceProperties)

Set the device properties which are then used to determine and set the Leader Weight.

uint8_t
otThreadGetLocalLeaderWeight(otInstance *aInstance)

Gets the Thread Leader Weight used when operating in the Leader role.

void
otThreadSetLocalLeaderWeight(otInstance *aInstance, uint8_t aWeight)

Sets the Thread Leader Weight used when operating in the Leader role.

uint32_t

Get the preferred Thread Leader Partition Id used when operating in the Leader role.

void
otThreadSetPreferredLeaderPartitionId(otInstance *aInstance, uint32_t aPartitionId)

Set the preferred Thread Leader Partition Id used when operating in the Leader role.

uint16_t
otThreadGetJoinerUdpPort(otInstance *aInstance)

Gets the Joiner UDP Port.

otThreadSetJoinerUdpPort(otInstance *aInstance, uint16_t aJoinerUdpPort)

Sets the Joiner UDP Port.

void
otThreadSetSteeringData(otInstance *aInstance, const otExtAddress *aExtAddress)

Set Steering data out of band.

uint32_t
otThreadGetContextIdReuseDelay(otInstance *aInstance)

Get the CONTEXT_ID_REUSE_DELAY parameter used in the Leader role.

void
otThreadSetContextIdReuseDelay(otInstance *aInstance, uint32_t aDelay)

Set the CONTEXT_ID_REUSE_DELAY parameter used in the Leader role.

uint8_t
otThreadGetNetworkIdTimeout(otInstance *aInstance)

Get the NETWORK_ID_TIMEOUT parameter.

void
otThreadSetNetworkIdTimeout(otInstance *aInstance, uint8_t aTimeout)

Set the NETWORK_ID_TIMEOUT parameter.

uint8_t
otThreadGetRouterUpgradeThreshold(otInstance *aInstance)

Get the ROUTER_UPGRADE_THRESHOLD parameter used in the REED role.

void
otThreadSetRouterUpgradeThreshold(otInstance *aInstance, uint8_t aThreshold)

Set the ROUTER_UPGRADE_THRESHOLD parameter used in the Leader role.

uint8_t
otThreadGetChildRouterLinks(otInstance *aInstance)

Get the MLE_CHILD_ROUTER_LINKS parameter used in the REED role.

otThreadSetChildRouterLinks(otInstance *aInstance, uint8_t aChildRouterLinks)

Set the MLE_CHILD_ROUTER_LINKS parameter used in the REED role.

otThreadReleaseRouterId(otInstance *aInstance, uint8_t aRouterId)

Release a Router ID that has been allocated by the device in the Leader role.

otThreadBecomeRouter(otInstance *aInstance)

Attempt to become a router.

otThreadBecomeLeader(otInstance *aInstance)

Become a leader and start a new partition.

uint8_t

Get the ROUTER_DOWNGRADE_THRESHOLD parameter used in the Router role.

void
otThreadSetRouterDowngradeThreshold(otInstance *aInstance, uint8_t aThreshold)

Set the ROUTER_DOWNGRADE_THRESHOLD parameter used in the Leader role.

uint8_t
otThreadGetRouterSelectionJitter(otInstance *aInstance)

Get the ROUTER_SELECTION_JITTER parameter used in the REED/Router role.

void
otThreadSetRouterSelectionJitter(otInstance *aInstance, uint8_t aRouterJitter)

Set the ROUTER_SELECTION_JITTER parameter used in the REED/Router role.

otThreadGetChildInfoById(otInstance *aInstance, uint16_t aChildId, otChildInfo *aChildInfo)

Gets diagnostic information for an attached Child by its Child ID or RLOC16.

otThreadGetChildInfoByIndex(otInstance *aInstance, uint16_t aChildIndex, otChildInfo *aChildInfo)

The function retains diagnostic information for an attached Child by the internal table index.

otThreadGetChildNextIp6Address(otInstance *aInstance, uint16_t aChildIndex, otChildIp6AddressIterator *aIterator, otIp6Address *aAddress)

Gets the next IPv6 address (using an iterator) for a given child.

uint8_t
otThreadGetRouterIdSequence(otInstance *aInstance)

Get the current Router ID Sequence.

uint8_t
otThreadGetMaxRouterId(otInstance *aInstance)

The function returns the maximum allowed router ID.

otThreadGetRouterInfo(otInstance *aInstance, uint16_t aRouterId, otRouterInfo *aRouterInfo)

The function retains diagnostic information for a given Thread Router.

otThreadGetNextCacheEntry(otInstance *aInstance, otCacheEntryInfo *aEntryInfo, otCacheEntryIterator *aIterator)

Gets the next EID cache entry (using an iterator).

void
otThreadGetPskc(otInstance *aInstance, otPskc *aPskc)

Get the Thread PSKc.

otThreadGetPskcRef(otInstance *aInstance)

Get Key Reference to Thread PSKc stored.

otThreadSetPskc(otInstance *aInstance, const otPskc *aPskc)

Set the Thread PSKc.

otThreadSetPskcRef(otInstance *aInstance, otPskcRef aKeyRef)

Set the Key Reference to the Thread PSKc.

int8_t
otThreadGetParentPriority(otInstance *aInstance)

Get the assigned parent priority.

otThreadSetParentPriority(otInstance *aInstance, int8_t aParentPriority)

Set the parent priority.

uint8_t
otThreadGetMaxChildIpAddresses(otInstance *aInstance)

Gets the maximum number of IP addresses that each MTD child may register with this device as parent.

otThreadSetMaxChildIpAddresses(otInstance *aInstance, uint8_t aMaxIpAddresses)

Sets or restores the maximum number of IP addresses that each MTD child may register with this device as parent.

void
otThreadRegisterNeighborTableCallback(otInstance *aInstance, otNeighborTableCallback aCallback)

Registers a neighbor table callback function.

void
otThreadSetCcmEnabled(otInstance *aInstance, bool aEnabled)

Sets whether the device was commissioned using CCM.

void
otThreadSetThreadVersionCheckEnabled(otInstance *aInstance, bool aEnabled)

Sets whether the Security Policy TLV version-threshold for routing (VR field) is enabled.

void
otThreadGetRouterIdRange(otInstance *aInstance, uint8_t *aMinRouterId, uint8_t *aMaxRouterId)

Gets the range of router IDs that are allowed to assign to nodes within the thread network.

otThreadSetRouterIdRange(otInstance *aInstance, uint8_t aMinRouterId, uint8_t aMaxRouterId)

Sets the range of router IDs that are allowed to assign to nodes within the thread network.

uint32_t

Gets the current Interval Max value used by Advertisement trickle timer.

bool
otThreadIsRouterIdAllocated(otInstance *aInstance, uint8_t aRouterId)

Indicates whether or not a Router ID is currently allocated.

void
otThreadGetNextHopAndPathCost(otInstance *aInstance, uint16_t aDestRloc16, uint16_t *aNextHopRloc16, uint8_t *aPathCost)

Gets the next hop and path cost towards a given RLOC16 destination.

Macros#

#define

Initializer for otChildIP6AddressIterator.

Enumeration Documentation#

otCacheEntryState#

otCacheEntryState

Defines the EID cache entry state.

Enumerator
OT_CACHE_ENTRY_STATE_CACHED
OT_CACHE_ENTRY_STATE_SNOOPED
OT_CACHE_ENTRY_STATE_QUERY
OT_CACHE_ENTRY_STATE_RETRY_QUERY

otPowerSupply#

otPowerSupply

Represents the power supply property on a device.

This is used as a property in otDeviceProperties to calculate the leader weight.

Enumerator
OT_POWER_SUPPLY_BATTERY

Battery powered.

OT_POWER_SUPPLY_EXTERNAL

Externally powered (mains-powered).

OT_POWER_SUPPLY_EXTERNAL_STABLE

Stable external power with a battery backup or UPS.

OT_POWER_SUPPLY_EXTERNAL_UNSTABLE

Potentially unstable ext power (e.g. light bulb powered via a switch).


otNeighborTableEvent#

otNeighborTableEvent

Defines the constants used in otNeighborTableCallback to indicate changes in neighbor table.

Enumerator
OT_NEIGHBOR_TABLE_EVENT_CHILD_ADDED

A child is being added.

OT_NEIGHBOR_TABLE_EVENT_CHILD_REMOVED

A child is being removed.

OT_NEIGHBOR_TABLE_EVENT_CHILD_MODE_CHANGED

An existing child's mode is changed.

OT_NEIGHBOR_TABLE_EVENT_ROUTER_ADDED

A router is being added.

OT_NEIGHBOR_TABLE_EVENT_ROUTER_REMOVED

A router is being removed.


Typedef Documentation#

otChildIp6AddressIterator#

typedef uint16_t otChildIp6AddressIterator

Used to iterate through IPv6 addresses of a Thread Child entry.


otCacheEntryState#

typedef enum otCacheEntryState otCacheEntryState

Defines the EID cache entry state.


otCacheEntryInfo#

typedef struct otCacheEntryInfo otCacheEntryInfo

Represents an EID cache entry.


otCacheEntryIterator#

typedef struct otCacheEntryIterator otCacheEntryIterator

Represents an iterator used for iterating through the EID cache table entries.

To initialize the iterator and start from the first entry in the cache table, set all its fields in the structure to zero (e.g., memset the iterator to zero).


otDeviceProperties#

typedef struct otDeviceProperties otDeviceProperties

Represents the device properties which are used for calculating the local leader weight on a device.

The parameters are set based on device's capability, whether acting as border router, its power supply config, etc.

mIsUnstable indicates operational stability of device and is determined via a vendor specific mechanism. It can include the following cases:

  • Device internally detects that it loses external power supply more often than usual. What is usual is determined by the vendor.

  • Device internally detects that it reboots more often than usual. What is usual is determined by the vendor.


otNeighborTableCallback#

typedef void(* otNeighborTableCallback) (otNeighborTableEvent aEvent, const otNeighborTableEntryInfo *aEntryInfo) )(otNeighborTableEvent aEvent, const otNeighborTableEntryInfo *aEntryInfo)

Pointer is called to notify that there is a change in the neighbor table.

Parameters
TypeDirectionArgument NameDescription
[in]aEvent

A event flag.

[in]aEntryInfo

A pointer to table entry info.


Function Documentation#

otThreadGetMaxAllowedChildren#

uint16_t otThreadGetMaxAllowedChildren (otInstance * aInstance)

Gets the maximum number of children currently allowed.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The maximum number of children currently allowed.

See Also


otThreadSetMaxAllowedChildren#

otError otThreadSetMaxAllowedChildren (otInstance * aInstance, uint16_t aMaxChildren)

Sets the maximum number of children currently allowed.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint16_t[in]aMaxChildren

The maximum allowed children.

This parameter can only be set when Thread protocol operation has been stopped.

See Also


otThreadIsRouterEligible#

bool otThreadIsRouterEligible (otInstance * aInstance)

Indicates whether or not the device is router-eligible.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.


otThreadSetRouterEligible#

otError otThreadSetRouterEligible (otInstance * aInstance, bool aEligible)

Sets whether or not the device is router-eligible.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

bool[in]aEligible

TRUE to configure the device as router-eligible, FALSE otherwise.

If aEligible is false and the device is currently operating as a router, this call will cause the device to detach and attempt to reattach as a child.


otThreadSetPreferredRouterId#

otError otThreadSetPreferredRouterId (otInstance * aInstance, uint8_t aRouterId)

Set the preferred Router Id.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t[in]aRouterId

The preferred Router Id.

Upon becoming a router/leader the node attempts to use this Router Id. If the preferred Router Id is not set or if it can not be used, a randomly generated router id is picked. This property can be set only when the device role is either detached or disabled.

Note

  • This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.


otThreadGetDeviceProperties#

const otDeviceProperties * otThreadGetDeviceProperties (otInstance * aInstance)

Get the current device properties.

Parameters
TypeDirectionArgument NameDescription
otInstance *N/AaInstance

Requires OPENTHREAD_CONFIG_MLE_DEVICE_PROPERTY_LEADER_WEIGHT_ENABLE.

Returns

  • The device properties otDeviceProperties.


otThreadSetDeviceProperties#

void otThreadSetDeviceProperties (otInstance * aInstance, const otDeviceProperties * aDeviceProperties)

Set the device properties which are then used to determine and set the Leader Weight.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

const otDeviceProperties *[in]aDeviceProperties

The device properties.

Requires OPENTHREAD_CONFIG_MLE_DEVICE_PROPERTY_LEADER_WEIGHT_ENABLE.


otThreadGetLocalLeaderWeight#

uint8_t otThreadGetLocalLeaderWeight (otInstance * aInstance)

Gets the Thread Leader Weight used when operating in the Leader role.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The Thread Leader Weight value.

See Also


otThreadSetLocalLeaderWeight#

void otThreadSetLocalLeaderWeight (otInstance * aInstance, uint8_t aWeight)

Sets the Thread Leader Weight used when operating in the Leader role.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t[in]aWeight

The Thread Leader Weight value.

Directly sets the Leader Weight to the new value, replacing its previous value (which may have been determined from the current otDeviceProperties).

See Also


otThreadGetPreferredLeaderPartitionId#

uint32_t otThreadGetPreferredLeaderPartitionId (otInstance * aInstance)

Get the preferred Thread Leader Partition Id used when operating in the Leader role.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The Thread Leader Partition Id value.


otThreadSetPreferredLeaderPartitionId#

void otThreadSetPreferredLeaderPartitionId (otInstance * aInstance, uint32_t aPartitionId)

Set the preferred Thread Leader Partition Id used when operating in the Leader role.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint32_t[in]aPartitionId

The Thread Leader Partition Id value.


otThreadGetJoinerUdpPort#

uint16_t otThreadGetJoinerUdpPort (otInstance * aInstance)

Gets the Joiner UDP Port.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The Joiner UDP Port number.

See Also


otThreadSetJoinerUdpPort#

otError otThreadSetJoinerUdpPort (otInstance * aInstance, uint16_t aJoinerUdpPort)

Sets the Joiner UDP Port.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint16_t[in]aJoinerUdpPort

The Joiner UDP Port number.

See Also


otThreadSetSteeringData#

void otThreadSetSteeringData (otInstance * aInstance, const otExtAddress * aExtAddress)

Set Steering data out of band.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

const otExtAddress *[in]aExtAddress

Address used to update the steering data. All zeros to clear the steering data (no steering data). All 0xFFs to set steering data/bloom filter to accept/allow all. A specific EUI64 which is then added to current steering data/bloom filter.

Configuration option OPENTHREAD_CONFIG_MLE_STEERING_DATA_SET_OOB_ENABLE should be set to enable setting of steering data out of band.


otThreadGetContextIdReuseDelay#

uint32_t otThreadGetContextIdReuseDelay (otInstance * aInstance)

Get the CONTEXT_ID_REUSE_DELAY parameter used in the Leader role.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The CONTEXT_ID_REUSE_DELAY value.

See Also


otThreadSetContextIdReuseDelay#

void otThreadSetContextIdReuseDelay (otInstance * aInstance, uint32_t aDelay)

Set the CONTEXT_ID_REUSE_DELAY parameter used in the Leader role.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint32_t[in]aDelay

The CONTEXT_ID_REUSE_DELAY value.

Note

  • This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.

See Also


otThreadGetNetworkIdTimeout#

uint8_t otThreadGetNetworkIdTimeout (otInstance * aInstance)

Get the NETWORK_ID_TIMEOUT parameter.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Note

  • This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.

Returns

  • The NETWORK_ID_TIMEOUT value.

See Also


otThreadSetNetworkIdTimeout#

void otThreadSetNetworkIdTimeout (otInstance * aInstance, uint8_t aTimeout)

Set the NETWORK_ID_TIMEOUT parameter.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t[in]aTimeout

The NETWORK_ID_TIMEOUT value.

Note

  • This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.

See Also


otThreadGetRouterUpgradeThreshold#

uint8_t otThreadGetRouterUpgradeThreshold (otInstance * aInstance)

Get the ROUTER_UPGRADE_THRESHOLD parameter used in the REED role.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The ROUTER_UPGRADE_THRESHOLD value.

See Also


otThreadSetRouterUpgradeThreshold#

void otThreadSetRouterUpgradeThreshold (otInstance * aInstance, uint8_t aThreshold)

Set the ROUTER_UPGRADE_THRESHOLD parameter used in the Leader role.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t[in]aThreshold

The ROUTER_UPGRADE_THRESHOLD value.

Note

  • This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.

See Also


otThreadGetChildRouterLinks#

uint8_t otThreadGetChildRouterLinks (otInstance * aInstance)

Get the MLE_CHILD_ROUTER_LINKS parameter used in the REED role.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

This parameter specifies the max number of neighboring routers with which the device (as an FED) will try to establish link.

Returns

  • The MLE_CHILD_ROUTER_LINKS value.

See Also


otThreadSetChildRouterLinks#

otError otThreadSetChildRouterLinks (otInstance * aInstance, uint8_t aChildRouterLinks)

Set the MLE_CHILD_ROUTER_LINKS parameter used in the REED role.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t[in]aChildRouterLinks

The MLE_CHILD_ROUTER_LINKS value.

See Also


otThreadReleaseRouterId#

otError otThreadReleaseRouterId (otInstance * aInstance, uint8_t aRouterId)

Release a Router ID that has been allocated by the device in the Leader role.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t[in]aRouterId

The Router ID to release. Valid range is [0, 62].

Note

  • This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.


otThreadBecomeRouter#

otError otThreadBecomeRouter (otInstance * aInstance)

Attempt to become a router.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Note

  • This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.


otThreadBecomeLeader#

otError otThreadBecomeLeader (otInstance * aInstance)

Become a leader and start a new partition.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Note

  • This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.


otThreadGetRouterDowngradeThreshold#

uint8_t otThreadGetRouterDowngradeThreshold (otInstance * aInstance)

Get the ROUTER_DOWNGRADE_THRESHOLD parameter used in the Router role.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The ROUTER_DOWNGRADE_THRESHOLD value.

See Also


otThreadSetRouterDowngradeThreshold#

void otThreadSetRouterDowngradeThreshold (otInstance * aInstance, uint8_t aThreshold)

Set the ROUTER_DOWNGRADE_THRESHOLD parameter used in the Leader role.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t[in]aThreshold

The ROUTER_DOWNGRADE_THRESHOLD value.

Note

  • This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.

See Also


otThreadGetRouterSelectionJitter#

uint8_t otThreadGetRouterSelectionJitter (otInstance * aInstance)

Get the ROUTER_SELECTION_JITTER parameter used in the REED/Router role.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The ROUTER_SELECTION_JITTER value.

See Also


otThreadSetRouterSelectionJitter#

void otThreadSetRouterSelectionJitter (otInstance * aInstance, uint8_t aRouterJitter)

Set the ROUTER_SELECTION_JITTER parameter used in the REED/Router role.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t[in]aRouterJitter

The ROUTER_SELECTION_JITTER value.

Note

  • This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.

See Also


otThreadGetChildInfoById#

otError otThreadGetChildInfoById (otInstance * aInstance, uint16_t aChildId, otChildInfo * aChildInfo)

Gets diagnostic information for an attached Child by its Child ID or RLOC16.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint16_t[in]aChildId

The Child ID or RLOC16 for the attached child.

otChildInfo *[out]aChildInfo

A pointer to where the child information is placed.


otThreadGetChildInfoByIndex#

otError otThreadGetChildInfoByIndex (otInstance * aInstance, uint16_t aChildIndex, otChildInfo * aChildInfo)

The function retains diagnostic information for an attached Child by the internal table index.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint16_t[in]aChildIndex

The table index.

otChildInfo *[out]aChildInfo

A pointer to where the child information is placed.

See Also

  • otGetMaxAllowedChildren


otThreadGetChildNextIp6Address#

otError otThreadGetChildNextIp6Address (otInstance * aInstance, uint16_t aChildIndex, otChildIp6AddressIterator * aIterator, otIp6Address * aAddress)

Gets the next IPv6 address (using an iterator) for a given child.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint16_t[in]aChildIndex

The child index.

otChildIp6AddressIterator *[inout]aIterator

A pointer to the iterator. On success the iterator will be updated to point to next entry in the list. To get the first IPv6 address the iterator should be set to OT_CHILD_IP6_ADDRESS_ITERATOR_INIT.

otIp6Address *[out]aAddress

A pointer to an IPv6 address where the child's next address is placed (on success).

See Also


otThreadGetRouterIdSequence#

uint8_t otThreadGetRouterIdSequence (otInstance * aInstance)

Get the current Router ID Sequence.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The Router ID Sequence.


otThreadGetMaxRouterId#

uint8_t otThreadGetMaxRouterId (otInstance * aInstance)

The function returns the maximum allowed router ID.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The maximum allowed router ID.


otThreadGetRouterInfo#

otError otThreadGetRouterInfo (otInstance * aInstance, uint16_t aRouterId, otRouterInfo * aRouterInfo)

The function retains diagnostic information for a given Thread Router.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint16_t[in]aRouterId

The router ID or RLOC16 for a given router.

otRouterInfo *[out]aRouterInfo

A pointer to where the router information is placed.


otThreadGetNextCacheEntry#

otError otThreadGetNextCacheEntry (otInstance * aInstance, otCacheEntryInfo * aEntryInfo, otCacheEntryIterator * aIterator)

Gets the next EID cache entry (using an iterator).

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otCacheEntryInfo *[out]aEntryInfo

A pointer to where the EID cache entry information is placed.

otCacheEntryIterator *[inout]aIterator

A pointer to an iterator. It will be updated to point to next entry on success. To get the first entry, initialize the iterator by setting all its fields to zero (e.g., memset the iterator structure to zero).


otThreadGetPskc#

void otThreadGetPskc (otInstance * aInstance, otPskc * aPskc)

Get the Thread PSKc.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otPskc *[out]aPskc

A pointer to an otPskc to return the retrieved Thread PSKc.

See Also


otThreadGetPskcRef#

otPskcRef otThreadGetPskcRef (otInstance * aInstance)

Get Key Reference to Thread PSKc stored.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Requires the build-time feature OPENTHREAD_CONFIG_PLATFORM_KEY_REFERENCES_ENABLE to be enabled.

Returns

  • Key Reference to PSKc

See Also


otThreadSetPskc#

otError otThreadSetPskc (otInstance * aInstance, const otPskc * aPskc)

Set the Thread PSKc.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

const otPskc *[in]aPskc

A pointer to the new Thread PSKc.

Will only succeed when Thread protocols are disabled. A successful call to this function will also invalidate the Active and Pending Operational Datasets in non-volatile memory.

See Also


otThreadSetPskcRef#

otError otThreadSetPskcRef (otInstance * aInstance, otPskcRef aKeyRef)

Set the Key Reference to the Thread PSKc.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otPskcRef[in]aKeyRef

Key Reference to the new Thread PSKc.

Requires the build-time feature OPENTHREAD_CONFIG_PLATFORM_KEY_REFERENCES_ENABLE to be enabled.

Will only succeed when Thread protocols are disabled. Upon success, this will also invalidate the Active and Pending Operational Datasets in non-volatile memory.

See Also


otThreadGetParentPriority#

int8_t otThreadGetParentPriority (otInstance * aInstance)

Get the assigned parent priority.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The assigned parent priority value, -2 means not assigned.

See Also


otThreadSetParentPriority#

otError otThreadSetParentPriority (otInstance * aInstance, int8_t aParentPriority)

Set the parent priority.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

int8_t[in]aParentPriority

The parent priority value.

Note

  • This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.

See Also


otThreadGetMaxChildIpAddresses#

uint8_t otThreadGetMaxChildIpAddresses (otInstance * aInstance)

Gets the maximum number of IP addresses that each MTD child may register with this device as parent.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • The maximum number of IP addresses that each MTD child may register with this device as parent.

See Also


otThreadSetMaxChildIpAddresses#

otError otThreadSetMaxChildIpAddresses (otInstance * aInstance, uint8_t aMaxIpAddresses)

Sets or restores the maximum number of IP addresses that each MTD child may register with this device as parent.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t[in]aMaxIpAddresses

The maximum number of IP addresses that each MTD child may register with this device as parent. 0 to clear the setting and restore the default.

Pass 0 to clear the setting and restore the default.

Available when OPENTHREAD_CONFIG_REFERENCE_DEVICE_ENABLE is enabled.

Note

  • Only used by Thread Test Harness to limit the address registrations of the reference parent in order to test the MTD DUT reaction.

See Also


otThreadRegisterNeighborTableCallback#

void otThreadRegisterNeighborTableCallback (otInstance * aInstance, otNeighborTableCallback aCallback)

Registers a neighbor table callback function.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otNeighborTableCallback[in]aCallback

A pointer to callback handler function.

The provided callback (if non-NULL) will be invoked when there is a change in the neighbor table (e.g., a child or a router neighbor entry is being added/removed or an existing child's mode is changed).

Subsequent calls to this method will overwrite the previous callback. Note that this callback in invoked while the neighbor/child table is being updated and always before the otStateChangedCallback.


otThreadSetCcmEnabled#

void otThreadSetCcmEnabled (otInstance * aInstance, bool aEnabled)

Sets whether the device was commissioned using CCM.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

bool[in]aEnabled

TRUE if the device was commissioned using CCM, FALSE otherwise.

Note

  • This API requires OPENTHREAD_CONFIG_REFERENCE_DEVICE_ENABLE, and is only used by Thread Test Harness to indicate whether this device was commissioned using CCM.


otThreadSetThreadVersionCheckEnabled#

void otThreadSetThreadVersionCheckEnabled (otInstance * aInstance, bool aEnabled)

Sets whether the Security Policy TLV version-threshold for routing (VR field) is enabled.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

bool[in]aEnabled

TRUE to enable Security Policy TLV version-threshold for routing, FALSE otherwise.

Note

  • This API requires OPENTHREAD_CONFIG_REFERENCE_DEVICE_ENABLE, and is only used by Thread Test Harness to indicate that thread protocol version check VR should be skipped.


otThreadGetRouterIdRange#

void otThreadGetRouterIdRange (otInstance * aInstance, uint8_t * aMinRouterId, uint8_t * aMaxRouterId)

Gets the range of router IDs that are allowed to assign to nodes within the thread network.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t *[out]aMinRouterId

The minimum router ID.

uint8_t *[out]aMaxRouterId

The maximum router ID.

Note

  • This API requires OPENTHREAD_CONFIG_REFERENCE_DEVICE_ENABLE, and is only used for test purpose. All the router IDs in the range [aMinRouterId, aMaxRouterId] are allowed.

See Also


otThreadSetRouterIdRange#

otError otThreadSetRouterIdRange (otInstance * aInstance, uint8_t aMinRouterId, uint8_t aMaxRouterId)

Sets the range of router IDs that are allowed to assign to nodes within the thread network.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t[in]aMinRouterId

The minimum router ID.

uint8_t[in]aMaxRouterId

The maximum router ID.

Note

  • This API requires OPENTHREAD_CONFIG_REFERENCE_DEVICE_ENABLE, and is only used for test purpose. All the router IDs in the range [aMinRouterId, aMaxRouterId] are allowed.

See Also


otThreadGetAdvertisementTrickleIntervalMax#

uint32_t otThreadGetAdvertisementTrickleIntervalMax (otInstance * aInstance)

Gets the current Interval Max value used by Advertisement trickle timer.

Parameters
TypeDirectionArgument NameDescription
otInstance *N/AaInstance

This API requires OPENTHREAD_CONFIG_REFERENCE_DEVICE_ENABLE, and is intended for testing only.

Returns

  • The Interval Max of Advertisement trickle timer in milliseconds.


otThreadIsRouterIdAllocated#

bool otThreadIsRouterIdAllocated (otInstance * aInstance, uint8_t aRouterId)

Indicates whether or not a Router ID is currently allocated.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint8_t[in]aRouterId

The router ID to check.


otThreadGetNextHopAndPathCost#

void otThreadGetNextHopAndPathCost (otInstance * aInstance, uint16_t aDestRloc16, uint16_t * aNextHopRloc16, uint8_t * aPathCost)

Gets the next hop and path cost towards a given RLOC16 destination.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint16_t[in]aDestRloc16

The RLOC16 of destination.

uint16_t *[out]aNextHopRloc16

A pointer to return RLOC16 of next hop, 0xfffe if no next hop.

uint8_t *[out]aPathCost

A pointer to return path cost towards destination.

Can be used with either aNextHopRloc16 or aPathCost being NULL indicating caller does not want to get the value.


Macro Definition Documentation#

OT_CHILD_IP6_ADDRESS_ITERATOR_INIT#

#define OT_CHILD_IP6_ADDRESS_ITERATOR_INIT
Value:
0

Initializer for otChildIP6AddressIterator.