Represents Backbone Router configuration.

Public Attributes#

uint16_t

Only used when get Primary Backbone Router information in the Thread Network.

uint16_t

Reregistration Delay (in seconds)

uint32_t

Multicast Listener Registration Timeout (in seconds)

uint8_t

Sequence Number.

Public Attribute Documentation#

mServer16#

uint16_t otBackboneRouterConfig::mServer16

Only used when get Primary Backbone Router information in the Thread Network.


Definition at line 58 of file include/openthread/backbone_router.h

mReregistrationDelay#

uint16_t otBackboneRouterConfig::mReregistrationDelay

Reregistration Delay (in seconds)


Definition at line 59 of file include/openthread/backbone_router.h

mMlrTimeout#

uint32_t otBackboneRouterConfig::mMlrTimeout

Multicast Listener Registration Timeout (in seconds)


Definition at line 60 of file include/openthread/backbone_router.h

mSequenceNumber#

uint8_t otBackboneRouterConfig::mSequenceNumber

Sequence Number.


Definition at line 61 of file include/openthread/backbone_router.h