Represents an iterator to iterate through the Border Router's discovered prefix table.
The fields in this type are opaque (intended for use by OpenThread core only) and therefore should not be accessed or used by caller.
Before using an iterator, it MUST be initialized using otBorderRoutingPrefixTableInitIterator()
.
Public Attribute Documentation#
mPtr1#
const void* otBorderRoutingPrefixTableIterator::mPtr1
Definition at line
84
of file include/openthread/border_routing.h
mPtr2#
const void* otBorderRoutingPrefixTableIterator::mPtr2
Definition at line
85
of file include/openthread/border_routing.h
mData0#
uint32_t otBorderRoutingPrefixTableIterator::mData0
Definition at line
86
of file include/openthread/border_routing.h
mData1#
uint32_t otBorderRoutingPrefixTableIterator::mData1
Definition at line
87
of file include/openthread/border_routing.h
mData2#
uint8_t otBorderRoutingPrefixTableIterator::mData2
Definition at line
88
of file include/openthread/border_routing.h
mData3#
uint8_t otBorderRoutingPrefixTableIterator::mData3
Definition at line
89
of file include/openthread/border_routing.h