Entropy#
This module includes the platform abstraction for entropy generation.
Functions#
otPlatEntropyGet(uint8_t *aOutput, uint16_t aOutputLength)
Fill buffer with entropy.
Function Documentation#
otPlatEntropyGet#
otError otPlatEntropyGet (uint8_t * aOutput, uint16_t aOutputLength)
Fill buffer with entropy.
Parameters
[out] | aOutput | A pointer to where the true random values are placed. Must not be NULL. |
[in] | aOutputLength | Size of |
MUST be implemented using a true random number generator (TRNG).
Definition at line
67
of file include/openthread/platform/entropy.h