Border Agent#

This module includes functions for the Thread Border Agent role.

Modules#

otBorderAgentId

otBorderAgentCounters

Enumerations#

enum
OT_BORDER_AGENT_STATE_DISABLED = 0
OT_BORDER_AGENT_STATE_STOPPED = 1
OT_BORDER_AGENT_STATE_STARTED = 2
OT_BORDER_AGENT_STATE_CONNECTED = 3
OT_BORDER_AGENT_STATE_ACCEPTED = 4
}

Represents Border Agent's Ephemeral Key Manager state.

Typedefs#

typedef struct otBorderAgentId

Represents a Border Agent Identifier.

typedef struct otBorderAgentCounters

Defines Border Agent counters.

Represents Border Agent's Ephemeral Key Manager state.

typedef void(*

Callback function pointer to signal state changes to the Border Agent's Ephemeral Key Manager.

Functions#

otBorderAgentGetCounters(otInstance *aInstance)

Gets the counters of the Thread Border Agent.

bool
otBorderAgentIsActive(otInstance *aInstance)

Indicates whether or not the Border Agent service is active and running.

uint16_t
otBorderAgentGetUdpPort(otInstance *aInstance)

Gets the UDP port of the Thread Border Agent service.

otBorderAgentGetId(otInstance *aInstance, otBorderAgentId *aId)

Gets the randomly generated Border Agent ID.

otBorderAgentSetId(otInstance *aInstance, const otBorderAgentId *aId)

Sets the Border Agent ID.

otBorderAgentEphemeralKeyGetState(otInstance *aInstance)

Gets the state of Border Agent's Ephemeral Key Manager.

void
otBorderAgentEphemeralKeySetEnabled(otInstance *aInstance, bool aEnabled)

Enables/disables the Border Agent's Ephemeral Key Manager.

otBorderAgentEphemeralKeyStart(otInstance *aInstance, const char *aKeyString, uint32_t aTimeout, uint16_t aUdpPort)

Starts using an ephemeral key for a given timeout duration.

void
otBorderAgentEphemeralKeyStop(otInstance *aInstance)

Stops the ephemeral key use and disconnects any session using it.

uint16_t

Gets the UDP port used by Border Agent's Ephemeral Key Manager.

void
otBorderAgentEphemeralKeySetCallback(otInstance *aInstance, otBorderAgentEphemeralKeyCallback aCallback, void *aContext)

Sets the callback function to notify state changes of Border Agent's Ephemeral Key Manager.

const char *
otBorderAgentEphemeralKeyStateToString(otBorderAgentEphemeralKeyState aState)

Converts a given otBorderAgentEphemeralKeyState to a human-readable string.

Macros#

#define

The length of Border Agent/Router ID in bytes.

#define

Minimum length of the ephemeral key string.

#define

Maximum length of the ephemeral key string.

#define

Default ephemeral key timeout interval in milliseconds.

#define

Maximum ephemeral key timeout interval in milliseconds.

Enumeration Documentation#

otBorderAgentEphemeralKeyState#

otBorderAgentEphemeralKeyState

Represents Border Agent's Ephemeral Key Manager state.

Enumerator
OT_BORDER_AGENT_STATE_DISABLED

Ephemeral Key Manager is disabled.

OT_BORDER_AGENT_STATE_STOPPED

Enabled, but no ephemeral key is in use (not set or started).

OT_BORDER_AGENT_STATE_STARTED

Ephemeral key is set. Listening to accept secure connections.

OT_BORDER_AGENT_STATE_CONNECTED

Session is established with an external commissioner candidate.

OT_BORDER_AGENT_STATE_ACCEPTED

Session is established and candidate is accepted as full commissioner.


Typedef Documentation#

otBorderAgentId#

typedef struct otBorderAgentId otBorderAgentId

Represents a Border Agent Identifier.


otBorderAgentCounters#

typedef struct otBorderAgentCounters otBorderAgentCounters

Defines Border Agent counters.

The mEpskc related counters require OPENTHREAD_CONFIG_BORDER_AGENT_EPHEMERAL_KEY_ENABLE.


otBorderAgentEphemeralKeyState#

typedef enum otBorderAgentEphemeralKeyState otBorderAgentEphemeralKeyState

Represents Border Agent's Ephemeral Key Manager state.


otBorderAgentEphemeralKeyCallback#

typedef void(* otBorderAgentEphemeralKeyCallback) (void *aContext) )(void *aContext)

Callback function pointer to signal state changes to the Border Agent's Ephemeral Key Manager.

Parameters
TypeDirectionArgument NameDescription
[in]aContext

A pointer to an arbitrary context (provided when callback is set).

This callback is invoked whenever the otBorderAgentEphemeralKeyGetState() gets changed.

Any OpenThread API, including otBorderAgent APIs, can be safely called from this callback.


Function Documentation#

otBorderAgentGetCounters#

const otBorderAgentCounters * otBorderAgentGetCounters (otInstance * aInstance)

Gets the counters of the Thread Border Agent.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • A pointer to the Border Agent counters.


otBorderAgentIsActive#

bool otBorderAgentIsActive (otInstance * aInstance)

Indicates whether or not the Border Agent service is active and running.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

While the Border Agent is active, external commissioner candidates can try to connect to and establish secure DTLS sessions with the Border Agent using PSKc. A connected commissioner can then petition to become a full commissioner.

If OPENTHREAD_CONFIG_BORDER_AGENT_EPHEMERAL_KEY_ENABLE is enabled, independent and separate DTLS transport and sessions are used for the ephemeral key. Therefore, the ephemeral key and Border Agent service can be enabled and used in parallel.


otBorderAgentGetUdpPort#

uint16_t otBorderAgentGetUdpPort (otInstance * aInstance)

Gets the UDP port of the Thread Border Agent service.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Returns

  • UDP port of the Border Agent.


otBorderAgentGetId#

otError otBorderAgentGetId (otInstance * aInstance, otBorderAgentId * aId)

Gets the randomly generated Border Agent ID.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otBorderAgentId *[out]aId

A pointer to buffer to receive the ID.

Requires OPENTHREAD_CONFIG_BORDER_AGENT_ID_ENABLE.

The ID is saved in persistent storage and survives reboots. The typical use case of the ID is to be published in the MeshCoP mDNS service as the id TXT value for the client to identify this Border Router/Agent device.

See Also


otBorderAgentSetId#

otError otBorderAgentSetId (otInstance * aInstance, const otBorderAgentId * aId)

Sets the Border Agent ID.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

const otBorderAgentId *[out]aId

A pointer to the Border Agent ID.

Requires OPENTHREAD_CONFIG_BORDER_AGENT_ID_ENABLE.

The Border Agent ID will be saved in persistent storage and survive reboots. It's required to set the ID only once after factory reset. If the ID has never been set by calling this function, a random ID will be generated and returned when otBorderAgentGetId is called.

See Also


otBorderAgentEphemeralKeyGetState#

otBorderAgentEphemeralKeyState otBorderAgentEphemeralKeyGetState (otInstance * aInstance)

Gets the state of Border Agent's Ephemeral Key Manager.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Requires OPENTHREAD_CONFIG_BORDER_AGENT_EPHEMERAL_KEY_ENABLE.

Returns

  • The current state of Ephemeral Key Manager.


otBorderAgentEphemeralKeySetEnabled#

void otBorderAgentEphemeralKeySetEnabled (otInstance * aInstance, bool aEnabled)

Enables/disables the Border Agent's Ephemeral Key Manager.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

bool[in]aEnabled

Whether to enable or disable the Ephemeral Key Manager.

Requires OPENTHREAD_CONFIG_BORDER_AGENT_EPHEMERAL_KEY_ENABLE.

If this function is called to disable, while an an ephemeral key is in use, the ephemeral key use will be stopped (as if otBorderAgentEphemeralKeyStop() is called).


otBorderAgentEphemeralKeyStart#

otError otBorderAgentEphemeralKeyStart (otInstance * aInstance, const char * aKeyString, uint32_t aTimeout, uint16_t aUdpPort)

Starts using an ephemeral key for a given timeout duration.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

const char *[in]aKeyString

The ephemeral key.

uint32_t[in]aTimeout

The timeout duration, in milliseconds, to use the ephemeral key. If zero, the default OT_BORDER_AGENT_DEFAULT_EPHEMERAL_KEY_TIMEOUT value is used. If the timeout value is larger than OT_BORDER_AGENT_MAX_EPHEMERAL_KEY_TIMEOUT, the maximum value is used instead.

uint16_t[in]aUdpPort

The UDP port to use with the ephemeral key. If the UDP port is zero, an ephemeral port will be used. otBorderAgentEphemeralKeyGetUdpPort() returns the current UDP port being used.

Requires OPENTHREAD_CONFIG_BORDER_AGENT_EPHEMERAL_KEY_ENABLE.

An ephemeral key can only be set when otBorderAgentEphemeralKeyGetState() is OT_BORDER_AGENT_STATE_STOPPED, i.e., enabled but not yet started. Otherwise, OT_ERROR_INVALID_STATE is returned. This means that setting the ephemeral key again while a previously set key is still in use will fail. Callers can stop the previous key by calling otBorderAgentEphemeralKeyStop() before starting with a new key.

The Ephemeral Key Manager and the Border Agent service (which uses PSKc) can be enabled and used in parallel, as they use independent and separate DTLS transport and sessions.

The given aKeyString is used directly as the ephemeral PSK (excluding the trailing null \0 character). Its length must be between OT_BORDER_AGENT_MIN_EPHEMERAL_KEY_LENGTH and OT_BORDER_AGENT_MAX_EPHEMERAL_KEY_LENGTH, inclusive. Otherwise OT_ERROR_INVALID_ARGS is returned.

When successfully set, the ephemeral key can be used only once by an external commissioner candidate to establish a secure session. After the commissioner candidate disconnects, the use of the ephemeral key is stopped. If the timeout expires, the use of the ephemeral key is stopped, and any connected session using the key is immediately disconnected.

The Ephemeral Key Manager limits the number of failed DTLS connections to 10 attempts. After the 10th failed attempt, the use of the ephemeral key is automatically stopped (even if the timeout has not yet expired).


otBorderAgentEphemeralKeyStop#

void otBorderAgentEphemeralKeyStop (otInstance * aInstance)

Stops the ephemeral key use and disconnects any session using it.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

Requires OPENTHREAD_CONFIG_BORDER_AGENT_EPHEMERAL_KEY_ENABLE.

If there is no ephemeral key in use, calling this function has no effect.


otBorderAgentEphemeralKeyGetUdpPort#

uint16_t otBorderAgentEphemeralKeyGetUdpPort (otInstance * aInstance)

Gets the UDP port used by Border Agent's Ephemeral Key Manager.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

Requires OPENTHREAD_CONFIG_BORDER_AGENT_EPHEMERAL_KEY_ENABLE.

The port is applicable if an ephemeral key is in use, i.e., the state is not OT_BORDER_AGENT_STATE_DISABLED or OT_BORDER_AGENT_STATE_STOPPED.

Returns

  • The UDP port being used by Border Agent's Ephemeral Key Manager (when active).


otBorderAgentEphemeralKeySetCallback#

void otBorderAgentEphemeralKeySetCallback (otInstance * aInstance, otBorderAgentEphemeralKeyCallback aCallback, void * aContext)

Sets the callback function to notify state changes of Border Agent's Ephemeral Key Manager.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

The OpenThread instance.

otBorderAgentEphemeralKeyCallback[in]aCallback

The callback function pointer.

void *[in]aContext

The arbitrary context to use with callback.

Requires OPENTHREAD_CONFIG_BORDER_AGENT_EPHEMERAL_KEY_ENABLE.

A subsequent call to this function will replace any previously set callback.


otBorderAgentEphemeralKeyStateToString#

const char * otBorderAgentEphemeralKeyStateToString (otBorderAgentEphemeralKeyState aState)

Converts a given otBorderAgentEphemeralKeyState to a human-readable string.

Parameters
TypeDirectionArgument NameDescription
otBorderAgentEphemeralKeyState[in]aState

The state to convert.

Returns

  • Human-readable string corresponding to aState.


Macro Definition Documentation#

OT_BORDER_AGENT_ID_LENGTH#

#define OT_BORDER_AGENT_ID_LENGTH
Value:
(16)

The length of Border Agent/Router ID in bytes.


OT_BORDER_AGENT_MIN_EPHEMERAL_KEY_LENGTH#

#define OT_BORDER_AGENT_MIN_EPHEMERAL_KEY_LENGTH
Value:
(6)

Minimum length of the ephemeral key string.


OT_BORDER_AGENT_MAX_EPHEMERAL_KEY_LENGTH#

#define OT_BORDER_AGENT_MAX_EPHEMERAL_KEY_LENGTH
Value:
(32)

Maximum length of the ephemeral key string.


OT_BORDER_AGENT_DEFAULT_EPHEMERAL_KEY_TIMEOUT#

#define OT_BORDER_AGENT_DEFAULT_EPHEMERAL_KEY_TIMEOUT
Value:
(2 * 60 * 1000u)

Default ephemeral key timeout interval in milliseconds.


OT_BORDER_AGENT_MAX_EPHEMERAL_KEY_TIMEOUT#

#define OT_BORDER_AGENT_MAX_EPHEMERAL_KEY_TIMEOUT
Value:
(10 * 60 * 1000u)

Maximum ephemeral key timeout interval in milliseconds.