Jam Detection#
This module includes functions for signal jamming detection feature.
The functions in this module are available when jam-detection feature (OPENTHREAD_CONFIG_JAM_DETECTION_ENABLE
) is enabled.
Typedefs#
Pointer is called if signal jam detection is enabled and a jam is detected.
Functions#
Set the Jam Detection RSSI Threshold (in dBm).
Get the Jam Detection RSSI Threshold (in dBm).
Set the Jam Detection Detection Window (in seconds).
Get the Jam Detection Detection Window (in seconds).
Set the Jam Detection Busy Period (in seconds).
Get the Jam Detection Busy Period (in seconds)
Start the jamming detection.
Stop the jamming detection.
Get the Jam Detection Status (enabled/disabled)
Get the Jam Detection State.
Get the current history bitmap.
Typedef Documentation#
otJamDetectionCallback#
typedef void(* otJamDetectionCallback) (bool aJamState, void *aContext) )(bool aJamState, void *aContext)
Pointer is called if signal jam detection is enabled and a jam is detected.
Type | Direction | Argument Name | Description |
---|---|---|---|
[in] | aJamState | Current jam state ( | |
[in] | aContext | A pointer to application-specific context. |
Function Documentation#
otJamDetectionSetRssiThreshold#
otError otJamDetectionSetRssiThreshold (otInstance * aInstance, int8_t aRssiThreshold)
Set the Jam Detection RSSI Threshold (in dBm).
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
int8_t | [in] | aRssiThreshold | The RSSI threshold. |
otJamDetectionGetRssiThreshold#
int8_t otJamDetectionGetRssiThreshold (otInstance * aInstance)
Get the Jam Detection RSSI Threshold (in dBm).
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
Returns
The Jam Detection RSSI Threshold.
otJamDetectionSetWindow#
otError otJamDetectionSetWindow (otInstance * aInstance, uint8_t aWindow)
Set the Jam Detection Detection Window (in seconds).
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
uint8_t | [in] | aWindow | The Jam Detection window (valid range is 1 to 63) |
otJamDetectionGetWindow#
uint8_t otJamDetectionGetWindow (otInstance * aInstance)
Get the Jam Detection Detection Window (in seconds).
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
Returns
The Jam Detection Window.
otJamDetectionSetBusyPeriod#
otError otJamDetectionSetBusyPeriod (otInstance * aInstance, uint8_t aBusyPeriod)
Set the Jam Detection Busy Period (in seconds).
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
uint8_t | [in] | aBusyPeriod | The Jam Detection busy period (should be non-zero and less than or equal to Jam Detection Window) |
The number of aggregate seconds within the detection window where the RSSI must be above threshold to trigger detection.
otJamDetectionGetBusyPeriod#
uint8_t otJamDetectionGetBusyPeriod (otInstance * aInstance)
Get the Jam Detection Busy Period (in seconds)
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
Returns
The Jam Detection Busy Period.
otJamDetectionStart#
otError otJamDetectionStart (otInstance * aInstance, otJamDetectionCallback aCallback, void * aContext)
Start the jamming detection.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
otJamDetectionCallback | [in] | aCallback | A pointer to a function called to notify of jamming state change. |
void * | [in] | aContext | A pointer to application-specific context. |
otJamDetectionStop#
otError otJamDetectionStop (otInstance * aInstance)
Stop the jamming detection.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
otJamDetectionIsEnabled#
bool otJamDetectionIsEnabled (otInstance * aInstance)
Get the Jam Detection Status (enabled/disabled)
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
Returns
The Jam Detection status (true if enabled, false otherwise).
otJamDetectionGetState#
bool otJamDetectionGetState (otInstance * aInstance)
Get the Jam Detection State.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
Returns
The Jam Detection state (
true
jam is detected, ‘false’ otherwise).
otJamDetectionGetHistoryBitmap#
uint64_t otJamDetectionGetHistoryBitmap (otInstance * aInstance)
Get the current history bitmap.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
This value provides information about current state of jamming detection module for monitoring/debugging purpose. It returns a 64-bit value where each bit corresponds to one second interval starting with bit 0 for the most recent interval and bit 63 for the oldest intervals (63 sec earlier). The bit is set to 1 if the jamming detection module observed/detected high signal level during the corresponding one second interval.
Returns
The current history bitmap.