You are viewing documentation for version:
Represents a received IEEE 802.15.4 Beacon.
Public Attributes#
IEEE 802.15.4 Extended Address.
bool
Native Commissioner flag.
bool
Result from MLE Discovery.
Public Attribute Documentation#
mExtAddress#
otExtAddress otActiveScanResult::mExtAddress
IEEE 802.15.4 Extended Address.
mNetworkName#
otNetworkName otActiveScanResult::mNetworkName
Thread Network Name.
mExtendedPanId#
otExtendedPanId otActiveScanResult::mExtendedPanId
Thread Extended PAN ID.
mSteeringData#
otSteeringData otActiveScanResult::mSteeringData
Steering Data.
mPanId#
uint16_t otActiveScanResult::mPanId
IEEE 802.15.4 PAN ID.
mJoinerUdpPort#
uint16_t otActiveScanResult::mJoinerUdpPort
Joiner UDP Port.
mChannel#
uint8_t otActiveScanResult::mChannel
IEEE 802.15.4 Channel.
mRssi
int8_t otActiveScanResult::mRssi
RSSI (dBm)
mLqi#
uint8_t otActiveScanResult::mLqi
LQI.
mVersion#
unsigned int otActiveScanResult::mVersion
Version.
mIsNative#
bool otActiveScanResult::mIsNative
Native Commissioner flag.
mDiscover#
bool otActiveScanResult::mDiscover
Result from MLE Discovery.
mIsJoinable#
bool otActiveScanResult::mIsJoinable
Joining Permitted flag.