Border Agent#
This module includes functions for the Thread Border Agent role.
Modules#
otBorderAgentMeshCoPServiceTxtData
Enumerations#
Represents Border Agent's Ephemeral Key Manager state.
Typedefs#
Represents a Border Agent Identifier.
Defines Border Agent counters.
Represents information about a Border Agent session.
Represents an iterator for Border Agent sessions.
Represents the Border Agent MeshCoP Service TXT data.
This callback informs the application of the changes in the state of the MeshCoP service.
Represents Border Agent's Ephemeral Key Manager state.
Callback function pointer to signal state changes to the Border Agent's Ephemeral Key Manager.
Functions#
Enables or disables the Border Agent service on the device.
Indicates whether or not the Border Agent service is enabled.
Indicates whether or not the Border Agent service is enabled and also active.
Gets the UDP port of the Thread Border Agent service.
Sets the callback function used by the Border Agent to notify of any changes to the state of the MeshCoP service.
Gets the MeshCoP service TXT data.
Sets the base name to construct the service instance name used when advertising the mDNS _meshcop._udp service by the Border Agent. 
Sets the vendor extra TXT data to be included when the Border Agent advertises the mDNS _meshcop._udp service. 
Gets the randomly generated Border Agent ID.
Sets the Border Agent ID.
Initializes a session iterator.
Retrieves the next Border Agent session information.
Gets the counters of the Thread Border Agent.
Gets the state of Border Agent's Ephemeral Key Manager.
Enables/disables the Border Agent's Ephemeral Key Manager.
Starts using an ephemeral key for a given timeout duration.
Stops the ephemeral key use and disconnects any session using it.
Gets the UDP port used by Border Agent's Ephemeral Key Manager.
Sets the callback function to notify state changes of Border Agent's Ephemeral Key Manager.
Converts a given otBorderAgentEphemeralKeyState to a human-readable string. 
Macros#
The length of Border Agent/Router ID in bytes.
Maximum length of the OT core generated MeshCoP Service TXT data.
Maximum string length of base name used in otBorderAgentSetMeshCoPServiceBaseName(). 
Minimum length of the ephemeral key string.
Maximum length of the ephemeral key string.
Default ephemeral key timeout interval in milliseconds.
Maximum ephemeral key timeout interval in milliseconds.
Enumeration Documentation#
otBorderAgentEphemeralKeyState#
otBorderAgentEphemeralKeyState
Represents Border Agent's Ephemeral Key Manager state.
| Enumerator | |
|---|---|
| OT_BORDER_AGENT_STATE_DISABLED | Ephemeral Key Manager is disabled. | 
| OT_BORDER_AGENT_STATE_STOPPED | Enabled, but no ephemeral key is in use (not set or started). | 
| OT_BORDER_AGENT_STATE_STARTED | Ephemeral key is set. Listening to accept secure connections. | 
| OT_BORDER_AGENT_STATE_CONNECTED | Session is established with an external commissioner candidate. | 
| OT_BORDER_AGENT_STATE_ACCEPTED | Session is established and candidate is accepted as full commissioner. | 
Typedef Documentation#
otBorderAgentId#
typedef struct otBorderAgentId otBorderAgentId
Represents a Border Agent Identifier.
otBorderAgentCounters#
typedef struct otBorderAgentCounters otBorderAgentCounters
Defines Border Agent counters.
The mEpskc related counters require OPENTHREAD_CONFIG_BORDER_AGENT_EPHEMERAL_KEY_ENABLE. 
otBorderAgentSessionInfo#
typedef struct otBorderAgentSessionInfo otBorderAgentSessionInfo
Represents information about a Border Agent session.
This structure is populated by otBorderAgentGetNextSessionInfo() during iteration over the list of sessions using an otBorderAgentSessionIterator.
To ensure consistent mLifetime calculations, the iterator's initialization time is stored within the iterator, and each session's mLifetime is calculated relative to this time. 
otBorderAgentSessionIterator#
typedef struct otBorderAgentSessionIterator otBorderAgentSessionIterator
Represents an iterator for Border Agent sessions.
The caller MUST NOT access or update the fields in this struct. It is intended for OpenThread internal use only.
otBorderAgentMeshCoPServiceTxtData#
typedef struct otBorderAgentMeshCoPServiceTxtData otBorderAgentMeshCoPServiceTxtData
Represents the Border Agent MeshCoP Service TXT data.
otBorderAgentMeshCoPServiceChangedCallback#
typedef void(* otBorderAgentMeshCoPServiceChangedCallback) (void *aContext) )(void *aContext)
This callback informs the application of the changes in the state of the MeshCoP service.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| [in] | aContext | A pointer to application-specific context. | 
In specific, the 'state' includes the MeshCoP TXT data originated from the Thread network and whether the Border Agent is Active (which can be obtained by otBorderAgentIsActive).
otBorderAgentEphemeralKeyState#
typedef enum otBorderAgentEphemeralKeyState otBorderAgentEphemeralKeyState
Represents Border Agent's Ephemeral Key Manager state.
otBorderAgentEphemeralKeyCallback#
typedef void(* otBorderAgentEphemeralKeyCallback) (void *aContext) )(void *aContext)
Callback function pointer to signal state changes to the Border Agent's Ephemeral Key Manager.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| [in] | aContext | A pointer to an arbitrary context (provided when callback is set). | 
This callback is invoked whenever the otBorderAgentEphemeralKeyGetState() gets changed.
Any OpenThread API, including otBorderAgent APIs, can be safely called from this callback.
Function Documentation#
otBorderAgentSetEnabled#
void otBorderAgentSetEnabled (otInstance * aInstance, bool aEnabled)
Enables or disables the Border Agent service on the device.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance. | 
| bool | [in] | aEnabled | A boolean to indicate whether to to enable (TRUE), or disable (FALSE). | 
By default, the Border Agent service is enabled when the OPENTHREAD_CONFIG_BORDER_AGENT_ENABLE feature is used. This function allows higher-layer code to explicitly control its state. This can be useful in scenarios such as:
- The higher-layer code wishes to delay the start of the Border Agent service (and its mDNS advertisement of the - _meshcop._udpservice on the infrastructure link). This allows time to prepare or determine vendor-specific TXT data entries for inclusion.
- Unit tests or test scripts might disable the Border Agent service to prevent it from interfering with specific test steps. For example, tests validating mDNS or DNS-SD functionality may disable the Border Agent to prevent its registration of the MeshCoP service. 
otBorderAgentIsEnabled#
bool otBorderAgentIsEnabled (otInstance * aInstance)
Indicates whether or not the Border Agent service is enabled.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance. | 
otBorderAgentIsActive#
bool otBorderAgentIsActive (otInstance * aInstance)
Indicates whether or not the Border Agent service is enabled and also active.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
While the Border Agent is active, external commissioner candidates can try to connect to and establish secure DTLS sessions with the Border Agent using PSKc. A connected commissioner can then petition to become a full commissioner.
If OPENTHREAD_CONFIG_BORDER_AGENT_EPHEMERAL_KEY_ENABLE is enabled, independent and separate DTLS transport and sessions are used for the ephemeral key. Therefore, the ephemeral key and Border Agent service can be enabled and used in parallel.
otBorderAgentGetUdpPort#
uint16_t otBorderAgentGetUdpPort (otInstance * aInstance)
Gets the UDP port of the Thread Border Agent service.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
Returns
- UDP port of the Border Agent. 
otBorderAgentSetMeshCoPServiceChangedCallback#
void otBorderAgentSetMeshCoPServiceChangedCallback (otInstance * aInstance, otBorderAgentMeshCoPServiceChangedCallback aCallback, void * aContext)
Sets the callback function used by the Border Agent to notify of any changes to the state of the MeshCoP service.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
| otBorderAgentMeshCoPServiceChangedCallback | [in] | aCallback | The callback to be invoked when there are any changes of the MeshCoP service. | 
| void * | [in] | aContext | A pointer to application-specific context. | 
The callback is invoked when the 'Is Active' state of the Border Agent or the MeshCoP service TXT data values change. For example, it is invoked when the network name or the extended PAN ID changes and passes the updated encoded TXT data to the application layer.
This callback is invoked once right after this API is called to provide initial states of the MeshCoP service.
otBorderAgentGetMeshCoPServiceTxtData#
otError otBorderAgentGetMeshCoPServiceTxtData (otInstance * aInstance, otBorderAgentMeshCoPServiceTxtData * aTxtData)
Gets the MeshCoP service TXT data.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
| otBorderAgentMeshCoPServiceTxtData * | [out] | aTxtData | A pointer to a MeshCoP Service TXT data struct to get the data. | 
The generated TXT data includes a subset of keys (depending on the device's current state and whether features are enabled) as specified in the documentation of the OT_BORDER_AGENT_MESHCOP_SERVICE_TXT_DATA_MAX_LENGTH constant. Notably, if OPENTHREAD_CONFIG_BORDER_AGENT_MESHCOP_SERVICE_ENABLE is enabled and otBorderAgentSetVendorTxtData() was used to set extra vendor-specific TXT data bytes, those vendor-specified TXT data bytes are NOT included in the TXT data returned by this function.
otBorderAgentSetMeshCoPServiceBaseName#
otError otBorderAgentSetMeshCoPServiceBaseName (otInstance * aInstance, const char * aBaseName)
Sets the base name to construct the service instance name used when advertising the mDNS _meshcop._udp service by the Border Agent. 
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance. | 
| const char * | [in] | aBaseName | The base name to use (MUST not be NULL). | 
Requires the OPENTHREAD_CONFIG_BORDER_AGENT_MESHCOP_SERVICE_ENABLE feature.
The name can also be configured using the OPENTHREAD_CONFIG_BORDER_AGENT_MESHCOP_SERVICE_BASE_NAME configuration option (which is the recommended way to specify this name). This API is provided for projects where the name needs to be set after device initialization and at run-time.
Per the Thread specification, the service instance should be a user-friendly name identifying the device model or product. A recommended format is "VendorName ProductName".
To construct the full name and ensure name uniqueness, the OpenThread Border Agent module will append the Extended Address of the device (as 16-character hex digits) to the given base name.
Note that the same name will be used for the ephemeral key service _meshcop-e._udp when the ephemeral key feature is enabled and used.
otBorderAgentSetVendorTxtData#
void otBorderAgentSetVendorTxtData (otInstance * aInstance, const uint8_t * aVendorData, uint16_t aVendorDataLength)
Sets the vendor extra TXT data to be included when the Border Agent advertises the mDNS _meshcop._udp service. 
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance. | 
| const uint8_t * | [in] | aVendorData | A pointer to the buffer containing the vendor TXT data. | 
| uint16_t | [in] | aVendorDataLength | The length of  | 
Requires the OPENTHREAD_CONFIG_BORDER_AGENT_MESHCOP_SERVICE_ENABLE feature.
The provided aVendorData bytes are appended as they appear in the buffer to the end of the TXT data generated by the Border Agent itself, and are then included in the advertised mDNS _meshcop._udp service.
This function itself does not perform any validation of the format of the provided aVendorData. Therefore, the caller MUST ensure it is formatted properly. Per the Thread specification, vendor-specific Key-Value TXT data pairs use TXT keys starting with 'v'. For example, vn for vendor name and generally v*.
The OpenThread stack will create and retain its own copy of the bytes in aVendorData. So, the buffer passed to this function does not need to persist beyond the scope of the call.
The vendor TXT data can be set at any time while the Border Agent is in any state. If there is a change from the previously set value, it will trigger an update of the registered mDNS service to advertise the new TXT data.
otBorderAgentGetId#
otError otBorderAgentGetId (otInstance * aInstance, otBorderAgentId * aId)
Gets the randomly generated Border Agent ID.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
| otBorderAgentId * | [out] | aId | A pointer to buffer to receive the ID. | 
Requires OPENTHREAD_CONFIG_BORDER_AGENT_ID_ENABLE.
The ID is saved in persistent storage and survives reboots. The typical use case of the ID is to be published in the MeshCoP mDNS service as the id TXT value for the client to identify this Border Router/Agent device.
See Also
otBorderAgentSetId#
otError otBorderAgentSetId (otInstance * aInstance, const otBorderAgentId * aId)
Sets the Border Agent ID.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
| const otBorderAgentId * | [out] | aId | A pointer to the Border Agent ID. | 
Requires OPENTHREAD_CONFIG_BORDER_AGENT_ID_ENABLE.
The Border Agent ID will be saved in persistent storage and survive reboots. It's required to set the ID only once after factory reset. If the ID has never been set by calling this function, a random ID will be generated and returned when otBorderAgentGetId is called.
See Also
otBorderAgentInitSessionIterator#
void otBorderAgentInitSessionIterator (otInstance * aInstance, otBorderAgentSessionIterator * aIterator)
Initializes a session iterator.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
| otBorderAgentSessionIterator * | [in] | aIterator | The iterator to initialize. | 
An iterator MUST be initialized before being used in otBorderAgentGetNextSessionInfo(). A previously initialized iterator can be re-initialized to start from the beginning of the session list.
otBorderAgentGetNextSessionInfo#
otError otBorderAgentGetNextSessionInfo (otBorderAgentSessionIterator * aIterator, otBorderAgentSessionInfo * aSessionInfo)
Retrieves the next Border Agent session information.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otBorderAgentSessionIterator * | [in] | aIterator | The iterator to use. | 
| otBorderAgentSessionInfo * | [out] | aSessionInfo | A pointer to an  | 
otBorderAgentGetCounters#
const otBorderAgentCounters * otBorderAgentGetCounters (otInstance * aInstance)
Gets the counters of the Thread Border Agent.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
Returns
- A pointer to the Border Agent counters. 
otBorderAgentEphemeralKeyGetState#
otBorderAgentEphemeralKeyState otBorderAgentEphemeralKeyGetState (otInstance * aInstance)
Gets the state of Border Agent's Ephemeral Key Manager.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
Requires OPENTHREAD_CONFIG_BORDER_AGENT_EPHEMERAL_KEY_ENABLE.
Returns
- The current state of Ephemeral Key Manager. 
otBorderAgentEphemeralKeySetEnabled#
void otBorderAgentEphemeralKeySetEnabled (otInstance * aInstance, bool aEnabled)
Enables/disables the Border Agent's Ephemeral Key Manager.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance. | 
| bool | [in] | aEnabled | Whether to enable or disable the Ephemeral Key Manager. | 
Requires OPENTHREAD_CONFIG_BORDER_AGENT_EPHEMERAL_KEY_ENABLE.
If this function is called to disable, while an an ephemeral key is in use, the ephemeral key use will be stopped (as if otBorderAgentEphemeralKeyStop() is called).
otBorderAgentEphemeralKeyStart#
otError otBorderAgentEphemeralKeyStart (otInstance * aInstance, const char * aKeyString, uint32_t aTimeout, uint16_t aUdpPort)
Starts using an ephemeral key for a given timeout duration.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance. | 
| const char * | [in] | aKeyString | The ephemeral key. | 
| uint32_t | [in] | aTimeout | The timeout duration, in milliseconds, to use the ephemeral key. If zero, the default  | 
| uint16_t | [in] | aUdpPort | The UDP port to use with the ephemeral key. If the UDP port is zero, an ephemeral port will be used.  | 
Requires OPENTHREAD_CONFIG_BORDER_AGENT_EPHEMERAL_KEY_ENABLE.
An ephemeral key can only be set when otBorderAgentEphemeralKeyGetState() is OT_BORDER_AGENT_STATE_STOPPED, i.e., enabled but not yet started. Otherwise, OT_ERROR_INVALID_STATE is returned. This means that setting the ephemeral key again while a previously set key is still in use will fail. Callers can stop the previous key by calling otBorderAgentEphemeralKeyStop() before starting with a new key.
The Ephemeral Key Manager and the Border Agent service (which uses PSKc) can be enabled and used in parallel, as they use independent and separate DTLS transport and sessions.
The given aKeyString is used directly as the ephemeral PSK (excluding the trailing null \0 character). Its length must be between OT_BORDER_AGENT_MIN_EPHEMERAL_KEY_LENGTH and OT_BORDER_AGENT_MAX_EPHEMERAL_KEY_LENGTH, inclusive. Otherwise OT_ERROR_INVALID_ARGS is returned.
When successfully set, the ephemeral key can be used only once by an external commissioner candidate to establish a secure session. After the commissioner candidate disconnects, the use of the ephemeral key is stopped. If the timeout expires, the use of the ephemeral key is stopped, and any connected session using the key is immediately disconnected.
The Ephemeral Key Manager limits the number of failed DTLS connections to 10 attempts. After the 10th failed attempt, the use of the ephemeral key is automatically stopped (even if the timeout has not yet expired).
otBorderAgentEphemeralKeyStop#
void otBorderAgentEphemeralKeyStop (otInstance * aInstance)
Stops the ephemeral key use and disconnects any session using it.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance. | 
Requires OPENTHREAD_CONFIG_BORDER_AGENT_EPHEMERAL_KEY_ENABLE.
If there is no ephemeral key in use, calling this function has no effect.
otBorderAgentEphemeralKeyGetUdpPort#
uint16_t otBorderAgentEphemeralKeyGetUdpPort (otInstance * aInstance)
Gets the UDP port used by Border Agent's Ephemeral Key Manager.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. | 
Requires OPENTHREAD_CONFIG_BORDER_AGENT_EPHEMERAL_KEY_ENABLE.
The port is applicable if an ephemeral key is in use, i.e., the state is not OT_BORDER_AGENT_STATE_DISABLED or OT_BORDER_AGENT_STATE_STOPPED.
Returns
- The UDP port being used by Border Agent's Ephemeral Key Manager (when active). 
otBorderAgentEphemeralKeySetCallback#
void otBorderAgentEphemeralKeySetCallback (otInstance * aInstance, otBorderAgentEphemeralKeyCallback aCallback, void * aContext)
Sets the callback function to notify state changes of Border Agent's Ephemeral Key Manager.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance. | 
| otBorderAgentEphemeralKeyCallback | [in] | aCallback | The callback function pointer. | 
| void * | [in] | aContext | The arbitrary context to use with callback. | 
Requires OPENTHREAD_CONFIG_BORDER_AGENT_EPHEMERAL_KEY_ENABLE.
A subsequent call to this function will replace any previously set callback.
otBorderAgentEphemeralKeyStateToString#
const char * otBorderAgentEphemeralKeyStateToString (otBorderAgentEphemeralKeyState aState)
Converts a given otBorderAgentEphemeralKeyState to a human-readable string. 
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otBorderAgentEphemeralKeyState | [in] | aState | The state to convert. | 
Returns
- Human-readable string corresponding to - aState.