Represents the local and peer IPv6 socket addresses.
Public Attributes#
The local IPv6 address.
The peer IPv6 address.
The local transport-layer port.
The peer transport-layer port.
The IPv6 Hop Limit value.
The ECN status of the packet, represented as in the IPv6 header.
TRUE if packets sent/received via host interface, FALSE otherwise.
TRUE to allow IPv6 Hop Limit 0 in mHopLimit, FALSE otherwise. 
TRUE to allow looping back multicast, FALSE otherwise.
Public Attribute Documentation#
mHopLimit#
uint8_t otMessageInfo::mHopLimit
The IPv6 Hop Limit value.
Only applies if mAllowZeroHopLimit is FALSE. If 0, IPv6 Hop Limit is default value OPENTHREAD_CONFIG_IP6_HOP_LIMIT_DEFAULT. Otherwise, specifies the IPv6 Hop Limit. 
mIsHostInterface#
bool otMessageInfo::mIsHostInterface
TRUE if packets sent/received via host interface, FALSE otherwise.
mAllowZeroHopLimit#
bool otMessageInfo::mAllowZeroHopLimit
TRUE to allow IPv6 Hop Limit 0 in mHopLimit, FALSE otherwise. 
mMulticastLoop#
bool otMessageInfo::mMulticastLoop
TRUE to allow looping back multicast, FALSE otherwise.