You are viewing documentation for version:
Includes the statistics of SRP server responses. 
Public Attributes#
uint32_t
The number of successful responses. 
uint32_t
The number of server failure responses. 
uint32_t
The number of format error responses. 
uint32_t
The number of 'name exists' responses. 
uint32_t
The number of refused responses. 
uint32_t
The number of other responses. 
Public Attribute Documentation#
mSuccess#
uint32_t otSrpServerResponseCounters::mSuccess
The number of successful responses. 
mServerFailure#
uint32_t otSrpServerResponseCounters::mServerFailure
The number of server failure responses. 
mFormatError#
uint32_t otSrpServerResponseCounters::mFormatError
The number of format error responses. 
mNameExists#
uint32_t otSrpServerResponseCounters::mNameExists
The number of 'name exists' responses. 
mRefused#
uint32_t otSrpServerResponseCounters::mRefused
The number of refused responses. 
mOther#
uint32_t otSrpServerResponseCounters::mOther
The number of other responses.