Alarm#
This module includes the platform abstraction for the alarm service.
Functions#
Set the alarm to fire at aDt microseconds after aT0. 
Stop the alarm.
Get the current time.
Signal that the alarm has fired.
Set the alarm to fire at aDt milliseconds after aT0. 
Stop the alarm.
Get the current time.
Signal that the alarm has fired.
Signal diagnostics module that the alarm has fired.
Function Documentation#
otPlatAlarmMicroStartAt#
void otPlatAlarmMicroStartAt (otInstance * aInstance, uint32_t aT0, uint32_t aDt)
Set the alarm to fire at aDt microseconds after aT0. 
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. | 
| uint32_t | [in] | aT0 | The reference time. | 
| uint32_t | [in] | aDt | The time delay in microseconds from  | 
For aT0, the platform MUST support all values in [0, 2^32-1]. For aDt, the platform MUST support all values in [0, 2^31-1].
otPlatAlarmMicroStop#
void otPlatAlarmMicroStop (otInstance * aInstance)
Stop the alarm.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. | 
otPlatAlarmMicroGetNow#
uint32_t otPlatAlarmMicroGetNow (void )
Get the current time.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
The current time MUST represent a free-running timer. When maintaining current time, the time value MUST utilize the entire range [0, 2^32-1] and MUST NOT wrap before 2^32.
Returns
- The current time in microseconds. 
otPlatAlarmMicroFired#
void otPlatAlarmMicroFired (otInstance * aInstance)
Signal that the alarm has fired.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. | 
otPlatAlarmMilliStartAt#
void otPlatAlarmMilliStartAt (otInstance * aInstance, uint32_t aT0, uint32_t aDt)
Set the alarm to fire at aDt milliseconds after aT0. 
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. | 
| uint32_t | [in] | aT0 | The reference time. | 
| uint32_t | [in] | aDt | The time delay in milliseconds from  | 
For aT0 the platform MUST support all values in [0, 2^32-1]. For aDt, the platform MUST support all values in [0, 2^31-1].
otPlatAlarmMilliStop#
void otPlatAlarmMilliStop (otInstance * aInstance)
Stop the alarm.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. | 
otPlatAlarmMilliGetNow#
uint32_t otPlatAlarmMilliGetNow (void )
Get the current time.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
The current time MUST represent a free-running timer. When maintaining current time, the time value MUST utilize the entire range [0, 2^32-1] and MUST NOT wrap before 2^32.
Returns
- The current time in milliseconds. 
otPlatAlarmMilliFired#
void otPlatAlarmMilliFired (otInstance * aInstance)
Signal that the alarm has fired.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. | 
otPlatDiagAlarmFired#
void otPlatDiagAlarmFired (otInstance * aInstance)
Signal diagnostics module that the alarm has fired.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| otInstance * | [in] | aInstance | The OpenThread instance structure. |