CoAP#

This module includes functions that control CoAP communication.

The functions in this module are available when CoAP API feature (OPENTHREAD_CONFIG_COAP_API_ENABLE) is enabled.

Modules#

otCoapOption

otCoapOptionIterator

otCoapResource

otCoapBlockwiseResource

otCoapTxParameters

Enumerations#

enum
OT_COAP_TYPE_CONFIRMABLE = 0
OT_COAP_TYPE_NON_CONFIRMABLE = 1
OT_COAP_TYPE_ACKNOWLEDGMENT = 2
OT_COAP_TYPE_RESET = 3
}

CoAP Type values (2 bit unsigned integer).

enum
OT_COAP_CODE_EMPTY = OT_COAP_CODE(0, 0)
OT_COAP_CODE_GET = OT_COAP_CODE(0, 1)
OT_COAP_CODE_POST = OT_COAP_CODE(0, 2)
OT_COAP_CODE_PUT = OT_COAP_CODE(0, 3)
OT_COAP_CODE_DELETE = OT_COAP_CODE(0, 4)
OT_COAP_CODE_RESPONSE_MIN = OT_COAP_CODE(2, 0)
OT_COAP_CODE_CREATED = OT_COAP_CODE(2, 1)
OT_COAP_CODE_DELETED = OT_COAP_CODE(2, 2)
OT_COAP_CODE_VALID = OT_COAP_CODE(2, 3)
OT_COAP_CODE_CHANGED = OT_COAP_CODE(2, 4)
OT_COAP_CODE_CONTENT = OT_COAP_CODE(2, 5)
OT_COAP_CODE_CONTINUE = OT_COAP_CODE(2, 31)
OT_COAP_CODE_BAD_REQUEST = OT_COAP_CODE(4, 0)
OT_COAP_CODE_UNAUTHORIZED = OT_COAP_CODE(4, 1)
OT_COAP_CODE_BAD_OPTION = OT_COAP_CODE(4, 2)
OT_COAP_CODE_FORBIDDEN = OT_COAP_CODE(4, 3)
OT_COAP_CODE_NOT_FOUND = OT_COAP_CODE(4, 4)
OT_COAP_CODE_METHOD_NOT_ALLOWED = OT_COAP_CODE(4, 5)
OT_COAP_CODE_NOT_ACCEPTABLE = OT_COAP_CODE(4, 6)
OT_COAP_CODE_REQUEST_INCOMPLETE = OT_COAP_CODE(4, 8)
OT_COAP_CODE_PRECONDITION_FAILED = OT_COAP_CODE(4, 12)
OT_COAP_CODE_REQUEST_TOO_LARGE = OT_COAP_CODE(4, 13)
OT_COAP_CODE_UNSUPPORTED_FORMAT = OT_COAP_CODE(4, 15)
OT_COAP_CODE_INTERNAL_ERROR = OT_COAP_CODE(5, 0)
OT_COAP_CODE_NOT_IMPLEMENTED = OT_COAP_CODE(5, 1)
OT_COAP_CODE_BAD_GATEWAY = OT_COAP_CODE(5, 2)
OT_COAP_CODE_SERVICE_UNAVAILABLE = OT_COAP_CODE(5, 3)
OT_COAP_CODE_GATEWAY_TIMEOUT = OT_COAP_CODE(5, 4)
OT_COAP_CODE_PROXY_NOT_SUPPORTED = OT_COAP_CODE(5, 5)
}

CoAP Code values.

enum
OT_COAP_OPTION_IF_MATCH = 1
OT_COAP_OPTION_URI_HOST = 3
OT_COAP_OPTION_E_TAG = 4
OT_COAP_OPTION_IF_NONE_MATCH = 5
OT_COAP_OPTION_OBSERVE = 6
OT_COAP_OPTION_URI_PORT = 7
OT_COAP_OPTION_LOCATION_PATH = 8
OT_COAP_OPTION_URI_PATH = 11
OT_COAP_OPTION_CONTENT_FORMAT = 12
OT_COAP_OPTION_MAX_AGE = 14
OT_COAP_OPTION_URI_QUERY = 15
OT_COAP_OPTION_ACCEPT = 17
OT_COAP_OPTION_LOCATION_QUERY = 20
OT_COAP_OPTION_BLOCK2 = 23
OT_COAP_OPTION_BLOCK1 = 27
OT_COAP_OPTION_SIZE2 = 28
OT_COAP_OPTION_PROXY_URI = 35
OT_COAP_OPTION_PROXY_SCHEME = 39
OT_COAP_OPTION_SIZE1 = 60
}

CoAP Option Numbers.

enum
OT_COAP_OPTION_CONTENT_FORMAT_TEXT_PLAIN = 0
OT_COAP_OPTION_CONTENT_FORMAT_COSE_ENCRYPT0 = 16
OT_COAP_OPTION_CONTENT_FORMAT_COSE_MAC0 = 17
OT_COAP_OPTION_CONTENT_FORMAT_COSE_SIGN1 = 18
OT_COAP_OPTION_CONTENT_FORMAT_LINK_FORMAT = 40
OT_COAP_OPTION_CONTENT_FORMAT_XML = 41
OT_COAP_OPTION_CONTENT_FORMAT_OCTET_STREAM = 42
OT_COAP_OPTION_CONTENT_FORMAT_EXI = 47
OT_COAP_OPTION_CONTENT_FORMAT_JSON = 50
OT_COAP_OPTION_CONTENT_FORMAT_JSON_PATCH_JSON = 51
OT_COAP_OPTION_CONTENT_FORMAT_MERGE_PATCH_JSON = 52
OT_COAP_OPTION_CONTENT_FORMAT_CBOR = 60
OT_COAP_OPTION_CONTENT_FORMAT_CWT = 61
OT_COAP_OPTION_CONTENT_FORMAT_COSE_ENCRYPT = 96
OT_COAP_OPTION_CONTENT_FORMAT_COSE_MAC = 97
OT_COAP_OPTION_CONTENT_FORMAT_COSE_SIGN = 98
OT_COAP_OPTION_CONTENT_FORMAT_COSE_KEY = 101
OT_COAP_OPTION_CONTENT_FORMAT_COSE_KEY_SET = 102
OT_COAP_OPTION_CONTENT_FORMAT_SENML_JSON = 110
OT_COAP_OPTION_CONTENT_FORMAT_SENSML_JSON = 111
OT_COAP_OPTION_CONTENT_FORMAT_SENML_CBOR = 112
OT_COAP_OPTION_CONTENT_FORMAT_SENSML_CBOR = 113
OT_COAP_OPTION_CONTENT_FORMAT_SENML_EXI = 114
OT_COAP_OPTION_CONTENT_FORMAT_SENSML_EXI = 115
OT_COAP_OPTION_CONTENT_FORMAT_COAP_GROUP_JSON = 256
OT_COAP_OPTION_CONTENT_FORMAT_SENML_XML = 310
OT_COAP_OPTION_CONTENT_FORMAT_SENSML_XML = 311
}

CoAP Content Format codes.

enum
OT_COAP_OPTION_BLOCK_SZX_16 = 0
OT_COAP_OPTION_BLOCK_SZX_32 = 1
OT_COAP_OPTION_BLOCK_SZX_64 = 2
OT_COAP_OPTION_BLOCK_SZX_128 = 3
OT_COAP_OPTION_BLOCK_SZX_256 = 4
OT_COAP_OPTION_BLOCK_SZX_512 = 5
OT_COAP_OPTION_BLOCK_SZX_1024 = 6
}

CoAP Block Size Exponents.

Typedefs#

typedef enum otCoapType

CoAP Type values (2 bit unsigned integer).

typedef enum otCoapCode

CoAP Code values.

typedef enum otCoapOptionType

CoAP Option Numbers.

typedef struct otCoapOption

Represents a CoAP option.

typedef struct otCoapOptionIterator

Acts as an iterator for CoAP options.

CoAP Content Format codes.

typedef enum otCoapBlockSzx

CoAP Block Size Exponents.

typedef void(*
otCoapResponseHandler)(void *aContext, otMessage *aMessage, const otMessageInfo *aMessageInfo, otError aResult)

Pointer is called when a CoAP response is received or on the request timeout.

typedef void(*
otCoapRequestHandler)(void *aContext, otMessage *aMessage, const otMessageInfo *aMessageInfo)

Pointer is called when a CoAP request with a given Uri-Path is received.

typedef otError(*
otCoapBlockwiseReceiveHook)(void *aContext, const uint8_t *aBlock, uint32_t aPosition, uint16_t aBlockLength, bool aMore, uint32_t aTotalLength)

Pointer is called when a CoAP message with a block-wise transfer option is received.

typedef otError(*
otCoapBlockwiseTransmitHook)(void *aContext, uint8_t *aBlock, uint32_t aPosition, uint16_t *aBlockLength, bool *aMore)

Pointer is called before the next block in a block-wise transfer is sent.

typedef struct otCoapResource

Represents a CoAP resource.

Represents a CoAP resource with block-wise transfer.

typedef struct otCoapTxParameters

Represents the CoAP transmission parameters.

Functions#

void
otCoapMessageInit(otMessage *aMessage, otCoapType aType, otCoapCode aCode)

Initializes the CoAP header.

otCoapMessageInitResponse(otMessage *aResponse, const otMessage *aRequest, otCoapType aType, otCoapCode aCode)

Initializes a response message.

otCoapMessageSetToken(otMessage *aMessage, const uint8_t *aToken, uint8_t aTokenLength)

Sets the Token value and length in a header.

void
otCoapMessageGenerateToken(otMessage *aMessage, uint8_t aTokenLength)

Sets the Token length and randomizes its value.

otCoapMessageAppendContentFormatOption(otMessage *aMessage, otCoapOptionContentFormat aContentFormat)

Appends the Content Format CoAP option as specified in https://tools.ietf.org/html/rfc7252#page-92.

otCoapMessageAppendOption(otMessage *aMessage, uint16_t aNumber, uint16_t aLength, const void *aValue)

Appends a CoAP option in a header.

otCoapMessageAppendUintOption(otMessage *aMessage, uint16_t aNumber, uint32_t aValue)

Appends an unsigned integer CoAP option as specified in https://tools.ietf.org/html/rfc7252#section-3.2.

otCoapMessageAppendObserveOption(otMessage *aMessage, uint32_t aObserve)

Appends an Observe option.

otCoapMessageAppendUriPathOptions(otMessage *aMessage, const char *aUriPath)

Appends a Uri-Path option.

uint16_t
otCoapBlockSizeFromExponent(otCoapBlockSzx aSize)

Converts a CoAP Block option SZX field to the actual block size.

otCoapMessageAppendBlock2Option(otMessage *aMessage, uint32_t aNum, bool aMore, otCoapBlockSzx aSize)

Appends a Block2 option.

otCoapMessageAppendBlock1Option(otMessage *aMessage, uint32_t aNum, bool aMore, otCoapBlockSzx aSize)

Appends a Block1 option.

otCoapMessageAppendProxyUriOption(otMessage *aMessage, const char *aUriPath)

Appends a Proxy-Uri option.

otCoapMessageAppendMaxAgeOption(otMessage *aMessage, uint32_t aMaxAge)

Appends a Max-Age option.

otCoapMessageAppendUriQueryOption(otMessage *aMessage, const char *aUriQuery)

Appends a single Uri-Query option.

otCoapMessageSetPayloadMarker(otMessage *aMessage)

Adds Payload Marker indicating beginning of the payload to the CoAP header.

otCoapMessageGetType(const otMessage *aMessage)

Returns the Type value.

otCoapMessageGetCode(const otMessage *aMessage)

Returns the Code value.

void
otCoapMessageSetCode(otMessage *aMessage, otCoapCode aCode)

Sets the Code value.

const char *
otCoapMessageCodeToString(const otMessage *aMessage)

Returns the CoAP Code as human readable string.

uint16_t
otCoapMessageGetMessageId(const otMessage *aMessage)

Returns the Message ID value.

uint8_t
otCoapMessageGetTokenLength(const otMessage *aMessage)

Returns the Token length.

const uint8_t *
otCoapMessageGetToken(const otMessage *aMessage)

Returns a pointer to the Token value.

otCoapOptionIteratorInit(otCoapOptionIterator *aIterator, const otMessage *aMessage)

Initialises an iterator for the options in the given message.

const otCoapOption *
otCoapOptionIteratorGetFirstOptionMatching(otCoapOptionIterator *aIterator, uint16_t aOption)

Returns a pointer to the first option matching the specified option number.

const otCoapOption *
otCoapOptionIteratorGetFirstOption(otCoapOptionIterator *aIterator)

Returns a pointer to the first option.

const otCoapOption *
otCoapOptionIteratorGetNextOptionMatching(otCoapOptionIterator *aIterator, uint16_t aOption)

Returns a pointer to the next option matching the specified option number.

const otCoapOption *
otCoapOptionIteratorGetNextOption(otCoapOptionIterator *aIterator)

Returns a pointer to the next option.

otCoapOptionIteratorGetOptionUintValue(otCoapOptionIterator *aIterator, uint64_t *aValue)

Fills current option value into aValue assuming the current value is an unsigned integer encoded according to https://tools.ietf.org/html/rfc7252#section-3.2.

otCoapOptionIteratorGetOptionValue(otCoapOptionIterator *aIterator, void *aValue)

Fills current option value into aValue.

otCoapNewMessage(otInstance *aInstance, const otMessageSettings *aSettings)

Creates a new CoAP message.

otCoapSendRequestWithParameters(otInstance *aInstance, otMessage *aMessage, const otMessageInfo *aMessageInfo, otCoapResponseHandler aHandler, void *aContext, const otCoapTxParameters *aTxParameters)

Sends a CoAP request with custom transmission parameters.

otCoapSendRequestBlockWiseWithParameters(otInstance *aInstance, otMessage *aMessage, const otMessageInfo *aMessageInfo, otCoapResponseHandler aHandler, void *aContext, const otCoapTxParameters *aTxParameters, otCoapBlockwiseTransmitHook aTransmitHook, otCoapBlockwiseReceiveHook aReceiveHook)

Sends a CoAP request block-wise with custom transmission parameters.

otCoapSendRequestBlockWise(otInstance *aInstance, otMessage *aMessage, const otMessageInfo *aMessageInfo, otCoapResponseHandler aHandler, void *aContext, otCoapBlockwiseTransmitHook aTransmitHook, otCoapBlockwiseReceiveHook aReceiveHook)

Sends a CoAP request block-wise.

otCoapSendRequest(otInstance *aInstance, otMessage *aMessage, const otMessageInfo *aMessageInfo, otCoapResponseHandler aHandler, void *aContext)

Sends a CoAP request.

otCoapStart(otInstance *aInstance, uint16_t aPort)

Starts the CoAP server.

otCoapStop(otInstance *aInstance)

Stops the CoAP server.

void
otCoapAddResource(otInstance *aInstance, otCoapResource *aResource)

Adds a resource to the CoAP server.

void
otCoapRemoveResource(otInstance *aInstance, otCoapResource *aResource)

Removes a resource from the CoAP server.

void
otCoapAddBlockWiseResource(otInstance *aInstance, otCoapBlockwiseResource *aResource)

Adds a block-wise resource to the CoAP server.

void
otCoapRemoveBlockWiseResource(otInstance *aInstance, otCoapBlockwiseResource *aResource)

Removes a block-wise resource from the CoAP server.

void
otCoapSetDefaultHandler(otInstance *aInstance, otCoapRequestHandler aHandler, void *aContext)

Sets the default handler for unhandled CoAP requests.

otCoapSendResponseWithParameters(otInstance *aInstance, otMessage *aMessage, const otMessageInfo *aMessageInfo, const otCoapTxParameters *aTxParameters)

Sends a CoAP response from the server with custom transmission parameters.

otCoapSendResponseBlockWiseWithParameters(otInstance *aInstance, otMessage *aMessage, const otMessageInfo *aMessageInfo, const otCoapTxParameters *aTxParameters, void *aContext, otCoapBlockwiseTransmitHook aTransmitHook)

Sends a CoAP response block-wise from the server with custom transmission parameters.

otCoapSendResponseBlockWise(otInstance *aInstance, otMessage *aMessage, const otMessageInfo *aMessageInfo, void *aContext, otCoapBlockwiseTransmitHook aTransmitHook)

Sends a CoAP response block-wise from the server.

otCoapSendResponse(otInstance *aInstance, otMessage *aMessage, const otMessageInfo *aMessageInfo)

Sends a CoAP response from the server.

Macros#

#define

Default CoAP port, as specified in RFC 7252.

#define

Default token length.

#define

Max token length as specified (RFC 7252).

#define

Max retransmit supported by OpenThread.

#define

Minimal ACK timeout in milliseconds supported by OpenThread.

#define

Helper macro to define CoAP Code values.

Enumeration Documentation#

otCoapType#

otCoapType

CoAP Type values (2 bit unsigned integer).

Enumerator
OT_COAP_TYPE_CONFIRMABLE

Confirmable.

OT_COAP_TYPE_NON_CONFIRMABLE

Non-confirmable.

OT_COAP_TYPE_ACKNOWLEDGMENT

Acknowledgment.

OT_COAP_TYPE_RESET

Reset.


otCoapCode#

otCoapCode

CoAP Code values.

Enumerator
OT_COAP_CODE_EMPTY

Empty message code.

OT_COAP_CODE_GET

Get.

OT_COAP_CODE_POST

Post.

OT_COAP_CODE_PUT

Put.

OT_COAP_CODE_DELETE

Delete.

OT_COAP_CODE_RESPONSE_MIN

2.00

OT_COAP_CODE_CREATED

Created.

OT_COAP_CODE_DELETED

Deleted.

OT_COAP_CODE_VALID

Valid.

OT_COAP_CODE_CHANGED

Changed.

OT_COAP_CODE_CONTENT

Content.

OT_COAP_CODE_CONTINUE

RFC7959 Continue.

OT_COAP_CODE_BAD_REQUEST

Bad Request.

OT_COAP_CODE_UNAUTHORIZED

Unauthorized.

OT_COAP_CODE_BAD_OPTION

Bad Option.

OT_COAP_CODE_FORBIDDEN

Forbidden.

OT_COAP_CODE_NOT_FOUND

Not Found.

OT_COAP_CODE_METHOD_NOT_ALLOWED

Method Not Allowed.

OT_COAP_CODE_NOT_ACCEPTABLE

Not Acceptable.

OT_COAP_CODE_REQUEST_INCOMPLETE

RFC7959 Request Entity Incomplete.

OT_COAP_CODE_PRECONDITION_FAILED

Precondition Failed.

OT_COAP_CODE_REQUEST_TOO_LARGE

Request Entity Too Large.

OT_COAP_CODE_UNSUPPORTED_FORMAT

Unsupported Content-Format.

OT_COAP_CODE_INTERNAL_ERROR

Internal Server Error.

OT_COAP_CODE_NOT_IMPLEMENTED

Not Implemented.

OT_COAP_CODE_BAD_GATEWAY

Bad Gateway.

OT_COAP_CODE_SERVICE_UNAVAILABLE

Service Unavailable.

OT_COAP_CODE_GATEWAY_TIMEOUT

Gateway Timeout.

OT_COAP_CODE_PROXY_NOT_SUPPORTED

Proxying Not Supported.


otCoapOptionType#

otCoapOptionType

CoAP Option Numbers.

Enumerator
OT_COAP_OPTION_IF_MATCH

If-Match.

OT_COAP_OPTION_URI_HOST

Uri-Host.

OT_COAP_OPTION_E_TAG

ETag.

OT_COAP_OPTION_IF_NONE_MATCH

If-None-Match.

OT_COAP_OPTION_OBSERVE

Observe [RFC7641].

OT_COAP_OPTION_URI_PORT

Uri-Port.

OT_COAP_OPTION_LOCATION_PATH

Location-Path.

OT_COAP_OPTION_URI_PATH

Uri-Path.

OT_COAP_OPTION_CONTENT_FORMAT

Content-Format.

OT_COAP_OPTION_MAX_AGE

Max-Age.

OT_COAP_OPTION_URI_QUERY

Uri-Query.

OT_COAP_OPTION_ACCEPT

Accept.

OT_COAP_OPTION_LOCATION_QUERY

Location-Query.

OT_COAP_OPTION_BLOCK2

Block2 (RFC7959)

OT_COAP_OPTION_BLOCK1

Block1 (RFC7959)

OT_COAP_OPTION_SIZE2

Size2 (RFC7959)

OT_COAP_OPTION_PROXY_URI

Proxy-Uri.

OT_COAP_OPTION_PROXY_SCHEME

Proxy-Scheme.

OT_COAP_OPTION_SIZE1

Size1.


otCoapOptionContentFormat#

otCoapOptionContentFormat

CoAP Content Format codes.

The full list is documented at https://www.iana.org/assignments/core-parameters/core-parameters.xhtml#content-formats

Enumerator
OT_COAP_OPTION_CONTENT_FORMAT_TEXT_PLAIN

text/plain; charset=utf-8: [RFC2046][RFC3676][RFC5147]

OT_COAP_OPTION_CONTENT_FORMAT_COSE_ENCRYPT0

application/cose; cose-type="cose-encrypt0": [RFC8152]

OT_COAP_OPTION_CONTENT_FORMAT_COSE_MAC0

application/cose; cose-type="cose-mac0": [RFC8152]

OT_COAP_OPTION_CONTENT_FORMAT_COSE_SIGN1

application/cose; cose-type="cose-sign1": [RFC8152]

OT_COAP_OPTION_CONTENT_FORMAT_LINK_FORMAT

application/link-format: [RFC6690]

OT_COAP_OPTION_CONTENT_FORMAT_XML

application/xml: [RFC3023]

OT_COAP_OPTION_CONTENT_FORMAT_OCTET_STREAM

application/octet-stream: [RFC2045][RFC2046]

OT_COAP_OPTION_CONTENT_FORMAT_EXI

application/exi: ["Efficient XML Interchange (EXI) Format 1.0 (Second Edition)", February 2014]

OT_COAP_OPTION_CONTENT_FORMAT_JSON

application/json: [RFC7159]

OT_COAP_OPTION_CONTENT_FORMAT_JSON_PATCH_JSON

application/json-patch+json: [RFC6902]

OT_COAP_OPTION_CONTENT_FORMAT_MERGE_PATCH_JSON

application/merge-patch+json: [RFC7396]

OT_COAP_OPTION_CONTENT_FORMAT_CBOR

application/cbor: [RFC7049]

OT_COAP_OPTION_CONTENT_FORMAT_CWT

application/cwt: [RFC8392]

OT_COAP_OPTION_CONTENT_FORMAT_COSE_ENCRYPT

application/cose; cose-type="cose-encrypt": [RFC8152]

OT_COAP_OPTION_CONTENT_FORMAT_COSE_MAC

application/cose; cose-type="cose-mac": [RFC8152]

OT_COAP_OPTION_CONTENT_FORMAT_COSE_SIGN

application/cose; cose-type="cose-sign": [RFC8152]

OT_COAP_OPTION_CONTENT_FORMAT_COSE_KEY

application/cose-key: [RFC8152]

OT_COAP_OPTION_CONTENT_FORMAT_COSE_KEY_SET

application/cose-key-set: [RFC8152]

OT_COAP_OPTION_CONTENT_FORMAT_SENML_JSON

application/senml+json: [RFC8428]

OT_COAP_OPTION_CONTENT_FORMAT_SENSML_JSON

application/sensml+json: [RFC8428]

OT_COAP_OPTION_CONTENT_FORMAT_SENML_CBOR

application/senml+cbor: [RFC8428]

OT_COAP_OPTION_CONTENT_FORMAT_SENSML_CBOR

application/sensml+cbor: [RFC8428]

OT_COAP_OPTION_CONTENT_FORMAT_SENML_EXI

application/senml-exi: [RFC8428]

OT_COAP_OPTION_CONTENT_FORMAT_SENSML_EXI

application/sensml-exi: [RFC8428]

OT_COAP_OPTION_CONTENT_FORMAT_COAP_GROUP_JSON

application/coap-group+json: [RFC7390]

OT_COAP_OPTION_CONTENT_FORMAT_SENML_XML

application/senml+xml: [RFC8428]

OT_COAP_OPTION_CONTENT_FORMAT_SENSML_XML

application/sensml+xml: [RFC8428]


otCoapBlockSzx#

otCoapBlockSzx

CoAP Block Size Exponents.

Enumerator
OT_COAP_OPTION_BLOCK_SZX_16
OT_COAP_OPTION_BLOCK_SZX_32
OT_COAP_OPTION_BLOCK_SZX_64
OT_COAP_OPTION_BLOCK_SZX_128
OT_COAP_OPTION_BLOCK_SZX_256
OT_COAP_OPTION_BLOCK_SZX_512
OT_COAP_OPTION_BLOCK_SZX_1024

Typedef Documentation#

otCoapType#

typedef enum otCoapType otCoapType

CoAP Type values (2 bit unsigned integer).


otCoapCode#

typedef enum otCoapCode otCoapCode

CoAP Code values.


otCoapOptionType#

typedef enum otCoapOptionType otCoapOptionType

CoAP Option Numbers.


otCoapOption#

typedef struct otCoapOption otCoapOption

Represents a CoAP option.


otCoapOptionIterator#

typedef struct otCoapOptionIterator otCoapOptionIterator

Acts as an iterator for CoAP options.


otCoapOptionContentFormat#

typedef enum otCoapOptionContentFormat otCoapOptionContentFormat

CoAP Content Format codes.

The full list is documented at https://www.iana.org/assignments/core-parameters/core-parameters.xhtml#content-formats


otCoapBlockSzx#

typedef enum otCoapBlockSzx otCoapBlockSzx

CoAP Block Size Exponents.


otCoapResponseHandler#

typedef void(* otCoapResponseHandler) (void *aContext, otMessage *aMessage, const otMessageInfo *aMessageInfo, otError aResult) )(void *aContext, otMessage *aMessage, const otMessageInfo *aMessageInfo, otError aResult)

Pointer is called when a CoAP response is received or on the request timeout.

Parameters
TypeDirectionArgument NameDescription
[in]aContext

A pointer to application-specific context.

[in]aMessage

A pointer to the message buffer containing the response. NULL if no response was received.

[in]aMessageInfo

A pointer to the message info for aMessage. NULL if no response was received.

[in]aResult

A result of the CoAP transaction.


otCoapRequestHandler#

typedef void(* otCoapRequestHandler) (void *aContext, otMessage *aMessage, const otMessageInfo *aMessageInfo) )(void *aContext, otMessage *aMessage, const otMessageInfo *aMessageInfo)

Pointer is called when a CoAP request with a given Uri-Path is received.

Parameters
TypeDirectionArgument NameDescription
[in]aContext

A pointer to arbitrary context information.

[in]aMessage

A pointer to the message.

[in]aMessageInfo

A pointer to the message info for aMessage.


otCoapBlockwiseReceiveHook#

typedef otError(* otCoapBlockwiseReceiveHook) (void *aContext, const uint8_t *aBlock, uint32_t aPosition, uint16_t aBlockLength, bool aMore, uint32_t aTotalLength) )(void *aContext, const uint8_t *aBlock, uint32_t aPosition, uint16_t aBlockLength, bool aMore, uint32_t aTotalLength)

Pointer is called when a CoAP message with a block-wise transfer option is received.

Parameters
TypeDirectionArgument NameDescription
[in]aContext

A pointer to application-specific context.

[in]aBlock

A pointer to the block segment.

[in]aPosition

The position of aBlock in a sequence in bytes.

[in]aBlockLength

The length of the block segment in bytes.

[in]aMore

Flag if more block segments are following.

[in]aTotalLength

The total length in bytes of the transferred information (indicated by a Size1 or Size2 option).

Is available when OPENTHREAD_CONFIG_COAP_BLOCKWISE_TRANSFER_ENABLE configuration is enabled.


otCoapBlockwiseTransmitHook#

typedef otError(* otCoapBlockwiseTransmitHook) (void *aContext, uint8_t *aBlock, uint32_t aPosition, uint16_t *aBlockLength, bool *aMore) )(void *aContext, uint8_t *aBlock, uint32_t aPosition, uint16_t *aBlockLength, bool *aMore)

Pointer is called before the next block in a block-wise transfer is sent.

Parameters
TypeDirectionArgument NameDescription
[in]aContext

A pointer to application-specific context.

[inout]aBlock

A pointer to where the block segment can be written to.

[in]aPosition

The position in a sequence from which to obtain the block segment.

[inout]aBlockLength

On entry, the maximum block segment length in bytes.

[out]aMore

A pointer to the flag if more block segments will follow.

Is available when OPENTHREAD_CONFIG_COAP_BLOCKWISE_TRANSFER_ENABLE configuration is enabled.

Warnings

  • By changing the value of aBlockLength, the block size of the whole exchange is renegotiated. It is recommended to do this after the first block has been received as later changes could cause problems with other CoAP implementations.


otCoapResource#

typedef struct otCoapResource otCoapResource

Represents a CoAP resource.


otCoapBlockwiseResource#

typedef struct otCoapBlockwiseResource otCoapBlockwiseResource

Represents a CoAP resource with block-wise transfer.


otCoapTxParameters#

typedef struct otCoapTxParameters otCoapTxParameters

Represents the CoAP transmission parameters.

Note

  • mAckTimeout * ((2 ** (mMaxRetransmit + 1)) - 1) * (mAckRandomFactorNumerator / mAckRandomFactorDenominator) must not exceed what can be represented by a uint32_t (0xffffffff). This limitation allows OpenThread to avoid 64-bit arithmetic.


Function Documentation#

otCoapMessageInit#

void otCoapMessageInit (otMessage * aMessage, otCoapType aType, otCoapCode aCode)

Initializes the CoAP header.

Parameters
TypeDirectionArgument NameDescription
otMessage *[inout]aMessage

A pointer to the CoAP message to initialize.

otCoapType[in]aType

CoAP message type.

otCoapCode[in]aCode

CoAP message code.


otCoapMessageInitResponse#

otError otCoapMessageInitResponse (otMessage * aResponse, const otMessage * aRequest, otCoapType aType, otCoapCode aCode)

Initializes a response message.

Parameters
TypeDirectionArgument NameDescription
otMessage *[inout]aResponse

A pointer to the CoAP response message.

const otMessage *[in]aRequest

A pointer to the CoAP request message.

otCoapType[in]aType

CoAP message type.

otCoapCode[in]aCode

CoAP message code.

Note

  • Both message ID and token are set according to aRequest.


otCoapMessageSetToken#

otError otCoapMessageSetToken (otMessage * aMessage, const uint8_t * aToken, uint8_t aTokenLength)

Sets the Token value and length in a header.

Parameters
TypeDirectionArgument NameDescription
otMessage *[inout]aMessage

A pointer to the CoAP message.

const uint8_t *[in]aToken

A pointer to the Token value.

uint8_t[in]aTokenLength

The Length of aToken.


otCoapMessageGenerateToken#

void otCoapMessageGenerateToken (otMessage * aMessage, uint8_t aTokenLength)

Sets the Token length and randomizes its value.

Parameters
TypeDirectionArgument NameDescription
otMessage *[inout]aMessage

A pointer to the CoAP message.

uint8_t[in]aTokenLength

The Length of a Token to set.


otCoapMessageAppendContentFormatOption#

otError otCoapMessageAppendContentFormatOption (otMessage * aMessage, otCoapOptionContentFormat aContentFormat)

Appends the Content Format CoAP option as specified in https://tools.ietf.org/html/rfc7252#page-92.

Parameters
TypeDirectionArgument NameDescription
otMessage *[inout]aMessage

A pointer to the CoAP message.

otCoapOptionContentFormat[in]aContentFormat

One of the content formats listed in otCoapOptionContentFormat above.

This must be called before setting otCoapMessageSetPayloadMarker if a payload is to be included in the message.

The function is a convenience wrapper around otCoapMessageAppendUintOption, and if the desired format type code isn't listed in otCoapOptionContentFormat, this base function should be used instead.


otCoapMessageAppendOption#

otError otCoapMessageAppendOption (otMessage * aMessage, uint16_t aNumber, uint16_t aLength, const void * aValue)

Appends a CoAP option in a header.

Parameters
TypeDirectionArgument NameDescription
otMessage *[inout]aMessage

A pointer to the CoAP message.

uint16_t[in]aNumber

The CoAP Option number.

uint16_t[in]aLength

The CoAP Option length.

const void *[in]aValue

A pointer to the CoAP value.


otCoapMessageAppendUintOption#

otError otCoapMessageAppendUintOption (otMessage * aMessage, uint16_t aNumber, uint32_t aValue)

Appends an unsigned integer CoAP option as specified in https://tools.ietf.org/html/rfc7252#section-3.2.

Parameters
TypeDirectionArgument NameDescription
otMessage *[inout]aMessage

A pointer to the CoAP message.

uint16_t[in]aNumber

The CoAP Option number.

uint32_t[in]aValue

The CoAP Option unsigned integer value.

See Also

  • otCoapMessageGetOptionUintValue


otCoapMessageAppendObserveOption#

otError otCoapMessageAppendObserveOption (otMessage * aMessage, uint32_t aObserve)

Appends an Observe option.

Parameters
TypeDirectionArgument NameDescription
otMessage *[inout]aMessage

A pointer to the CoAP message.

uint32_t[in]aObserve

Observe field value.


otCoapMessageAppendUriPathOptions#

otError otCoapMessageAppendUriPathOptions (otMessage * aMessage, const char * aUriPath)

Appends a Uri-Path option.

Parameters
TypeDirectionArgument NameDescription
otMessage *[inout]aMessage

A pointer to the CoAP message.

const char *[in]aUriPath

A pointer to a NULL-terminated string.


otCoapBlockSizeFromExponent#

uint16_t otCoapBlockSizeFromExponent (otCoapBlockSzx aSize)

Converts a CoAP Block option SZX field to the actual block size.

Parameters
TypeDirectionArgument NameDescription
otCoapBlockSzx[in]aSize

Block size exponent.

Returns

  • The actual size exponent value.


otCoapMessageAppendBlock2Option#

otError otCoapMessageAppendBlock2Option (otMessage * aMessage, uint32_t aNum, bool aMore, otCoapBlockSzx aSize)

Appends a Block2 option.

Parameters
TypeDirectionArgument NameDescription
otMessage *[inout]aMessage

A pointer to the CoAP message.

uint32_t[in]aNum

Current block number.

bool[in]aMore

Boolean to indicate more blocks are to be sent.

otCoapBlockSzx[in]aSize

Block Size Exponent.


otCoapMessageAppendBlock1Option#

otError otCoapMessageAppendBlock1Option (otMessage * aMessage, uint32_t aNum, bool aMore, otCoapBlockSzx aSize)

Appends a Block1 option.

Parameters
TypeDirectionArgument NameDescription
otMessage *[inout]aMessage

A pointer to the CoAP message.

uint32_t[in]aNum

Current block number.

bool[in]aMore

Boolean to indicate more blocks are to be sent.

otCoapBlockSzx[in]aSize

Block Size Exponent.


otCoapMessageAppendProxyUriOption#

otError otCoapMessageAppendProxyUriOption (otMessage * aMessage, const char * aUriPath)

Appends a Proxy-Uri option.

Parameters
TypeDirectionArgument NameDescription
otMessage *[inout]aMessage

A pointer to the CoAP message.

const char *[in]aUriPath

A pointer to a NULL-terminated string.


otCoapMessageAppendMaxAgeOption#

otError otCoapMessageAppendMaxAgeOption (otMessage * aMessage, uint32_t aMaxAge)

Appends a Max-Age option.

Parameters
TypeDirectionArgument NameDescription
otMessage *[inout]aMessage

A pointer to the CoAP message.

uint32_t[in]aMaxAge

The Max-Age value.


otCoapMessageAppendUriQueryOption#

otError otCoapMessageAppendUriQueryOption (otMessage * aMessage, const char * aUriQuery)

Appends a single Uri-Query option.

Parameters
TypeDirectionArgument NameDescription
otMessage *[inout]aMessage

A pointer to the CoAP message.

const char *[in]aUriQuery

A pointer to NULL-terminated string, which should contain a single key=value pair.


otCoapMessageSetPayloadMarker#

otError otCoapMessageSetPayloadMarker (otMessage * aMessage)

Adds Payload Marker indicating beginning of the payload to the CoAP header.

Parameters
TypeDirectionArgument NameDescription
otMessage *[inout]aMessage

A pointer to the CoAP message.


otCoapMessageGetType#

otCoapType otCoapMessageGetType (const otMessage * aMessage)

Returns the Type value.

Parameters
TypeDirectionArgument NameDescription
const otMessage *[in]aMessage

A pointer to the CoAP message.

Returns

  • The Type value.


otCoapMessageGetCode#

otCoapCode otCoapMessageGetCode (const otMessage * aMessage)

Returns the Code value.

Parameters
TypeDirectionArgument NameDescription
const otMessage *[in]aMessage

A pointer to the CoAP message.

Returns

  • The Code value.


otCoapMessageSetCode#

void otCoapMessageSetCode (otMessage * aMessage, otCoapCode aCode)

Sets the Code value.

Parameters
TypeDirectionArgument NameDescription
otMessage *[inout]aMessage

A pointer to the CoAP message to initialize.

otCoapCode[in]aCode

CoAP message code.


otCoapMessageCodeToString#

const char * otCoapMessageCodeToString (const otMessage * aMessage)

Returns the CoAP Code as human readable string.

Parameters
TypeDirectionArgument NameDescription
const otMessage *[in]aMessage

A pointer to the CoAP message.

@ returns The CoAP Code as string.


otCoapMessageGetMessageId#

uint16_t otCoapMessageGetMessageId (const otMessage * aMessage)

Returns the Message ID value.

Parameters
TypeDirectionArgument NameDescription
const otMessage *[in]aMessage

A pointer to the CoAP message.

Returns

  • The Message ID value.


otCoapMessageGetTokenLength#

uint8_t otCoapMessageGetTokenLength (const otMessage * aMessage)

Returns the Token length.

Parameters
TypeDirectionArgument NameDescription
const otMessage *[in]aMessage

A pointer to the CoAP message.

Returns

  • The Token length.


otCoapMessageGetToken#

const uint8_t * otCoapMessageGetToken (const otMessage * aMessage)

Returns a pointer to the Token value.

Parameters
TypeDirectionArgument NameDescription
const otMessage *[in]aMessage

A pointer to the CoAP message.

Returns

  • A pointer to the Token value.


otCoapOptionIteratorInit#

otError otCoapOptionIteratorInit (otCoapOptionIterator * aIterator, const otMessage * aMessage)

Initialises an iterator for the options in the given message.

Parameters
TypeDirectionArgument NameDescription
otCoapOptionIterator *[inout]aIterator

A pointer to the CoAP message option iterator.

const otMessage *[in]aMessage

A pointer to the CoAP message.


otCoapOptionIteratorGetFirstOptionMatching#

const otCoapOption * otCoapOptionIteratorGetFirstOptionMatching (otCoapOptionIterator * aIterator, uint16_t aOption)

Returns a pointer to the first option matching the specified option number.

Parameters
TypeDirectionArgument NameDescription
otCoapOptionIterator *[in]aIterator

A pointer to the CoAP message option iterator.

uint16_t[in]aOption

The option number sought.

Returns

  • A pointer to the first matching option. If no matching option is present NULL pointer is returned.


otCoapOptionIteratorGetFirstOption#

const otCoapOption * otCoapOptionIteratorGetFirstOption (otCoapOptionIterator * aIterator)

Returns a pointer to the first option.

Parameters
TypeDirectionArgument NameDescription
otCoapOptionIterator *[inout]aIterator

A pointer to the CoAP message option iterator.

Returns

  • A pointer to the first option. If no option is present NULL pointer is returned.


otCoapOptionIteratorGetNextOptionMatching#

const otCoapOption * otCoapOptionIteratorGetNextOptionMatching (otCoapOptionIterator * aIterator, uint16_t aOption)

Returns a pointer to the next option matching the specified option number.

Parameters
TypeDirectionArgument NameDescription
otCoapOptionIterator *[in]aIterator

A pointer to the CoAP message option iterator.

uint16_t[in]aOption

The option number sought.

Returns

  • A pointer to the next matching option. If no further matching option is present NULL pointer is returned.


otCoapOptionIteratorGetNextOption#

const otCoapOption * otCoapOptionIteratorGetNextOption (otCoapOptionIterator * aIterator)

Returns a pointer to the next option.

Parameters
TypeDirectionArgument NameDescription
otCoapOptionIterator *[inout]aIterator

A pointer to the CoAP message option iterator.

Returns

  • A pointer to the next option. If no more options are present NULL pointer is returned.


otCoapOptionIteratorGetOptionUintValue#

otError otCoapOptionIteratorGetOptionUintValue (otCoapOptionIterator * aIterator, uint64_t * aValue)

Fills current option value into aValue assuming the current value is an unsigned integer encoded according to https://tools.ietf.org/html/rfc7252#section-3.2.

Parameters
TypeDirectionArgument NameDescription
otCoapOptionIterator *[inout]aIterator

A pointer to the CoAP message option iterator.

uint64_t *[out]aValue

A pointer to an unsigned integer to receive the option value.

See Also


otCoapOptionIteratorGetOptionValue#

otError otCoapOptionIteratorGetOptionValue (otCoapOptionIterator * aIterator, void * aValue)

Fills current option value into aValue.

Parameters
TypeDirectionArgument NameDescription
otCoapOptionIterator *[inout]aIterator

A pointer to the CoAP message option iterator.

void *[out]aValue

A pointer to a buffer to receive the option value.


otCoapNewMessage#

otMessage * otCoapNewMessage (otInstance * aInstance, const otMessageSettings * aSettings)

Creates a new CoAP message.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

const otMessageSettings *[in]aSettings

A pointer to the message settings or NULL to set default settings.

Note

  • If aSettings is 'NULL', the link layer security is enabled and the message priority is set to OT_MESSAGE_PRIORITY_NORMAL by default.

Returns

  • A pointer to the message buffer or NULL if no message buffers are available or parameters are invalid.


otCoapSendRequestWithParameters#

otError otCoapSendRequestWithParameters (otInstance * aInstance, otMessage * aMessage, const otMessageInfo * aMessageInfo, otCoapResponseHandler aHandler, void * aContext, const otCoapTxParameters * aTxParameters)

Sends a CoAP request with custom transmission parameters.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otMessage *[in]aMessage

A pointer to the message to send.

const otMessageInfo *[in]aMessageInfo

A pointer to the message info associated with aMessage.

otCoapResponseHandler[in]aHandler

A function pointer that shall be called on response reception or timeout.

void *[in]aContext

A pointer to arbitrary context information. May be NULL if not used.

const otCoapTxParameters *[in]aTxParameters

A pointer to transmission parameters for this request. Use NULL for defaults. Otherwise, parameters given must meet the following conditions:

  1. mMaxRetransmit is no more than OT_COAP_MAX_RETRANSMIT.

  2. mAckRandomFactorNumerator / mAckRandomFactorDenominator must not be below 1.0.

  3. The calculated exchange life time must not overflow uint32_t.

If a response for a request is expected, respective function and context information should be provided. If no response is expected, these arguments should be NULL pointers.


otCoapSendRequestBlockWiseWithParameters#

otError otCoapSendRequestBlockWiseWithParameters (otInstance * aInstance, otMessage * aMessage, const otMessageInfo * aMessageInfo, otCoapResponseHandler aHandler, void * aContext, const otCoapTxParameters * aTxParameters, otCoapBlockwiseTransmitHook aTransmitHook, otCoapBlockwiseReceiveHook aReceiveHook)

Sends a CoAP request block-wise with custom transmission parameters.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otMessage *[in]aMessage

A pointer to the message to send.

const otMessageInfo *[in]aMessageInfo

A pointer to the message info associated with aMessage.

otCoapResponseHandler[in]aHandler

A function pointer that shall be called on response reception or timeout.

void *[in]aContext

A pointer to arbitrary context information. May be NULL if not used.

const otCoapTxParameters *[in]aTxParameters

A pointer to transmission parameters for this request. Use NULL for defaults.

otCoapBlockwiseTransmitHook[in]aTransmitHook

A pointer to a hook function for outgoing block-wise transfer.

otCoapBlockwiseReceiveHook[in]aReceiveHook

A pointer to a hook function for incoming block-wise transfer.

Is available when OPENTHREAD_CONFIG_COAP_BLOCKWISE_TRANSFER_ENABLE configuration is enabled.

If a response for a request is expected, respective function and context information should be provided. If the response is expected to be block-wise, a respective hook function should be provided. If no response is expected, these arguments should be NULL pointers.


otCoapSendRequestBlockWise#

static otError otCoapSendRequestBlockWise (otInstance * aInstance, otMessage * aMessage, const otMessageInfo * aMessageInfo, otCoapResponseHandler aHandler, void * aContext, otCoapBlockwiseTransmitHook aTransmitHook, otCoapBlockwiseReceiveHook aReceiveHook)

Sends a CoAP request block-wise.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otMessage *[in]aMessage

A pointer to the message to send.

const otMessageInfo *[in]aMessageInfo

A pointer to the message info associated with aMessage.

otCoapResponseHandler[in]aHandler

A function pointer that shall be called on response reception or timeout.

void *[in]aContext

A pointer to arbitrary context information. May be NULL if not used.

otCoapBlockwiseTransmitHook[in]aTransmitHook

A pointer to a hook function for outgoing block-wise transfer.

otCoapBlockwiseReceiveHook[in]aReceiveHook

A pointer to a hook function for incoming block-wise transfer.

Is available when OPENTHREAD_CONFIG_COAP_BLOCKWISE_TRANSFER_ENABLE configuration is enabled.

If a response for a request is expected, respective function and context information should be provided. If the response is expected to be block-wise, a respective hook function should be provided. If no response is expected, these arguments should be NULL pointers.


otCoapSendRequest#

static otError otCoapSendRequest (otInstance * aInstance, otMessage * aMessage, const otMessageInfo * aMessageInfo, otCoapResponseHandler aHandler, void * aContext)

Sends a CoAP request.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otMessage *[in]aMessage

A pointer to the message to send.

const otMessageInfo *[in]aMessageInfo

A pointer to the message info associated with aMessage.

otCoapResponseHandler[in]aHandler

A function pointer that shall be called on response reception or timeout.

void *[in]aContext

A pointer to arbitrary context information. May be NULL if not used.

If a response for a request is expected, respective function and context information should be provided. If no response is expected, these arguments should be NULL pointers.


otCoapStart#

otError otCoapStart (otInstance * aInstance, uint16_t aPort)

Starts the CoAP server.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

uint16_t[in]aPort

The local UDP port to bind to.


otCoapStop#

otError otCoapStop (otInstance * aInstance)

Stops the CoAP server.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.


otCoapAddResource#

void otCoapAddResource (otInstance * aInstance, otCoapResource * aResource)

Adds a resource to the CoAP server.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otCoapResource *[in]aResource

A pointer to the resource.


otCoapRemoveResource#

void otCoapRemoveResource (otInstance * aInstance, otCoapResource * aResource)

Removes a resource from the CoAP server.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otCoapResource *[in]aResource

A pointer to the resource.


otCoapAddBlockWiseResource#

void otCoapAddBlockWiseResource (otInstance * aInstance, otCoapBlockwiseResource * aResource)

Adds a block-wise resource to the CoAP server.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otCoapBlockwiseResource *[in]aResource

A pointer to the resource.


otCoapRemoveBlockWiseResource#

void otCoapRemoveBlockWiseResource (otInstance * aInstance, otCoapBlockwiseResource * aResource)

Removes a block-wise resource from the CoAP server.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otCoapBlockwiseResource *[in]aResource

A pointer to the resource.


otCoapSetDefaultHandler#

void otCoapSetDefaultHandler (otInstance * aInstance, otCoapRequestHandler aHandler, void * aContext)

Sets the default handler for unhandled CoAP requests.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otCoapRequestHandler[in]aHandler

A function pointer that shall be called when an unhandled request arrives.

void *[in]aContext

A pointer to arbitrary context information. May be NULL if not used.


otCoapSendResponseWithParameters#

otError otCoapSendResponseWithParameters (otInstance * aInstance, otMessage * aMessage, const otMessageInfo * aMessageInfo, const otCoapTxParameters * aTxParameters)

Sends a CoAP response from the server with custom transmission parameters.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otMessage *[in]aMessage

A pointer to the CoAP response to send.

const otMessageInfo *[in]aMessageInfo

A pointer to the message info associated with aMessage.

const otCoapTxParameters *[in]aTxParameters

A pointer to transmission parameters for this response. Use NULL for defaults.


otCoapSendResponseBlockWiseWithParameters#

otError otCoapSendResponseBlockWiseWithParameters (otInstance * aInstance, otMessage * aMessage, const otMessageInfo * aMessageInfo, const otCoapTxParameters * aTxParameters, void * aContext, otCoapBlockwiseTransmitHook aTransmitHook)

Sends a CoAP response block-wise from the server with custom transmission parameters.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otMessage *[in]aMessage

A pointer to the CoAP response to send.

const otMessageInfo *[in]aMessageInfo

A pointer to the message info associated with aMessage.

const otCoapTxParameters *[in]aTxParameters

A pointer to transmission parameters for this response. Use NULL for defaults.

void *[in]aContext

A pointer to arbitrary context information. May be NULL if not used.

otCoapBlockwiseTransmitHook[in]aTransmitHook

A pointer to a hook function for outgoing block-wise transfer.

Is available when OPENTHREAD_CONFIG_COAP_BLOCKWISE_TRANSFER_ENABLE configuration is enabled.


otCoapSendResponseBlockWise#

static otError otCoapSendResponseBlockWise (otInstance * aInstance, otMessage * aMessage, const otMessageInfo * aMessageInfo, void * aContext, otCoapBlockwiseTransmitHook aTransmitHook)

Sends a CoAP response block-wise from the server.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otMessage *[in]aMessage

A pointer to the CoAP response to send.

const otMessageInfo *[in]aMessageInfo

A pointer to the message info associated with aMessage.

void *[in]aContext

A pointer to arbitrary context information. May be NULL if not used.

otCoapBlockwiseTransmitHook[in]aTransmitHook

A pointer to a hook function for outgoing block-wise transfer.

Is available when OPENTHREAD_CONFIG_COAP_BLOCKWISE_TRANSFER_ENABLE configuration is enabled.


otCoapSendResponse#

static otError otCoapSendResponse (otInstance * aInstance, otMessage * aMessage, const otMessageInfo * aMessageInfo)

Sends a CoAP response from the server.

Parameters
TypeDirectionArgument NameDescription
otInstance *[in]aInstance

A pointer to an OpenThread instance.

otMessage *[in]aMessage

A pointer to the CoAP response to send.

const otMessageInfo *[in]aMessageInfo

A pointer to the message info associated with aMessage.


Macro Definition Documentation#

OT_DEFAULT_COAP_PORT#

#define OT_DEFAULT_COAP_PORT
Value:
5683

Default CoAP port, as specified in RFC 7252.


OT_COAP_DEFAULT_TOKEN_LENGTH#

#define OT_COAP_DEFAULT_TOKEN_LENGTH
Value:
2

Default token length.


OT_COAP_MAX_TOKEN_LENGTH#

#define OT_COAP_MAX_TOKEN_LENGTH
Value:
8

Max token length as specified (RFC 7252).


OT_COAP_MAX_RETRANSMIT#

#define OT_COAP_MAX_RETRANSMIT
Value:
20

Max retransmit supported by OpenThread.


OT_COAP_MIN_ACK_TIMEOUT#

#define OT_COAP_MIN_ACK_TIMEOUT
Value:
1000

Minimal ACK timeout in milliseconds supported by OpenThread.


OT_COAP_CODE#

#define OT_COAP_CODE
Value:
(c, d)

Helper macro to define CoAP Code values.